Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Can Someone Review my Schematic for Android GPIO?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 410 subscribers
  • Views 2084 views
  • Users 0 members are here
  • android
  • arduino nano
  • mcp2200
  • arduino
Related

Can Someone Review my Schematic for Android GPIO?

mjones517
mjones517 over 1 year ago

Okay, so I want to access Arduino GPIO pins via Android. My plan is to access them via a serial connection using an MCP2200. I can read / write to the serial port on Android, which can then interact with the Arduino.

The problem is I also want to be able to plug in the phone and have it charging while still being able to access the Arduino. I came up with this, but am pretty new to the electronics side of things and want to avoid blowing things up. Will this do what I want?

It's essentially two USB ports. One goes to the charger, the other to the phone. The Arduino and MCP2200 sit in the middle.

image

  • Sign in to reply
  • Cancel

Top Replies

  • wolfgangfriedrich
    wolfgangfriedrich over 1 year ago +2
    Short answer is: No this will not work in the current form. Long answer: The basics: Connect all GND pins on both USB connectors, Arduino+ VSS and a schematic GND symbol Connect all VBUS on both…
  • shabaz
    shabaz over 1 year ago +2
    Hi, I agree with everything Wolfgang mentioned. If you want to make life easier, it is possible for a few $ to obtain a ready-made USB OTG cable with extra port for charging. It will contain the electronics…
  • wolfgangfriedrich
    wolfgangfriedrich over 1 year ago in reply to mjones517 +2
    I agree with everything shabaz mentioned. But if you want to go the fun route and design your own solution,here we go. Even as a USB device you need the 12 MHz crystal. The chip needs some sort of…
Parents
  • wolfgangfriedrich
    0 wolfgangfriedrich over 1 year ago

    Short answer is: No this will not work in the current form.

    Long answer:

    The basics:

    Connect all GND pins on both USB connectors, Arduino+ VSS and a schematic GND symbol

    Connect all VBUS on both connectors + all pins that need +5V.

    Connect all SHELL on both connectors together.

    U2: read the whole datasheet, OSC1,2 need a 12 MHz crystal with load capacitors. Rst needs a resistor to vbus, capacitor to gnd. Add 100nF capacitors to all power pins.

    Now it gets complicated. If you connect CC1,2 on both USB connectors and the charger and Android speak USB PD, VBUS could be up to 20V and blow everything up. To avoid that you add 2 x 5.1 KOhm resistors to GND on 5he charger CC1,2 pins. This limits the charger to 5V, max 3A.

    I am not sure what you want to achieve with the diodes+ fuse.

    Did you make sure the Android device can be a USB host?

    Hint: turn U1 and U2 90deg CCW. Schematics are much easier to read when symbol pins are left and right. Add netnames to all signals, it helps a lot during layout.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mjones517
    0 mjones517 over 1 year ago in reply to wolfgangfriedrich

    First off, thank you for replying!

    A few clarifying questions.

    I am using none of the USB host features of the MCP2200. I'm only using the UART capability. I want to send serial commands, which I can then use to control the Arduino GPIO.

    If I could use the MCP2200 as a USB device I wouldn't need the Arduino. There's GPIO on the chip.

    So since I'm not using OSC1/2, do I still need the crystal?

    Also... The Schokkey diodes and fuse are to try and prevent the power from the battery from back flowing into the charger.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • wolfgangfriedrich
    0 wolfgangfriedrich over 1 year ago in reply to mjones517

    I agree with everything shabaz mentioned. 

    But if you want to go the fun route and design your own solution,here we go.

    Even as a USB device you need the 12 MHz crystal. The chip needs some sort of timing reference.

    The diodes are not needed,just think what would happen if you plug the charger straight into the phone. Thinking

    Ask away, we are here to help. 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • wolfgangfriedrich
    0 wolfgangfriedrich over 1 year ago in reply to mjones517

    I agree with everything shabaz mentioned. 

    But if you want to go the fun route and design your own solution,here we go.

    Even as a USB device you need the 12 MHz crystal. The chip needs some sort of timing reference.

    The diodes are not needed,just think what would happen if you plug the charger straight into the phone. Thinking

    Ask away, we are here to help.