Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum What do you think of Arduino Pro and which kit would you like to try out?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 412 subscribers
  • Views 2188 views
  • Users 0 members are here
  • rapid prototyping
  • arduino pro
  • prototyping with arduino
  • arduino
  • application kit
Related

What do you think of Arduino Pro and which kit would you like to try out?

vijeth_ds
vijeth_ds over 1 year ago

Arduino have a line of products aimed at industry with the 'Pro' line, from what you've seen of these so far (and let us know if you haven't) what are you interested in:

If you want to read more about Arduino Pro and Rapid Prototyping, check out the tech spotlight: Rapid Prototyping with Arduino®︎ Pro Application Kits 

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 1 year ago in reply to cstanton +4
    This is the render in the user docs, I thought it must be simplified, surely they would have some screws holding the boards together: However, no screws are visible in this photo from a video online…
  • shabaz
    shabaz over 1 year ago in reply to michaelkellett +2
    Just been peeking at the schematics PDF for one of the control boards (it has the microcontroller board plugged onto it). I don't understand why they would rely on tiny 0.4mm pitch connectors for the…
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to cstanton +2
    cstanton said: Raspberry Pi Compute Module does that too (quote is shabaz text) The compute module provides a combination of (SMD or edge) connector + mounting holes, that allow a firm connection. I…
Parents
  • michaelkellett
    michaelkellett over 1 year ago

    Not interested in any of them, Arduino as a beginners'  learning tool was great.

    Arduino as a cheap simple part for rapid prototyping - good.

    Arduino as an industrial product - non starter.

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 1 year ago in reply to michaelkellett

    Just been peeking at the schematics PDF for one of the control boards (it has the microcontroller board plugged onto it).

    I don't understand why they would rely on tiny 0.4mm pitch connectors for the heart of it (connections between the microcontroller board and the rest of it, i.e. quite a critical connection!) for what's supposed to be presumably reliable/industrial.  Raspberry Pi Compute Module does that too, for zero useful reason.

    Also, there's no isolation on the serial interfaces (I didn't check the other interfaces), but would have assumed that isolation on the serial connections at least could have been useful given they don't know the precise situation customers will subject them to.

    Also, on the one hand there's the suggestion of rapid prototyping, but on the other hand, it's really clear from their online store that they actually suggest it for real deployments. Pricing is unusual too; who wouldn't rather pay several times that for reliability in a real deployment. But for prototyping, it is overpriced for the kits, since no one kit (bundle) is likely to contain everything, nor be fully used, so the customer would need several of them.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 1 year ago in reply to shabaz
    shabaz said:
    I don't understand why they would rely on tiny 0.4mm pitch connectors for the heart of it (connections between the microcontroller board and the rest of it, i.e. quite a critical connection!) for what's supposed to be presumably reliable/industrial.  Raspberry Pi Compute Module does that too, for zero useful reason.

    Could it be an application in certain environments/countries that for whatever reason have that as their requirements or what's available to them?

    I wonder sometimes if it's a matter of different locations' standards or expectations in how they design.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to cstanton
    cstanton said:
    Raspberry Pi Compute Module does that too

    (quote is shabaz text)
    The compute module provides a combination of (SMD or edge) connector + mounting holes, that allow a firm connection. I think that that one is fit for use in industry. Beyond prototyping.

    The IO kit and case are flagged as "for prototyping". Those are more fit when designing software while the final hardware isn't available yet - or when developers don't have access to the final product that embeds the module.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to cstanton
    cstanton said:
    Raspberry Pi Compute Module does that too

    (quote is shabaz text)
    The compute module provides a combination of (SMD or edge) connector + mounting holes, that allow a firm connection. I think that that one is fit for use in industry. Beyond prototyping.

    The IO kit and case are flagged as "for prototyping". Those are more fit when designing software while the final hardware isn't available yet - or when developers don't have access to the final product that embeds the module.