Arduino Forum X-BEE module
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
  • Replies 5 replies
  • Subscribers 394 subscribers
  • Views 521 views
  • Users 0 members are here
  • arduino:
  • arduino rf
  • diy
  • arduino
Related

X-BEE module

Former Member
Former Member over 9 years ago

Hello,

 

I want to use the x-bee  for wireless serial comm. between two arduinos. How do i configure the X-bee modules.

Also, what are the possible uses of the X-bee. I am a beginner and do not have enough experience with wireless comm. How does the X-Bee work??

 

if i configure the X bee modules for just wireless serial comm, will i be able to send data wirelessly to the other device. will it work just like it would have worked, if the system was wired?.

 

 

reply would be greatly appreciated.

Thank you.

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 9 years ago +2
    Hi Anshuman, I do not know if it will be of help but Jeremy Blum in his great book "Exploring Arduino" ISBN: 978-1-118-54936-0 devotes the entire chapter 11 to Wireless Communication with X-Bee Radios…
  • shabaz
    shabaz over 9 years ago +1
    We had this question about a week ago. The answer is no, they won't work the same. You need to check the datasheets for the various xbee models, they are all different. But, in general, if there is no…
  • tonyboubady
    tonyboubady over 9 years ago +1
    Get this 2.5GHz wireless transceiver called nrf24l01, it's inexpensive, easy to use to start with wireless communication, loads of tutorials on web, you can connect 2 microcontrollers wirelessly which…
Parents
  • shabaz
    shabaz over 9 years ago

    We had this question about a week ago.

    The answer is no, they won't work the same. You need to check the datasheets for the various xbee models,

    they are all different.

    But, in general, if there is no packet verification and retransmission then you need to write code to do that.

    And the chances are you need to send data in certain packet sizes unless you've got yourself into a UART type

    mode - and even then you might need to verify bytes yourself and retransmit if needed.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 9 years ago

    We had this question about a week ago.

    The answer is no, they won't work the same. You need to check the datasheets for the various xbee models,

    they are all different.

    But, in general, if there is no packet verification and retransmission then you need to write code to do that.

    And the chances are you need to send data in certain packet sizes unless you've got yourself into a UART type

    mode - and even then you might need to verify bytes yourself and retransmit if needed.