Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Traveling X Z for Raspberry Pi Camera Module 3 via arduino mega 2560
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 25 replies
  • Subscribers 411 subscribers
  • Views 2637 views
  • Users 0 members are here
Related

Traveling X Z for Raspberry Pi Camera Module 3 via arduino mega 2560

coincoin_2026
coincoin_2026 8 months ago

Hello everyone,

I want to slide a Raspberry Pi Camera Module 3 along the X-axis, then the Z-axis, to center it on the target subject for a time-lapse.

To do this, I have two CH-SM1545-M3xP0.5 micro motors (2-phase, 4-wire bipolar – 12V – with a threaded shaft travel of 80mm), and each will be controlled by its own A4988 motor controller. Selecting or powering on one of the two motors will be done with a KCD3 ON-OFF-ON SPDT 3-position toggle switch. Depending on the switch position (right or left), the target motor will be powered, while the other will be off. One of the powered motors will be controlled by a potentiometer.

Here is the electrical diagram for a single motor and its Arduino code. This works well with IR boundary sensors.

image

image

I have several questions about the electrical schematic.

I don't want to replicate my schematic for each motor. I'll end up with two 12V power supplies and two potentiometers for positioning the X-axis motor on the X-axis and the same for the Z-axis.
Can I power both A4988s with 12V via a third A4988?
Or should I place the toggle switch between the third A4988 and the other two, or is it possible to connect it directly to the Arduino Mega 2560?

Thank you for your time and ideas. I have little experience and am very curious.

/* 
Arduino Mega + A4988
Capteurs (IR en U) + potentiomètre contrôle distance et direction après recul
 
--- Diagramme d’état : Moteur + Potar + Capteurs ---
 
[START / Moteur immobile]
         |
         | Potar bougé → au-delà zone morte
         v
[Déplacement par potar]
         |
         | Capteur déclenché (IR)
         v
[Recul 1 cm en micro-pas]
         |
         | Recul terminé
         v
[Moteur en PAUSE après recul]
         |
         | Potar manipulé par l'utilisateur (delta > zone morte)
         v
[Reprise contrôle par potar]
         |
         +--> [Déplacement par potar]
 
*/
 
// Moteur PIN
const int MOTOR_DIR_PIN = 2;
const int MOTOR_STEP_PIN = 3;
const int MOTOR_ENABLE_PIN = 6;
 
// EndStop PIN signal
const int ENDSTOP_IR0 = 7;
const int ENDSTOP_IR1 = 11;
 
// EndStop MSx PIN
const int MS1_PIN = 8;
const int MS2_PIN = 9;
const int MS3_PIN = 10;
 
// Potentiomètre PIN Signal
const int POT_PIN = A0;
 
// Paramètres moteur
const int Nb_Recul = 200;        // 1cm en full-step=400pas --- 0.5cm en full-step=200pas
const int microStepFactor = 16;   // micro-pas pour recul
 
/* 
Le moteur avance d’un pas à chaque impulsion STEP.
La vitesse du moteur dépend uniquement du temps entre deux impulsions.
motorDelayMax est grand, plus le mouvement minimal est lent et précis.
Plus motorDelayMin est petit, plus le moteur va vite.
*/
const int motorDelayMax = 1500;   // microsecondes max STEP µs (lent)  1500 ≈ 1 mm/s
const int motorDelayMin = 400;    // microsecondes min STEP µs (rapide) 400 ≈ 3,9 mm/s
 
/* 
La zone morte (deadZone) est un intervalle central autour de la valeur neutre du potar où aucun mouvement du moteur n’est déclenché.
Exemple : const int deadZone = 50;
Si le potentiomètre est entre -50 et +50 autour du centre, le moteur reste immobile.
*/
const int deadZone = 200;          // zone morte du potar
 
const int accelStep = 1;          // incrément de lissage pour acceleration 2  4
 
bool reculEffectue = false;       // vrai après recul
bool pauseAfterRecul = false;     // moteur en pause après recul
int potRef = 0;                   // valeur de référence du potar après recul
int ir0LastState = 0;
int ir1LastState = 0;
 
 
int currentDelay = motorDelayMax;
bool potInverted = false;         // true = inverser la direction du potar
 
// Fonction STEP simple
void stepMotor(int delayMicro) {
  digitalWrite(MOTOR_STEP_PIN, HIGH);
  delayMicroseconds(delayMicro);
  digitalWrite(MOTOR_STEP_PIN, LOW);
  delayMicroseconds(delayMicro);
}
 
void setup() {
  pinMode(MOTOR_DIR_PIN, OUTPUT);
  pinMode(MOTOR_STEP_PIN, OUTPUT);
  pinMode(MOTOR_ENABLE_PIN, OUTPUT);
 
  // pinMode(ENDSTOP_MECA, INPUT_PULLUP);
  pinMode(ENDSTOP_IR0, INPUT);
  pinMode(ENDSTOP_IR1, INPUT);
 
  pinMode(MS1_PIN, OUTPUT);
  pinMode(MS2_PIN, OUTPUT);
  pinMode(MS3_PIN, OUTPUT);
 
  // Micro-pas 1/16 pour recul
  digitalWrite(MS1_PIN, HIGH);
  digitalWrite(MS2_PIN, HIGH);
  digitalWrite(MS3_PIN, HIGH);
  digitalWrite(MOTOR_ENABLE_PIN, LOW);
 
  delay(100); // stabilisation capteurs
  ir0LastState = digitalRead(ENDSTOP_IR0);
  ir1LastState = digitalRead(ENDSTOP_IR1);
}
 
void loop() {
  // ===== Lecture potar =====
  int potValue = analogRead(POT_PIN) - 512;
  int potAbs = abs(potValue);
 
  // Détermination direction potar avec inversion si activé
  bool direction = potInverted ? (potValue < 0) : (potValue > 0);
 
  // ===== Lecture capteurs =====
  int ir0State = digitalRead(ENDSTOP_IR0);
  int ir1State = digitalRead(ENDSTOP_IR1);
 
  bool ir0Triggered  = (ir0State == HIGH && ir0LastState == LOW);
  bool ir1Triggered  = (ir1State == HIGH && ir1LastState == LOW);
 
  // ===== Recul 1 cm si capteur déclenché =====
  if(!reculEffectue && (ir0Triggered || ir1Triggered)){
    delay(50);
 
    // Micro-pas pour recul
    digitalWrite(MS1_PIN, HIGH);
    digitalWrite(MS2_PIN, HIGH);
    digitalWrite(MS3_PIN, HIGH);
    digitalWrite(MOTOR_DIR_PIN, !direction); // reculer dans sens opposé au potar
    for(int i=0; i<Nb_Recul*microStepFactor; i++){
      stepMotor(motorDelayMin);
    }
 
    // Recul terminé → moteur en pause
    reculEffectue = true;
    pauseAfterRecul = true;
    potRef = potValue; // mémoriser la valeur du potar après recul
 
    // Mise à jour états capteurs
    ir0LastState = digitalRead(ENDSTOP_IR0);
    ir1LastState = digitalRead(ENDSTOP_IR1);
 
    return; // ne rien faire d'autre
  }
 
  // ===== Vérification pause après recul =====
  if(pauseAfterRecul){
    int deltaPot = abs(potValue - potRef);
    if(deltaPot > deadZone){
      // l'utilisateur a bougé le potar → reprise
      pauseAfterRecul = false;
    } else {
      return; // moteur reste en pause
    }
  }
 
  // ===== STEP proportionnel au potar avec acceleration =====
  if(potAbs >= deadZone){
    // Micro-pas 1/16 pour recul
    digitalWrite(MS1_PIN, HIGH);
    digitalWrite(MS2_PIN, HIGH);
    digitalWrite(MS3_PIN, HIGH);
    /* 
    // Passer en full-step pour potar
    digitalWrite(MS1_PIN, LOW);
    digitalWrite(MS2_PIN, LOW);
    digitalWrite(MS3_PIN, LOW); 
    */
    digitalWrite(MOTOR_DIR_PIN, direction);
 
    // Calcul vitesse cible selon potar
    int targetDelay = map(potAbs, deadZone, 512, motorDelayMax, motorDelayMin);
    targetDelay = constrain(targetDelay, motorDelayMin, motorDelayMax);
 
    // Lissage acceleration/déceleration
    if(currentDelay < targetDelay)
      currentDelay += accelStep;
    else if(currentDelay > targetDelay)
      currentDelay -= accelStep;
 
    currentDelay = constrain(currentDelay, motorDelayMin, motorDelayMax);
 
    stepMotor(currentDelay);
 
    // Autoriser un nouveau recul si le potar est utilisé après recul
    if(reculEffectue){
      reculEffectue = false;
    }
  }
 
  // Mise à jour derniers états des capteurs
  ir0LastState = ir0State;
  ir1LastState = ir1State;
}

  • Sign in to reply
  • Cancel

Top Replies

  • coincoin_2026
    coincoin_2026 8 months ago in reply to coincoin_2026 +1
    For the moment, I'm focusing on powering the two A4988s in parallel. I'm using two linear micro stepper motors: CH-SM1545-M3xP0.5 - 2 phases - 4 bipolar wires - 12V. In my first lab setup (see first…
  • beacon_dave
    beacon_dave 8 months ago in reply to Jan Cumps +1
    There may be gearing involved which could prevent back-driving under gravity.
  • Jan Cumps
    Jan Cumps 8 months ago in reply to coincoin_2026 +1
    coincoin_2026 said: CH-SM1545-M3xP0.5 I used a similar motor , with the same driver IC. They are good https://youtu.be/r3zlFKSM6s8 https://youtu.be/HuXfmYXk8QY
Parents
  • dougw
    dougw 8 months ago

    The Mega has enough pins to connect both motor controllers at the same time. The switch can tell the Mega which motor to move with the pot.

    Both motor controllers can likely use the same power supply, just connect both in parallel. If the power supply can't supply enough power, you may need to use the motor controller enable pins to disable the controller that is not in use.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • coincoin_2026
    coincoin_2026 8 months ago in reply to dougw

    Thank you for your reply.
    Here is the wiring diagram for two A4988 motor controllers.

    However, I'm not sure about the parallel connections for the 12V supply between VMOT and the 3-pin toggle switch.image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps 8 months ago in reply to coincoin_2026

    That toggle switch is indeed strange. You are expected to always have the 12V connected to both boards. And use the software to send commands to motor 1 or 2. If you remove the 12V from a controller, it will not be able to hold the motor at its current position (it can't "keep its hold torque")

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps 8 months ago in reply to coincoin_2026

    That toggle switch is indeed strange. You are expected to always have the 12V connected to both boards. And use the software to send commands to motor 1 or 2. If you remove the 12V from a controller, it will not be able to hold the motor at its current position (it can't "keep its hold torque")

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave 8 months ago in reply to coincoin_2026

    As Doug points out above, you could achieve similar in software by using the Enable pins that are already wired to the Arduino. The switch then becomes a logic level input to the Arduino instead of a power switch to the controllers.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • coincoin_2026
    coincoin_2026 8 months ago in reply to coincoin_2026

    To select the motor, both drivers must be kept permanently powered (switching between them to select one or the other is not recommended).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave 8 months ago in reply to coincoin_2026

    You might want to consider powering your driver. You appear to have disconnected VDD and GND.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps 8 months ago in reply to beacon_dave

    there is a caveat with using enable: if the motor has to stay fixed in position, you need to have the enable on. Without the enable asserted, the driver puts the motor in "free" mode, where it has no breaking/keep-in-place power.

    Everything can be done in software, but EN may not be the way to do it. Sending the pulses to the right controller would work. It requires that STEP and DIR are separate signals for both motors.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Jan Cumps
    Jan Cumps 8 months ago in reply to beacon_dave

    there is a caveat with using enable: if the motor has to stay fixed in position, you need to have the enable on. Without the enable asserted, the driver puts the motor in "free" mode, where it has no breaking/keep-in-place power.

    Everything can be done in software, but EN may not be the way to do it. Sending the pulses to the right controller would work. It requires that STEP and DIR are separate signals for both motors.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • beacon_dave
    beacon_dave 8 months ago in reply to Jan Cumps

    Indeed but removing power to VMOT will have a similar effect.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps 8 months ago in reply to beacon_dave

    indeed. This is what I'd propose:

    image

    There is no need for a switch. 12V and EN should be asserted at all times (or have a good reason why not),

    EN and STEP split in ENX / ENZ and STEPX STEPZ.

    Software can make motor X and motor Z make right movements by setting the relevant DIR pin in the right direction, then send the STEP pulses.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps 8 months ago in reply to beacon_dave

    yes, with the additional disadvantage that the time to wait after VMOT is applied, is larger than the time to wait after asserting EN.

    ... and VMOT has to top up that 100 µF cap each time.

    Reasonable (and traditional) option is to have both active as long as the design is operational.
    There are reasons to do it different, but I don't see any need for that in coincoin_2026 's requirements.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave 8 months ago in reply to Jan Cumps

    And the design spec stated:  Slight smile

    coincoin_2026 said:
    Selecting or powering on one of the two motors will be done with a KCD3 ON-OFF-ON SPDT 3-position toggle switch. Depending on the switch position (right or left), the target motor will be powered, while the other will be off.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps 8 months ago in reply to beacon_dave

    yes, I don't think it's a correct approach. It's not a requirement, it's a (odd) implementation decision.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave 8 months ago in reply to Jan Cumps

    There may be gearing involved which could prevent back-driving under gravity.