Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Anyone Have stability issues with Arduino Uno Q?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 18 replies
  • Subscribers 411 subscribers
  • Views 1448 views
  • Users 0 members are here
  • On the line design challenge
  • arduino uno q
  • arduino
Related

Anyone Have stability issues with Arduino Uno Q?

SensoredHacker0
SensoredHacker0 5 months ago

So im at my PC typing away. The Uno Q ran my code on the first try on the first day i got it, a couple days ago.
made some more tests, for 2 days everything was working great. Then, without warning, did not move it, or touch it, it stopped.
ok fine I guess. Then I tried to upload new test code. it compiles, and claims to have been uploaded. but the code doesnt work. 


The hardware which was attached, when it failed:
a Max33041E shield, and the Ethernet R3 shield. these had been working for a couple days straight. 

Not like the code is buggy, but like it doesn't even init the serial print lines. 
bash my head on the wall for a while. 
Press Reset. nothing. Un plug it, wait, re insert usb power.
$dmesg shows it, loading without issue.  

Pull the shields off, load blink. same thing, it compiles, and claims to upload, but the code never runs. 

I haven't reinstalled the boot-loader, by the time I thought to try that, I'd already gone to bed. 
But I've never had such random problems before. Ive got arduino running in projects that have run for 6 years straight not problem.

besides reloading the bootloader and one have some ideas?


Are there stability issues with the Arduino Uno Q I should know about?

Perhaps the most frustrating thing was that the LED matrix was making little hearts and arduino logos the whole time. 
meanwhile blink wont run. 

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz 5 months ago in reply to ralphjy +4
    I'm glad you guys are investigating the Q and working through the issues. It will help everyone. However, got to strongly disagree with this: The Q can't really be expected to be compared reliability…
  • ralphjy
    ralphjy 5 months ago +3
    The Q can't really be expected to be compared reliability/stability wise with previous Arduinos. With the new hybird MPU/MCU structure it is going to have a lot more issues than the MCU only boards. I…
  • ralphjy
    ralphjy 5 months ago in reply to shabaz +2
    I agree with your comments, but just to clarify what I meant - the Q has much more complexity and many more points of failure, both in hardware and software. I do think the current implementation is faulty…
Parents
  • shabaz
    shabaz 5 months ago

    That's concerning. Q has so much potential, but it's currently let down because of (it feels to me) lack of focus by Arduino. If it's going to stop starting up correctly after some power cycles, then it just won't get used, people will switch to other control boards. They have to take this seriously and eliminate such flakiness from the software/OS build or hardware, this to me is a showstopper, otherwise no-one can trust using it. I bought a Q to try it out, but will wait till it's more mature (hopefully). Also, a few of the other Arduino boards have at least perceived problems, since Mbed is EOL very shortly, and I wonder how long till any replacement Arduino libraries will be reliable. Think Arduino needs to have better messaging at a minimum, so users are not in the dark.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • BigG
    BigG 5 months ago in reply to shabaz

    Arduino has switched to using Zephyr RTOS: https://github.com/arduino/ArduinoCore-zephyr

    Still a long way to go to get to version 1 - they're at version 0.55.

    My guess is that it'll go version 1 once the next Zephyr LTS version is released next year.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz 5 months ago in reply to BigG

    I hope they hurry up. That's a long time to be unsure if things will be stable and if the API or subtle behavior will change.

    Sad to say that it appears right now for an amount of networking capability, one might want to simply walk away and consider non-Arduino boards, unless they pull their socks up.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz 5 months ago in reply to BigG

    I hope they hurry up. That's a long time to be unsure if things will be stable and if the API or subtle behavior will change.

    Sad to say that it appears right now for an amount of networking capability, one might want to simply walk away and consider non-Arduino boards, unless they pull their socks up.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • BigG
    BigG 5 months ago in reply to shabaz

    I think by default you still use MBed. You need to manually switch to the Zephyr option. Personally, having persevered with getting to know Zephyr RTOS, I find it really good.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • ralphjy
    ralphjy 5 months ago in reply to BigG

    If you are using the Q, the default is using Zephyr - both in AppLab and the standalone Arduino IDE.  Creates problems with legacy hardware because some (many?) third party libraries are not updated.  I ran into problems with the Arducam libraries.  Right now the only option is to port it yourself (a handful of class definition changes).  Hope the manufacturers will update their libraries to Zephyr soon.

    The standalone IDE does work with the Q, but I wouldn't recommend it.  Not sure what the real use case is.  I tried it because it is more familiar to me and I hoped to reuse code, but I don't think that Arduino is really going to support using software external to AppLab for the Q.  Have not investigated if it is possible to remove AppLab to get back the system resources.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • BigG
    BigG 5 months ago in reply to ralphjy

    Ah right, I did not know that. Agree, many of the old libraries will simply do not work. It's a case of rethinking our old ways when doing things with Zephyr. Info is there. It needs understanding. That's tricky without tutorials.

    docs.zephyrproject.org/.../README.html