Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum The Grande Arduino
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 29 replies
  • Subscribers 411 subscribers
  • Views 1268 views
  • Users 0 members are here
  • VENTUNO Q
  • arduino
  • arduino ventuno q
Related

The Grande Arduino

cstanton
cstanton 1 month ago

Arduino VENTUNO Q

Arduino have been kind to us today, I have the good fortune of being sent an Arduino VENTUNO Q ahead of our VENTUNO Q RoadTest (which is still open for applications until the 9th of October).

My initial impression's that it's a bit smaller than expected, but like all Arduino products it is well built.

We have plans to explore the functionality of this new bit of kit on the element14 Community alongside those writing a review, so you won't be alone in your explorations when you're selected Slight smile

At present we're exploring what cameras we can connect up to it, support is still in development from Arduino, but will be forthcoming. 

If you have any questions, I'll see if I can answer them, but we do have a rather comprehensive FAQ with questions fielded by Arduino engineers here:  ARDUINO VENTUNO Q  

  • Sign in to reply
  • Cancel

Top Replies

  • ralphjy
    ralphjy 1 month ago in reply to geralds +3
    I was more complaining about the use of the space and the fact that once you put a shield on it is not visible.
  • cstanton
    cstanton 1 month ago in reply to dang74 +2
    dang74 said: When you're dealing with a problem it can feel like you are all alone, so I applaud this. I've explored this idea in a few different ways, each RoadTest always has an 'escalation contact…
  • geralds
    geralds 1 month ago +2
    Hi Christopher cstanton , I pre-ordered the Ventuno Q from Arduino in mid-August, and it arrived today. Visually, it’s a great-looking piece of kit. Its size matches the Eurocard standard (160x100mm…
Parents
  • embeddedguy
    embeddedguy 1 month ago

    Nice looking board. Glad to see the that the board also comes with power supply and usbc cable. 

    Yes, I agree with your impression that it is bit smaller than expected. Cause I found the Uno Q also smaller than expected. Also, the PCB thickness is very low. I got nRF54-dk with the package and it was thicker than Uno-Q. It was surprising that a board with processor is thinner than a board with controller. Smiley

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton 1 month ago in reply to embeddedguy
    embeddedguy said:
    Glad to see the that the board also comes with power supply and usbc cable. 

    It does when you buy it, at the moment there's a special offer where you effectively get them for free when ordered together.

    embeddedguy said:
    Cause I found the Uno Q also smaller than expected

    They did a great job at keeping it to the "Arduino UNO" layout and size, do you find it produces a lot of heat under effort though?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • embeddedguy
    embeddedguy 1 month ago in reply to cstanton
    cstanton said:
    do you find it produces a lot of heat under effort though?

    Nope. The Uno Q does not heat that much. And I do not think that there is a need for any kind of heat sink or fan. I have not run some computer vision model yet. But still I think it is very good in that case. 

    cstanton said:
    They did a great job at keeping it to the "Arduino UNO" layout and size

    Yes that is impressive. Such a small PCB. I think they have inner layers as well but they have kept the low thickness. That is impressive. 

    Only the downside for now that I see is that some of the standard interfaces are missing compared to RPI. i.e. USB, MIPI, HDMI, etc. 

    But that is also fine. There will be soon some HaTs that can do that. !

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • embeddedguy
    embeddedguy 1 month ago in reply to cstanton
    cstanton said:
    do you find it produces a lot of heat under effort though?

    Nope. The Uno Q does not heat that much. And I do not think that there is a need for any kind of heat sink or fan. I have not run some computer vision model yet. But still I think it is very good in that case. 

    cstanton said:
    They did a great job at keeping it to the "Arduino UNO" layout and size

    Yes that is impressive. Such a small PCB. I think they have inner layers as well but they have kept the low thickness. That is impressive. 

    Only the downside for now that I see is that some of the standard interfaces are missing compared to RPI. i.e. USB, MIPI, HDMI, etc. 

    But that is also fine. There will be soon some HaTs that can do that. !