Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum The Grande Arduino
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 29 replies
  • Subscribers 411 subscribers
  • Views 1278 views
  • Users 0 members are here
  • VENTUNO Q
  • arduino
  • arduino ventuno q
Related

The Grande Arduino

cstanton
cstanton 1 month ago

Arduino VENTUNO Q

Arduino have been kind to us today, I have the good fortune of being sent an Arduino VENTUNO Q ahead of our VENTUNO Q RoadTest (which is still open for applications until the 9th of October).

My initial impression's that it's a bit smaller than expected, but like all Arduino products it is well built.

We have plans to explore the functionality of this new bit of kit on the element14 Community alongside those writing a review, so you won't be alone in your explorations when you're selected Slight smile

At present we're exploring what cameras we can connect up to it, support is still in development from Arduino, but will be forthcoming. 

If you have any questions, I'll see if I can answer them, but we do have a rather comprehensive FAQ with questions fielded by Arduino engineers here:  ARDUINO VENTUNO Q  

  • Sign in to reply
  • Cancel

Top Replies

  • ralphjy
    ralphjy 1 month ago in reply to geralds +3
    I was more complaining about the use of the space and the fact that once you put a shield on it is not visible.
  • cstanton
    cstanton 1 month ago in reply to dang74 +2
    dang74 said: When you're dealing with a problem it can feel like you are all alone, so I applaud this. I've explored this idea in a few different ways, each RoadTest always has an 'escalation contact…
  • geralds
    geralds 1 month ago +2
    Hi Christopher cstanton , I pre-ordered the Ventuno Q from Arduino in mid-August, and it arrived today. Visually, it’s a great-looking piece of kit. Its size matches the Eurocard standard (160x100mm…
Parents
  • geralds
    geralds 1 month ago

    Hi Christopher  cstanton ,

    I pre-ordered the Ventuno Q from Arduino in mid-August, and it arrived today.
    Visually, it’s a great-looking piece of kit.
    Its size matches the Eurocard standard (160x100mm), with a height of 50mm including the supplied standoffs.

    Unboxing:
    All parts are well packaged.

    VentunoQ-Box

    First impression: the PCB is neatly assembled, and the components are securely mounted.

    VentunoQ-top VentunoQ-bot VentunoQ-euro


    A small detail:
    You can mount a standoff above the LED matrix, behind the "User" button.
    You have to be careful here to orient the hex nut so that it doesn't push against adjacent components; otherwise, they could get torn off.

    VentunoQ-nut

    "Bughopper" module:
    Behind this standoff, there is a pin header for the Bughopper, in case you need to debug the Ventuno Q.

    VentunoQ-debug

    Audio module:
    Various modules can be attached to the underside; I bought the audio module. There is also currently a prototype board available for custom circuits.

    VentunoQ-aud

    VentunoQ-aud-plug

    Plugin careful such modules. Such modules you cannot connect on/off many times.

    Power supply:
    Similar to the RPi 5, it’s a 65W USB-C wall adapter.

    VentunoQ-supply

    Well then... That covers the unboxing.

    Then, I also have RPi compatible cameras and 7" displays; so, I'll see how I can connect them to the Arduino Ventuno Q.

    Now..., I'm as excited as a guitar string to see what "melodies" the Arduino Ventuno Q will play.

    I would be very happy to post my experiences with the Ventuno Q (I also have the Uno Q) here, or in a dedicated forum.

    Arduino App Lab

    Best Regards

    Gerald

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • ralphjy
    ralphjy 1 month ago in reply to geralds

    Nice looking board.  Not sure why Arduino likes that LED matrix so much.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • ralphjy
    ralphjy 1 month ago in reply to geralds

    Nice looking board.  Not sure why Arduino likes that LED matrix so much.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • geralds
    geralds 1 month ago in reply to ralphjy
    ralphjy said:
    Not sure why Arduino likes that LED matrix so much.

    I think this comes from Microchip, not as the first (I think), but also from the Intel 8048, 8049 controllers.
    Look for that, the PIC now the Atmel's as well as use this (LED-matrix).

    The ideas are saving numbers of port pins because small µC's haven't many pins.
    Multi usage the ports is a very old method.

    In this kind you can combine keyboards together with LEDs.

    The very old method was printing graphic images in the MSDOS aera using dot matrix printers. 
    -> Snoopy and Charlie Brown, the peanuts.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • ralphjy
    ralphjy 1 month ago in reply to geralds

    I was more complaining about the use of the space and the fact that once you put a shield on it is not visible.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • geralds
    geralds 1 month ago in reply to ralphjy

    yep. this is a good argument.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave 1 month ago in reply to ralphjy
    ralphjy said:
    once you put a shield on it is not visible

    I'm guessing they might argue that there is a Modulino LED Matrix for that Slight smile

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • ralphjy
    ralphjy 1 month ago in reply to beacon_dave

    Right, that’s where it should be.  It was probably an okay fit for the Uno R4 (although still has the shield issue).  I just don’t see why you would put something like that on a Ventuno Q.  I’ve found an 8x13 matrix isn’t that useful although it would be fun for kids.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave 1 month ago in reply to ralphjy

    I thought it might have been to improve on the single LED blinky experience you got with the UNO, to allow new users to do something a bit more visually appealing straight out of the box.

    If you look at the micro:bit, then quite often the first coding projects are to get something to display on the LED matrix before reaching for the breadboard. I find the single character scrolling text a bit painful though.

    However if that was the case, then I am surprised that they didn't include the LED matrix on the R4 Minima.

    I think something like a 128x64 OLED display would be more useful these days though. I guess if it was removable, then you could get the best of both worlds.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps 1 month ago in reply to beacon_dave
    beacon_dave said:
    I thought it might have been to improve on the single LED blinky experience you got with the UNO, to allow new users to do something a bit more visually appealing straight out of the box

    The single LED blinky is ingenious. It's clear to the newbie that they did something "real electronic".

    And it's easy to go from there and understand the few lines of blinky code.

    That is: if you don't use the Raspberry Pico blinky's recent version. That 's almost an antipattern on how to get someone started...
    They have a simpler version, but that doesn't work on pico-w ...