Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum The Grande Arduino
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 29 replies
  • Subscribers 411 subscribers
  • Views 1278 views
  • Users 0 members are here
  • VENTUNO Q
  • arduino
  • arduino ventuno q
Related

The Grande Arduino

cstanton
cstanton 1 month ago

Arduino VENTUNO Q

Arduino have been kind to us today, I have the good fortune of being sent an Arduino VENTUNO Q ahead of our VENTUNO Q RoadTest (which is still open for applications until the 9th of October).

My initial impression's that it's a bit smaller than expected, but like all Arduino products it is well built.

We have plans to explore the functionality of this new bit of kit on the element14 Community alongside those writing a review, so you won't be alone in your explorations when you're selected Slight smile

At present we're exploring what cameras we can connect up to it, support is still in development from Arduino, but will be forthcoming. 

If you have any questions, I'll see if I can answer them, but we do have a rather comprehensive FAQ with questions fielded by Arduino engineers here:  ARDUINO VENTUNO Q  

  • Sign in to reply
  • Cancel

Top Replies

  • ralphjy
    ralphjy 1 month ago in reply to geralds +3
    I was more complaining about the use of the space and the fact that once you put a shield on it is not visible.
  • cstanton
    cstanton 1 month ago in reply to dang74 +2
    dang74 said: When you're dealing with a problem it can feel like you are all alone, so I applaud this. I've explored this idea in a few different ways, each RoadTest always has an 'escalation contact…
  • geralds
    geralds 1 month ago +2
    Hi Christopher cstanton , I pre-ordered the Ventuno Q from Arduino in mid-August, and it arrived today. Visually, it’s a great-looking piece of kit. Its size matches the Eurocard standard (160x100mm…
Parents
  • geralds
    geralds 1 month ago

    Hi Christopher  cstanton ,

    I pre-ordered the Ventuno Q from Arduino in mid-August, and it arrived today.
    Visually, it’s a great-looking piece of kit.
    Its size matches the Eurocard standard (160x100mm), with a height of 50mm including the supplied standoffs.

    Unboxing:
    All parts are well packaged.

    VentunoQ-Box

    First impression: the PCB is neatly assembled, and the components are securely mounted.

    VentunoQ-top VentunoQ-bot VentunoQ-euro


    A small detail:
    You can mount a standoff above the LED matrix, behind the "User" button.
    You have to be careful here to orient the hex nut so that it doesn't push against adjacent components; otherwise, they could get torn off.

    VentunoQ-nut

    "Bughopper" module:
    Behind this standoff, there is a pin header for the Bughopper, in case you need to debug the Ventuno Q.

    VentunoQ-debug

    Audio module:
    Various modules can be attached to the underside; I bought the audio module. There is also currently a prototype board available for custom circuits.

    VentunoQ-aud

    VentunoQ-aud-plug

    Plugin careful such modules. Such modules you cannot connect on/off many times.

    Power supply:
    Similar to the RPi 5, it’s a 65W USB-C wall adapter.

    VentunoQ-supply

    Well then... That covers the unboxing.

    Then, I also have RPi compatible cameras and 7" displays; so, I'll see how I can connect them to the Arduino Ventuno Q.

    Now..., I'm as excited as a guitar string to see what "melodies" the Arduino Ventuno Q will play.

    I would be very happy to post my experiences with the Ventuno Q (I also have the Uno Q) here, or in a dedicated forum.

    Arduino App Lab

    Best Regards

    Gerald

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton 1 month ago in reply to geralds

     geralds do you want to write up a review for it since you already have it? We can add you to the RoadTesters list.

    maybe OwainM can send you a few accessories.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • cstanton
    cstanton 1 month ago in reply to geralds

     geralds do you want to write up a review for it since you already have it? We can add you to the RoadTesters list.

    maybe OwainM can send you a few accessories.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • geralds
    geralds 1 month ago in reply to cstanton

    Hi  cstanton 

    Yes, it would be an honor for me to write a review.
    Yes, the accessories would be a great help.

    Many thanks for that.

    Best Regards

    Gerald

    ---

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • geralds
    geralds 1 month ago in reply to cstanton

    Hi Christopher  cstanton 

    Hi  OwainM 

    First of all, thank you for the invitation to participate in the road test.
    I'll write more details in the PM.

    -> This is an important step for the testing process.
    As previously mentioned, I am using an RPi-compatible 7-inch QLED touch display: the Waveshare 7HP-CAPQLED.
    https://www.waveshare.com/wiki/7HP-CAPQLED#External_guides

    Since I didn't know whether the display would be detected, I had to perform this initial test—taking it "step by step," so to speak.

    Today, I powered up both the Ventuno Q and the display for the first time.

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image


    After switching on the Ventuno Q, the LED matrix displayed its animation. That marked a successful initial test.

    Next, I turned on the display (while keeping the Ventuno Q powered on); for about 30 to 40 seconds, it seemed like "nothing" was happening.

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    But in fact, something was going on:
    The Ventuno Q was scanning for connected hardware without any indication to the status-LEDs.
    It detected the display and immediately adjusted the parameters—both the display geometry and the touch panel settings.

    During those first few seconds... (see the video), I didn't realize the display was synchronizing with the computer; I toggled the power on and off a few times.
    I assumed nothing was installed on the Ventuno Q yet.

    But an Ubuntu operating system was already installed; suddenly, the fan sped up and the LED matrix turned off.
    That’s when I realized everything was actually fine.
    So, the initial startup turned out to be a simple process.

    I then tapped the "Power" button in the top-right corner of the display, a menu opened, and I shut the system down.
    Done—the initial startup, including the display and touch panel, worked perfectly right away.
    Hooray! The system is up and running.
    Yep, as I said, since I didn't have any information on this yet, I had to take this step first.
    Now I can move on to working with additional hardware and the software.

    I hope this proves useful to the other road testers when they start up their Ventuno Q systems for the first time.
    Because that could also affect what accessories they have.

    Best Regards

    Gerald

    ---