Arduino Forum Sensor
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
  • Replies 8 replies
  • Subscribers 393 subscribers
  • Views 651 views
  • Users 0 members are here
Related

Sensor

Former Member
Former Member over 9 years ago

I would like to ask if there are any sensors that I could use in detecting the level of powder in a case while reloading. The only thing I can find commercially only tell you when a case is empty or over full. I want to know if it has a level between those two.

1. the level I want

2. anything short of that level

3. anything above that level.

 

any advice would be great thanks

Keith

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 9 years ago +1
    Traditionally the most accurate linear position sensor is an LVDT (linear variable differential transducer) but they can be expensive. A linear potentiometer is a pretty good low-cost alternative. Maybe…
Parents
  • DAB
    DAB over 9 years ago

    I would use a pressure sensor to measure the weight of the container.

     

    Once you know the weight for an empty one, and then a full one, you can see about where you are with what is left.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • DAB
    DAB over 9 years ago

    I would use a pressure sensor to measure the weight of the container.

     

    Once you know the weight for an empty one, and then a full one, you can see about where you are with what is left.

     

    DAB