Arduino Forum Arduino paraffin oil / water dot matrix display
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
  • Replies 14 replies
  • Subscribers 400 subscribers
  • Views 1002 views
  • Users 0 members are here
  • display_unit
  • peristaltic_pump
  • tube
  • ardexpert
  • arduino
  • hose
Related

Arduino paraffin oil / water dot matrix display

hwhardsoft
hwhardsoft over 9 years ago

Hi,

 

I want to introduce this  demo project for the Maker Faire in Hannover last weekend. The project was inspired by the work of the artist Julius Popp. We are using a transparent hose, 2 peristaltic pumps and an Arduino Uno with motor shield (both mounted in an Arduino Din rail enclosure ) to build a simple display.

The pumps pressing a pattern of water and red paraffin oil in the hose. In the end a text will be visible. For the Maker Faire we've used 2 alternating texts "Maker" and "faire" (see the picture below).

 

Source code and additional infos are available on our website.

 

imageimage

imageimage

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 9 years ago +2
    Nice work. It shows that a few simple parts can be put together to make something that seems impossible.
  • clem57
    clem57 over 9 years ago +1
    Very ingenious use of physics and electronics!
  • gadget.iom
    gadget.iom over 9 years ago +1
    Awesome! The video didn't make what was happening particularly clear, but it comes up nicely on the white board. Did you get any video of it working at the faire?
Parents
  • hwhardsoft
    hwhardsoft over 9 years ago

    I've updated the pictures -  a new video comes soon.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to hwhardsoft

    Frankly now the text is more readable. How much complex was in this context to use a bit larger tubes (that means, I know, more liquid and probably a more powerful peristaltic pumps)?

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • hwhardsoft
    hwhardsoft over 9 years ago in reply to balearicdynamics

    I've tried 5mm diameter tubes before, but it works better with 3mm hose. If the inner diameter of the hose is too thick the forces of adhesion and cohesion are not strong enough to hold bubbles of the liquids together.... Perhaps this is possible with other liquids.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • hwhardsoft
    hwhardsoft over 9 years ago in reply to balearicdynamics

    I've tried 5mm diameter tubes before, but it works better with 3mm hose. If the inner diameter of the hose is too thick the forces of adhesion and cohesion are not strong enough to hold bubbles of the liquids together.... Perhaps this is possible with other liquids.