Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum 16*2 LCD getting weird characters
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 34 replies
  • Subscribers 425 subscribers
  • Views 13428 views
  • Users 0 members are here
  • lcd
  • arduino
Related

16*2 LCD getting weird characters

jrcs
jrcs over 10 years ago

Hi all.

 

This is my first post so I hope it is at the right place.

 

I'm working on a project whose objective is to control two ac loads (one ac fan, controlled by phase angle control and one ac motor controlled by a 5V relay) and output to an LCD the room temperature and the % of fan speed.

 

 

The code I wrote seem to work fine without the AC loads connected. I tested it for long periods of time (+12 hours) and everything is ok.

 

The problem is when I connect both (or just one) AC loads, I always end up with my LCD info corrupted like this:

 

image

 

https://1drv.ms/i/s!Ah12lhUG5VG8g9FOhR9Y0ccFTsq2Rg

 

Sometimes past 2 minutes, sometimes past 10 minutes... It's random but it always end up like this.

 

 

I'm guessing it's noise problems due to the loads switching TRIAC/Relay. The TRIAC its connected trough a optocoupler but the relay it's directly connected to the arduino.

 

 

First, I put the lcd.clear() function in my code to "rebuild" the info from time to time but it doesen't work 100% and it's not a "clean" solution for the pourpose.

 

 

The AC loads are connected to the grid but the arduino is powered from my computer's usb port. Already put an EMI filter into AC main input of my loads but no solution.

 

Is there a solution to this problem? Any help?

Sorry for my poor english but I'm a little bit rusty.

 

Regards

  • Sign in to reply
  • Cancel

Top Replies

  • niko.vicencio
    niko.vicencio over 9 years ago +3
    Hi I had the same problem, the lcd showed random characters when the electromechanical relay commutated. I solved this problem, changing the relay by a ssr (Solid state relay). I hope that my answer help…
  • WarrenW
    WarrenW over 10 years ago +2
    How are you driving the relay from the arduino? Direct off the micro or via a transistor? Does the relay have a snubber cap across the coil and a back emf diode? Does the arduino have a filter capacitor…
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +2
    Can you please provide a schematic of your setup and also a full picture (Cant see all your connections in the one provided. You can upload them right into this community post. I have done what your describing…
Parents
  • jrcs
    jrcs over 10 years ago

    Hi all.

    Thanks in advance for your help. I'll try to answer to all of you clearly but I know my english it's not very good (nor technical).

     

    mcb1 When I disconnect just the ac motor from the relay (and keep the relay coil connected and controlled by the Arduino) the noise disappears. Could it be the AC motor producing the spikes?? I added a snubber circuit just to be sure but didn't help.

     

    The lamp (is actually a AC Fan) is not the problem. It is controlled by phase angle control and being connected or not doesn't change the spikes.

     

    If I remove the 5v power to the relay coil I have no spikes... but the motor obviously doesn't turn on so...

     

    I've put a flyback diode directly into the relay coil aswell but didn't help.

     

     

    The zero crossing detector is just to trigger the triac and power the AC Fan (Ventilador).

    The AC motor connected to the relay is turned on for a few seconds (3 to 10 seconds) and off for 40 seconds regardless of zerocross detected or not... but I can try to change the program to only switch the relay when zerocross is detected.

     

     

    dougw the supply on the laptop's usb port can give 500mA and the usb charger can give 2A. I tried both ways and got the same result.

     

    A small resistor/inductor and a capacitor in the power supply wire ? In the whole system supply wire or just the relay supply wire?

    I'll try to learn how to feed the digital with the Schottky diode.

     

     

    Thank you all for your time.

    Regards.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 9 years ago in reply to jrcs

    Just filter the power to the low power circuit being affected by the noise (the LCD and arduino)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dougw
    dougw over 9 years ago in reply to jrcs

    Just filter the power to the low power circuit being affected by the noise (the LCD and arduino)