Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum 16*2 LCD getting weird characters
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 34 replies
  • Subscribers 425 subscribers
  • Views 13380 views
  • Users 0 members are here
  • lcd
  • arduino
Related

16*2 LCD getting weird characters

jrcs
jrcs over 10 years ago

Hi all.

 

This is my first post so I hope it is at the right place.

 

I'm working on a project whose objective is to control two ac loads (one ac fan, controlled by phase angle control and one ac motor controlled by a 5V relay) and output to an LCD the room temperature and the % of fan speed.

 

 

The code I wrote seem to work fine without the AC loads connected. I tested it for long periods of time (+12 hours) and everything is ok.

 

The problem is when I connect both (or just one) AC loads, I always end up with my LCD info corrupted like this:

 

image

 

https://1drv.ms/i/s!Ah12lhUG5VG8g9FOhR9Y0ccFTsq2Rg

 

Sometimes past 2 minutes, sometimes past 10 minutes... It's random but it always end up like this.

 

 

I'm guessing it's noise problems due to the loads switching TRIAC/Relay. The TRIAC its connected trough a optocoupler but the relay it's directly connected to the arduino.

 

 

First, I put the lcd.clear() function in my code to "rebuild" the info from time to time but it doesen't work 100% and it's not a "clean" solution for the pourpose.

 

 

The AC loads are connected to the grid but the arduino is powered from my computer's usb port. Already put an EMI filter into AC main input of my loads but no solution.

 

Is there a solution to this problem? Any help?

Sorry for my poor english but I'm a little bit rusty.

 

Regards

  • Sign in to reply
  • Cancel

Top Replies

  • niko.vicencio
    niko.vicencio over 9 years ago +3
    Hi I had the same problem, the lcd showed random characters when the electromechanical relay commutated. I solved this problem, changing the relay by a ssr (Solid state relay). I hope that my answer help…
  • WarrenW
    WarrenW over 10 years ago +2
    How are you driving the relay from the arduino? Direct off the micro or via a transistor? Does the relay have a snubber cap across the coil and a back emf diode? Does the arduino have a filter capacitor…
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +2
    Can you please provide a schematic of your setup and also a full picture (Cant see all your connections in the one provided. You can upload them right into this community post. I have done what your describing…
Parents
  • jrcs
    jrcs over 10 years ago

    Hi neilk

     

    I'm sorry I haven't made myself clear. The relay is a module driven by a transistor. A module like this: http://www.elecfreaks.com/store/images/BK_SRD.jpg

    You can see it in the photo of the system itself.

     

    The arduino is not directly driving the relay coil. I'm using the module. I'm sorry for my mistake.

     

    Regards

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • neilk
    neilk over 10 years ago in reply to jrcs

    Understood. However, is the module being powered from the same supply as the Arduino?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jrcs
    jrcs over 10 years ago in reply to neilk

    Yes. The module's VCC and GND are the same as the Arduino (laptop usb port or usb charger. I have tried with both solutions)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 10 years ago in reply to jrcs

    The simpliest way to verify which part is causing it is to eliminate one item at a time.

     

    You can remove the lamp, then the ventilator.

    I suspect that the mains side is not the issue, so move to the control side.

     

    I'd suggest removing the 5v power feed to the relay first as this is likely to cause a spike, which drops the volts and upsets the LCD.

    As you have said it's quite likely this is the cause.

     

    In order to provide isolation you could try feeding the power to the relay via a diode.

    Add a 470uF (preferably bigger) on the relay side of the diode.

    This will help keep the spikes away from the Arduino supply.

     

    The rule of thumb for filter caps is 1000uF per amp.

    Because these are spikes something around 10,000uF is going to help along with a 0.1uF cap as well.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • mcb1
    mcb1 over 10 years ago in reply to jrcs

    The simpliest way to verify which part is causing it is to eliminate one item at a time.

     

    You can remove the lamp, then the ventilator.

    I suspect that the mains side is not the issue, so move to the control side.

     

    I'd suggest removing the 5v power feed to the relay first as this is likely to cause a spike, which drops the volts and upsets the LCD.

    As you have said it's quite likely this is the cause.

     

    In order to provide isolation you could try feeding the power to the relay via a diode.

    Add a 470uF (preferably bigger) on the relay side of the diode.

    This will help keep the spikes away from the Arduino supply.

     

    The rule of thumb for filter caps is 1000uF per amp.

    Because these are spikes something around 10,000uF is going to help along with a 0.1uF cap as well.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • mcb1
    mcb1 over 10 years ago in reply to mcb1

    Just a thought.

    You appear to have a zero crossing detector.

    The purpose is to switch the load when it is at zero, which is fine.

     

    I don't suppose the relay output is being switched ON/OFF as it goes past the zero cross point.??

    In theory it should just switch ON when the zero point is detected and stay ON.

     

    The easist way to prove it is to short the pin to ground and recheck for switching noise.

     

     

    Mark