Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum 16*2 LCD getting weird characters
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 34 replies
  • Subscribers 425 subscribers
  • Views 13383 views
  • Users 0 members are here
  • lcd
  • arduino
Related

16*2 LCD getting weird characters

jrcs
jrcs over 10 years ago

Hi all.

 

This is my first post so I hope it is at the right place.

 

I'm working on a project whose objective is to control two ac loads (one ac fan, controlled by phase angle control and one ac motor controlled by a 5V relay) and output to an LCD the room temperature and the % of fan speed.

 

 

The code I wrote seem to work fine without the AC loads connected. I tested it for long periods of time (+12 hours) and everything is ok.

 

The problem is when I connect both (or just one) AC loads, I always end up with my LCD info corrupted like this:

 

image

 

https://1drv.ms/i/s!Ah12lhUG5VG8g9FOhR9Y0ccFTsq2Rg

 

Sometimes past 2 minutes, sometimes past 10 minutes... It's random but it always end up like this.

 

 

I'm guessing it's noise problems due to the loads switching TRIAC/Relay. The TRIAC its connected trough a optocoupler but the relay it's directly connected to the arduino.

 

 

First, I put the lcd.clear() function in my code to "rebuild" the info from time to time but it doesen't work 100% and it's not a "clean" solution for the pourpose.

 

 

The AC loads are connected to the grid but the arduino is powered from my computer's usb port. Already put an EMI filter into AC main input of my loads but no solution.

 

Is there a solution to this problem? Any help?

Sorry for my poor english but I'm a little bit rusty.

 

Regards

  • Sign in to reply
  • Cancel

Top Replies

  • niko.vicencio
    niko.vicencio over 9 years ago +3
    Hi I had the same problem, the lcd showed random characters when the electromechanical relay commutated. I solved this problem, changing the relay by a ssr (Solid state relay). I hope that my answer help…
  • WarrenW
    WarrenW over 10 years ago +2
    How are you driving the relay from the arduino? Direct off the micro or via a transistor? Does the relay have a snubber cap across the coil and a back emf diode? Does the arduino have a filter capacitor…
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +2
    Can you please provide a schematic of your setup and also a full picture (Cant see all your connections in the one provided. You can upload them right into this community post. I have done what your describing…
Parents
  • jrcs
    jrcs over 10 years ago

    Hi all,

     

    Thank you all for your time.

     

    I took a picture today of the system today. It's not very "clean" but I was really short on time to test it. You can see it here: https://1drv.ms/i/s!Ah12lhUG5VG8g9FU0eNo8CpDdW1WYQ  I'll try to post the schematic later today when I arrive home.

     

    I have done some measurements with a scope with a borrowed scope. The 5V supply is getting lots of spikes when I open or close the relay (more when I close it so I only took pictures of closing).

     

    This is what I measure: https://1drv.ms/i/s!Ah12lhUG5VG8g9FRBvXyADPi7U7WZQ

     

    Then I add 2x470uF capacitores to 5V: https://1drv.ms/i/s!Ah12lhUG5VG8g9FS6mhCWvuhGU6JZw

     

    Not very helpfull. So I was reading around and added a snubber in paralel with the motor to see if it gets any better: https://1drv.ms/i/s!Ah12lhUG5VG8g9FTdvyVX-heJbancA

     

    So, basically I think the problem is the coil on the relay that is giving me all this spikes.

     

     

    I measured the system with the phase angle control and I get some noise at low firing angles but it doesn't seem to be enough for the problem... the noise is very low.

     

     

    Thank you all in advance.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jrcs
    jrcs over 10 years ago

    Hi all,

     

    Thank you all for your time.

     

    I took a picture today of the system today. It's not very "clean" but I was really short on time to test it. You can see it here: https://1drv.ms/i/s!Ah12lhUG5VG8g9FU0eNo8CpDdW1WYQ  I'll try to post the schematic later today when I arrive home.

     

    I have done some measurements with a scope with a borrowed scope. The 5V supply is getting lots of spikes when I open or close the relay (more when I close it so I only took pictures of closing).

     

    This is what I measure: https://1drv.ms/i/s!Ah12lhUG5VG8g9FRBvXyADPi7U7WZQ

     

    Then I add 2x470uF capacitores to 5V: https://1drv.ms/i/s!Ah12lhUG5VG8g9FS6mhCWvuhGU6JZw

     

    Not very helpfull. So I was reading around and added a snubber in paralel with the motor to see if it gets any better: https://1drv.ms/i/s!Ah12lhUG5VG8g9FTdvyVX-heJbancA

     

    So, basically I think the problem is the coil on the relay that is giving me all this spikes.

     

     

    I measured the system with the phase angle control and I get some noise at low firing angles but it doesn't seem to be enough for the problem... the noise is very low.

     

     

    Thank you all in advance.