Arduino
  • Products
  • More
Arduino
Arduino Forum How o measure 4-20 mA Current
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 420 subscribers
  • Views 5610 views
  • Users 0 members are here
  • frontpage
Related

How o measure 4-20 mA Current

oksbwn
oksbwn over 10 years ago

I need to measure 4-20mA current output from some sensors. How can i do that ? Currently i use resistive drop to get the analog voltage and provide that to ADC of the controller. Are their any current input ADC ?

  • Sign in to reply
  • Cancel

Top Replies

  • kulky64
    kulky64 over 10 years ago +2
    That's basically how you do it. You can check various manufacturers reference designs, for example: Analog Devices: http://www.analog.com/en/design-center/reference-designs/hardware-reference-design/circuits…
  • uscdadnyc
    uscdadnyc over 10 years ago in reply to oksbwn +2
    Is the situation: (a) Measuring DC Current (at Currents mentioned) AS you would using a (temporary) Test Instrument? OR (b) Circuitry that you would build that attaches to the circuitry that you want to…
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +2
    4-20mA is a nice standard for instrumentation measurement and is used in industry extensively. the nice thing about it is it has automatic fault detections as zero = 4mA, any less than 4 means an error…
Parents
  • kulky64
    kulky64 over 10 years ago

    That's basically how you do it. You can check various manufacturers reference designs, for example:

     

    Analog Devices:

    http://www.analog.com/en/design-center/reference-designs/hardware-reference-design/circuits-from-the-lab/cn0336.html#rd-overview

    http://www.analog.com/en/design-center/evaluation-hardware-and-software/cu_eb_plc_demo_system.html

     

    Texas Instruments:

    Single Supply Analog Input Module Reference Design with 16-Bit, 8-Channel ADC for PLC - TIPD166 - TI Tool Folder

    Analog Input Module for Industrial Outputs and Temperature Sensors Reference Design - TIPD164 - TI Tool Folder

     

    Maxim:

    https://www.maximintegrated.com/en/products/interface/current-loop-products-4-20ma.html

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • kulky64
    kulky64 over 10 years ago

    That's basically how you do it. You can check various manufacturers reference designs, for example:

     

    Analog Devices:

    http://www.analog.com/en/design-center/reference-designs/hardware-reference-design/circuits-from-the-lab/cn0336.html#rd-overview

    http://www.analog.com/en/design-center/evaluation-hardware-and-software/cu_eb_plc_demo_system.html

     

    Texas Instruments:

    Single Supply Analog Input Module Reference Design with 16-Bit, 8-Channel ADC for PLC - TIPD166 - TI Tool Folder

    Analog Input Module for Industrial Outputs and Temperature Sensors Reference Design - TIPD164 - TI Tool Folder

     

    Maxim:

    https://www.maximintegrated.com/en/products/interface/current-loop-products-4-20ma.html

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • oksbwn
    oksbwn over 10 years ago in reply to kulky64

    Thanks..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • uscdadnyc
    uscdadnyc over 10 years ago in reply to oksbwn

    Is the situation: (a) Measuring DC Current (at Currents mentioned) AS you would using a (temporary) Test Instrument? OR (b) Circuitry that you would build that attaches to the circuitry that you want to monitor? IF (b) then the previously post Comments will do.

    However if the situation is (a) then consider a "Portapow Premium USB+DC Power Monitor (portapow.co.uk). I have one and it works great. Remember this is DC. The documentation is lousy, but I drew-up several diagrams that explains the various connections. Will try to post them here BUT I haven't

    gotten a Win10 Driver for the Scanner Portion of my Samsung SCX-4016scx MFP. WRT that I am attempting a "virtual" WinXP  w/i my Win10 PC. But that is Tangential to this discussion.

    USCDADNYC (NY NY USA)