Arduino
  • Products
  • More
Arduino
Arduino Forum How o measure 4-20 mA Current
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 420 subscribers
  • Views 5600 views
  • Users 0 members are here
  • frontpage
Related

How o measure 4-20 mA Current

oksbwn
oksbwn over 10 years ago

I need to measure 4-20mA current output from some sensors. How can i do that ? Currently i use resistive drop to get the analog voltage and provide that to ADC of the controller. Are their any current input ADC ?

  • Sign in to reply
  • Cancel

Top Replies

  • kulky64
    kulky64 over 10 years ago +2
    That's basically how you do it. You can check various manufacturers reference designs, for example: Analog Devices: http://www.analog.com/en/design-center/reference-designs/hardware-reference-design/circuits…
  • uscdadnyc
    uscdadnyc over 10 years ago in reply to oksbwn +2
    Is the situation: (a) Measuring DC Current (at Currents mentioned) AS you would using a (temporary) Test Instrument? OR (b) Circuitry that you would build that attaches to the circuitry that you want to…
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +2
    4-20mA is a nice standard for instrumentation measurement and is used in industry extensively. the nice thing about it is it has automatic fault detections as zero = 4mA, any less than 4 means an error…
  • kulky64
    kulky64 over 10 years ago

    That's basically how you do it. You can check various manufacturers reference designs, for example:

     

    Analog Devices:

    http://www.analog.com/en/design-center/reference-designs/hardware-reference-design/circuits-from-the-lab/cn0336.html#rd-overview

    http://www.analog.com/en/design-center/evaluation-hardware-and-software/cu_eb_plc_demo_system.html

     

    Texas Instruments:

    Single Supply Analog Input Module Reference Design with 16-Bit, 8-Channel ADC for PLC - TIPD166 - TI Tool Folder

    Analog Input Module for Industrial Outputs and Temperature Sensors Reference Design - TIPD164 - TI Tool Folder

     

    Maxim:

    https://www.maximintegrated.com/en/products/interface/current-loop-products-4-20ma.html

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • oksbwn
    oksbwn over 10 years ago in reply to kulky64

    Thanks..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • uscdadnyc
    uscdadnyc over 10 years ago in reply to oksbwn

    Is the situation: (a) Measuring DC Current (at Currents mentioned) AS you would using a (temporary) Test Instrument? OR (b) Circuitry that you would build that attaches to the circuitry that you want to monitor? IF (b) then the previously post Comments will do.

    However if the situation is (a) then consider a "Portapow Premium USB+DC Power Monitor (portapow.co.uk). I have one and it works great. Remember this is DC. The documentation is lousy, but I drew-up several diagrams that explains the various connections. Will try to post them here BUT I haven't

    gotten a Win10 Driver for the Scanner Portion of my Samsung SCX-4016scx MFP. WRT that I am attempting a "virtual" WinXP  w/i my Win10 PC. But that is Tangential to this discussion.

    USCDADNYC (NY NY USA)

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago

    4-20mA is a nice standard for instrumentation measurement and is used in industry extensively. the nice thing about it is it has automatic fault detections as zero = 4mA, any less than 4 means an error, more than 20 also an error. being a current loop also means impervious to alot of noise sources and also lead length can be significant subject to the ability of the source to provide enough volts. It can even be measured by many series devices... anyway I digress (I spent many years in the Gas industry using 4-20mA transducers for pressure, flow and temperature.

     

    Your current approach has been the mainstay for what seems forever. Use a resistor to measure the current (IE, convert the current to a voltage), typically a 200Ohm or 250Ohm is used to then provide a 5V FSD,but of course if your measurement device is only able to handle a lower voltage, reduce the sense resistor appropriately.

     

    I am not aware of any current input ADC, those that claim to support 4-20mA are basically providing the current sense resistor themselves so you're no better off except for perhaps a lower BOM or board footprint.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • oksbwn
    oksbwn over 10 years ago in reply to Robert Peter Oakes

    Thanks Peter..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mprojects
    mprojects over 10 years ago

    You can use the 4-20mA R click from MikroElektronika which combines the current measurement circuits and also provides 16V supply for the loop. Best way is to use it on an Arduino Uno click shield.

     

    4-20mA R Click - mikroBUSTm sized board which serves as a receiver in a 4-20mA current loop standard

    Arduino Uno click shield - mikroBUSTm host sockets extension for Arduino Uno compatible boards

     

    You can find here some tutorials on using the 4-20mA T (transmitter) and  4-20mA R (receiver) boards:

     

    https://microcontroller-projects.com/4-20ma-arduino-tutorial-hardware/

    https://microcontroller-projects.com/4-20ma-current-loop-arduino-transmitter/

    https://microcontroller-projects.com/4-20ma-current-loop-arduino-receiver/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bhaskar.anil430
    bhaskar.anil430 over 8 years ago

    I wrote this article for reading 4-20mA using Arduino. I am using ADS1115 and INA196 to read the current and convert into digital values.

    feel free to check out.

    https://ncd.io/how-to-read-4-20ma-current-loop-sensors/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • prodegyprogeny
    prodegyprogeny over 8 years ago

    i was looking for something lik this to and i found this on tindie
    https://www.tindie.com/products/Circuitar/adc-4-20-nanoshield-ads1115-for-4-20ma-sensors/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 8 years ago

    A couple of others that might work:

    ACS712

    INA219