Arduino Forum Arduino Mega 2560 connection issues
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
  • Replies 4 replies
  • Subscribers 402 subscribers
  • Views 727 views
  • Users 0 members are here
  • troubleshooting
  • arduino mega 2560
  • troubleshoot
  • arduino
  • arduino mega
Related

Arduino Mega 2560 connection issues

victorduchateau
victorduchateau over 9 years ago

Hi,

 

I've been using Arduinos for quite a while now and know a lot about them. But recently none of my Arduino Mega 2560's would connect to any of my computers (Mac and Windows).

When I plug my Arduino Mega's in my computer, no serial port will show up in the tools section in the arduino program (one of the arduinos even is brand new and never used).

On Windows when I go to device manager, the COM port also doesn't show up there either.

 

I'm sure there's an easy fix for this

 

Please reply if you know a solution

Thanks

Victor

  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago

    It is also possible the 8U2 chip (Not FTDI on the older mega) is fried, this can happen depending on what you do with the device. I have had it happen once.

     

    You can re-flash them using the ISP header near the USB connector. (Assuming it is a code issue and not a hardware issue.

     

    If it is fried then you can replace the device and program it from the code supplied by Arduino.

     

    I am running the latest windows 10 and it is still detecting my board with no issues and it is using the old 8U2 chip with original firmware.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago

    It is also possible the 8U2 chip (Not FTDI on the older mega) is fried, this can happen depending on what you do with the device. I have had it happen once.

     

    You can re-flash them using the ISP header near the USB connector. (Assuming it is a code issue and not a hardware issue.

     

    If it is fried then you can replace the device and program it from the code supplied by Arduino.

     

    I am running the latest windows 10 and it is still detecting my board with no issues and it is using the old 8U2 chip with original firmware.