Arduino Forum Arduino Mega 2560 connection issues
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
  • Replies 4 replies
  • Subscribers 402 subscribers
  • Views 727 views
  • Users 0 members are here
  • troubleshooting
  • arduino mega 2560
  • troubleshoot
  • arduino
  • arduino mega
Related

Arduino Mega 2560 connection issues

victorduchateau
victorduchateau over 9 years ago

Hi,

 

I've been using Arduinos for quite a while now and know a lot about them. But recently none of my Arduino Mega 2560's would connect to any of my computers (Mac and Windows).

When I plug my Arduino Mega's in my computer, no serial port will show up in the tools section in the arduino program (one of the arduinos even is brand new and never used).

On Windows when I go to device manager, the COM port also doesn't show up there either.

 

I'm sure there's an easy fix for this

 

Please reply if you know a solution

Thanks

Victor

  • Sign in to reply
  • Cancel
Parents
  • mprojects
    mprojects over 9 years ago

    Try to uninstall and then reinstall the FTDI drivers.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • victorduchateau
    victorduchateau over 9 years ago in reply to mprojects

    Thanks for the quick reply!

     

    I did what you said and the newest board now works. The old Arduino Mega however still doesn't work.

     

    Regards

    Victor

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mprojects
    mprojects over 9 years ago in reply to victorduchateau

    As I remember, the older mega use anAtmega16U2 to perform USB-UART function. If so, they will appear with the "lemon" sign in  Device Manager. You can either remove the driver and let the computer re-detect it, or you can try to use driver update and hope it works. In the worst case scenario, uninstall the IDE and then reinstall it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • mprojects
    mprojects over 9 years ago in reply to victorduchateau

    As I remember, the older mega use anAtmega16U2 to perform USB-UART function. If so, they will appear with the "lemon" sign in  Device Manager. You can either remove the driver and let the computer re-detect it, or you can try to use driver update and hope it works. In the worst case scenario, uninstall the IDE and then reinstall it.