Arduino Forum Frequency Generator with 2x Variable Resistors
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
  • Replies 4 replies
  • Subscribers 391 subscribers
  • Views 496 views
  • Users 0 members are here
Related

Frequency Generator with 2x Variable Resistors

toxsickcity
toxsickcity over 8 years ago

Hi Guys,

 

I need serious help with starting a project, I am going to connect this to a pair of Valves, these Solenoid Valves will be very precise and will be under up to 30PSI pressure.

I need to have 1 solenoid OPEN and the OTHER CLOSED or VICE VERSA...

 

I will use an Arduino to control this and I have not started yet

 

I need to make a signal output on Pin 1 and Pin 2 be opposite! eg

when Pin 1 is OFF / Pin 2 is ON

when Pin 1 is ON / Pin 2 is OFF

 

this next section I am speaking of PIN 1.. (remembering PIN 2 will always be doing the opposite!!!)

I need to have 1 Variable Resistor (VR1)(Potentiometer) to control how long pin 1 stays ON (I was thinking a value of 0-100% of VR2)

I also need a 2nd Variable Resistor (VR2)to control how long it takes for Pin 1 to reset the cycle!

 

eg the output should be able to: Pin 1 again,. remembering Pin 2 will always be opposite!

Pin 1 stays on for 1 second every 5 seconds

or

Pin 1 stays on for 100ms every 1second

or

Pin 1 stays on for 200ms every 300ms

 

I would say the range should be, here I am unsure on converting...

I want to be able to slow to 5 seconds and go fast as (10hz - 10 times/second) is 10hz = 100ms?

 

Thanks

Shaun

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 8 years ago +4
    It sounds like a dual 555 timer chip (556) could perform all the timing you need - variable duty cycle at a variable frequency. They can operate up to 15 Volts, so should run off the same supply as the…
  • mcb1
    mcb1 over 8 years ago +3
    Sounds simple. There are a couple of ways to do the 'opposite pin' thing. You'll need to drive the valve with a transistor or Mosfet regardless of what method is used. Unless you have something else you…
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to shabaz +2
    ... using rotary encoders instead of potentiometers could help here. You can then define both their range and dynamic behaviour in the source code. You could refine the output with huge chunks when the…
Parents
  • mcb1
    mcb1 over 8 years ago

    Sounds simple.

     

    There are a couple of ways to do the 'opposite pin' thing.

    You'll need to drive the valve with a transistor or Mosfet regardless of what method is used.

    Unless you have something else you haven't specified, the 'other' valve will always be opposite.

     

    This hardware could include the second output that is opposite in phase (ie off when the driver/pin1 is on).

     

     

    Regarding your analogue input, you simply have to specify the range of control.

    I think you commented 0.1sec (10Hz) to 5 secs.for the 'cycletime', but you've only said it should be on for 100-200mS.

     

    If the 'cycletime' is 0.1Hz which is 100mS, and the duration is 100mS, it would be ON all the time ... presumably not the intention.

    .

     

    Let's presume the timing doesn't need to be accurate, then a potentiometer is fine.

    You can easily use the MAP command to change the 0-1024 value you'll get from the AnalogRead command and use it to control the on time/duration time.

    0.1 is 100mS and 5 secs is 5000mS which is a normal integer.

    I don't have the IDE here, but I would map 0 to 100 and 1024 to 5000 or the other option is 0 to 5000 and 1024 to 100.

     

    MAP is a linear conversion, but you can use a logarithmic potentiometer which has a non linear characteristic to make it seem more even.

     

     

    An example exists in the IDE.

    Blinkwithoutdelay uses the millis() timer and would be what I'd suggest.

    You'll have two seperate timer variables, one for 'cycletime' and the other for 'duration'

     

     

    Hope this helps start you out.

    You'll need to fill in the blanks I mentioned.

     

    Cheers

    Mark

     

    .

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • mcb1
    mcb1 over 8 years ago

    Sounds simple.

     

    There are a couple of ways to do the 'opposite pin' thing.

    You'll need to drive the valve with a transistor or Mosfet regardless of what method is used.

    Unless you have something else you haven't specified, the 'other' valve will always be opposite.

     

    This hardware could include the second output that is opposite in phase (ie off when the driver/pin1 is on).

     

     

    Regarding your analogue input, you simply have to specify the range of control.

    I think you commented 0.1sec (10Hz) to 5 secs.for the 'cycletime', but you've only said it should be on for 100-200mS.

     

    If the 'cycletime' is 0.1Hz which is 100mS, and the duration is 100mS, it would be ON all the time ... presumably not the intention.

    .

     

    Let's presume the timing doesn't need to be accurate, then a potentiometer is fine.

    You can easily use the MAP command to change the 0-1024 value you'll get from the AnalogRead command and use it to control the on time/duration time.

    0.1 is 100mS and 5 secs is 5000mS which is a normal integer.

    I don't have the IDE here, but I would map 0 to 100 and 1024 to 5000 or the other option is 0 to 5000 and 1024 to 100.

     

    MAP is a linear conversion, but you can use a logarithmic potentiometer which has a non linear characteristic to make it seem more even.

     

     

    An example exists in the IDE.

    Blinkwithoutdelay uses the millis() timer and would be what I'd suggest.

    You'll have two seperate timer variables, one for 'cycletime' and the other for 'duration'

     

     

    Hope this helps start you out.

    You'll need to fill in the blanks I mentioned.

     

    Cheers

    Mark

     

    .

    • Cancel
    • Vote Up +3 Vote Down