Arduino Forum Frequency Generator with 2x Variable Resistors
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
  • Replies 4 replies
  • Subscribers 391 subscribers
  • Views 496 views
  • Users 0 members are here
Related

Frequency Generator with 2x Variable Resistors

toxsickcity
toxsickcity over 8 years ago

Hi Guys,

 

I need serious help with starting a project, I am going to connect this to a pair of Valves, these Solenoid Valves will be very precise and will be under up to 30PSI pressure.

I need to have 1 solenoid OPEN and the OTHER CLOSED or VICE VERSA...

 

I will use an Arduino to control this and I have not started yet

 

I need to make a signal output on Pin 1 and Pin 2 be opposite! eg

when Pin 1 is OFF / Pin 2 is ON

when Pin 1 is ON / Pin 2 is OFF

 

this next section I am speaking of PIN 1.. (remembering PIN 2 will always be doing the opposite!!!)

I need to have 1 Variable Resistor (VR1)(Potentiometer) to control how long pin 1 stays ON (I was thinking a value of 0-100% of VR2)

I also need a 2nd Variable Resistor (VR2)to control how long it takes for Pin 1 to reset the cycle!

 

eg the output should be able to: Pin 1 again,. remembering Pin 2 will always be opposite!

Pin 1 stays on for 1 second every 5 seconds

or

Pin 1 stays on for 100ms every 1second

or

Pin 1 stays on for 200ms every 300ms

 

I would say the range should be, here I am unsure on converting...

I want to be able to slow to 5 seconds and go fast as (10hz - 10 times/second) is 10hz = 100ms?

 

Thanks

Shaun

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 8 years ago +4
    It sounds like a dual 555 timer chip (556) could perform all the timing you need - variable duty cycle at a variable frequency. They can operate up to 15 Volts, so should run off the same supply as the…
  • mcb1
    mcb1 over 8 years ago +3
    Sounds simple. There are a couple of ways to do the 'opposite pin' thing. You'll need to drive the valve with a transistor or Mosfet regardless of what method is used. Unless you have something else you…
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to shabaz +2
    ... using rotary encoders instead of potentiometers could help here. You can then define both their range and dynamic behaviour in the source code. You could refine the output with huge chunks when the…
Parents
  • shabaz
    shabaz over 8 years ago

    Hi Shaun,

     

    I think the Arduino is the wrong part for this. The result won't be great, there will be granularity issues and furthermore jitter due to noise in the VR1/2 value read (unless digitally filtered which means more code and some latency).

    There are easier solutions like this one, see the datasheet for detail:

    http://www.linear.com/product/LTC6992-1

    For the inverted output, one idea is to use an inverter logic gate IC.

    An alternative way using easy-to-obtain parts (but a bigger circuit) would be to generate a triangle or sawtooth wave under control of a variable resistor, and then use a comparator to convert to pulses (with a second variable resistor controlling the pulse width by changing the comparator threshold).

    Although I cannot design the circuit for you, for an idea, see the circuit here: Raspberry Pi enabled Christmas Lights

    By changing the value of R1 in the sawtooth generator circuit there, you can change the frequency (this is equivalent to your VR2).

    The circuit below that on the same web page shows the comparator acting as the PWM generator, controlling the pulse width.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 8 years ago

    Hi Shaun,

     

    I think the Arduino is the wrong part for this. The result won't be great, there will be granularity issues and furthermore jitter due to noise in the VR1/2 value read (unless digitally filtered which means more code and some latency).

    There are easier solutions like this one, see the datasheet for detail:

    http://www.linear.com/product/LTC6992-1

    For the inverted output, one idea is to use an inverter logic gate IC.

    An alternative way using easy-to-obtain parts (but a bigger circuit) would be to generate a triangle or sawtooth wave under control of a variable resistor, and then use a comparator to convert to pulses (with a second variable resistor controlling the pulse width by changing the comparator threshold).

    Although I cannot design the circuit for you, for an idea, see the circuit here: Raspberry Pi enabled Christmas Lights

    By changing the value of R1 in the sawtooth generator circuit there, you can change the frequency (this is equivalent to your VR2).

    The circuit below that on the same web page shows the comparator acting as the PWM generator, controlling the pulse width.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to shabaz

    ... using rotary encoders instead of potentiometers could help here. You can then define both their range and dynamic behaviour in the source code.

    You could refine the output with huge chunks when the encoder is turned fast, and small steps when turned slow.

    • Cancel
    • Vote Up +2 Vote Down