Arduino Forum FM Radio review
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
  • Replies 28 replies
  • Subscribers 403 subscribers
  • Views 4461 views
  • Users 0 members are here
  • fm radio
  • rotary_encoder
  • i2c lcd
  • speaker amplifier
  • arduino
Related

FM Radio review

hofa
hofa over 8 years ago

Hi everyone,

 

This is my first ever electronics project. I'm an IT infrastructure professional but as most of my kind, I only deal with servers, switches, routers, operating systems and so forth. I designed and breadboarded a simple fm radio with an Arduino UNO and I'm here to ask what I could improve before soldering everything together with an Arduino Nano.

 

Components (is it correct to call these 'active components'?):

  • Aruino Uno (despite what the scheme says, planning the use a nano for the finished product)
  • TEA5767 on an I2C board
  • A 2x16 LCD connected through an I2C board
  • XH-M177 speaker amplifier (with to 8ohm 0,5 W speakers) with a volume knob (PotMeter) which clicks off when rotated all the way left.
  • Rotary encoder for tuning

 

Edit: new scheme after recomendations. I stated that a 100nF capacitor was enough for the LCD not to go haywire when clicking off the volume button... that was incorrect, switched it back to a 100uF (I don't have any others).

image

 

I added one capacitor because the LCD would go haywire when I switched off/on the amplifier. What do you guys think about this scheme? I am going to add a simple on/off switch to completely turn of the circuitry when not in use.

 

I tried catching the off switch from the amplifier but power still seems to go through after it clicked off. I found one pin that still produced around 1V (in stead of 5V) but I don't know how to use that because it's still letting current through and a digitalRead would not be able to catch the 'off' action, right?

Edit: wrong: The threshold is about 0.3*VCC (= 1.5V when VCC = 5V) so that's enough to catch it. Maybe I'll put a resistor in place to be more certain... Changed the code accordingly.

 

Also, I don't understand the concept around pull-down and pull-up resistors. I watched the latest TBHS (BB8 with LED art) and he speaks about it but it's all a bit too fast for me. I really do want to understand it.

 

The code as it is below, feel free to comment on this too (edited this too after being able to catch the volume knob off switch state):

 

//Libraries
#include <TEA5767.h>
#include <LiquidCrystal_I2C.h>
#include <MD_REncoder.h>
#include <EEPROM.h>

//I2C address 63 (0x3F) = Radio
//I2C address 96 (0x60) = LCD

//Constants
const int radioPin = 7;
const int ampReadPin = 2;
const int ampPowerPin = 3;
const int REclk = 4;
const int REdt = 5;
const int REsw = 6;
const boolean debug = false;
#define I2C_ADDR    0x3F

//Variables
double old_freq;
double temp_freq;
double freq;
boolean ampReadPower;
boolean ampReadPower_old;
int stereo;
int stereo_old;
int signal_level;
int signal_level_old;
int REdt_old;
int REdt_temp;
int REclk_temp;
unsigned char buf[5];
unsigned long ms;
boolean rotPot = true;
int slowDown = 30000;

//Signal chars
byte level1[8] = {0b00000,0b00000,0b00000,0b00000,0b00000,0b00000,0b00011,0b11111};
byte level2[8] = {0b00000,0b00000,0b00000,0b00000,0b00001,0b01111,0b11111,0b11111};
byte level3[8] = {0b00000,0b00000,0b00000,0b00111,0b11111,0b11111,0b11111,0b11111};
byte level4[8] = {0b00000,0b00011,0b11111,0b11111,0b11111,0b11111,0b11111,0b11111};
byte level5[8] = {0b01111,0b11111,0b11111,0b11111,0b11111,0b11111,0b11111,0b11111};
byte loading[8] = {0b00000,0b00000,0b00000,0b11111,0b11111,0b00000,0b00000,0b00000};

//I2C pinout SLC and SDA - Arduino pins A5 and A4
LiquidCrystal_I2C lcd(I2C_ADDR, 16, 2);
TEA5767 Radio;

// Rotary encoder
MD_REncoder R = MD_REncoder(4, 5);

void setup() {
  Serial.begin(57600);

  // Initiate rotary encoder
  R.begin();

  // Set amplifier pins
  pinMode(ampReadPin, INPUT);
  pinMode(ampPowerPin, OUTPUT);
  digitalWrite(ampPowerPin, LOW);

  // Set Rotary Encoder pins
  pinMode(REclk, INPUT);
  pinMode(REdt, INPUT);
  pinMode(REsw, INPUT);

  // Initiate LCD
  lcd.begin ();
  lcd.backlight();
  lcd.display();
  lcd.clear();
    
  // Set radio pin
  pinMode(radioPin, OUTPUT);
  digitalWrite(radioPin, HIGH);
  
  // Initiate Radio
  Radio.init();
  EEPROM.get(0, freq);
  Radio.set_frequency(freq);
  Radio.read_status(buf);
  stereo = Radio.stereo(buf);
  signal_level = Radio.signal_level(buf);
  
  // create signal characters
  lcd.createChar(1, level1);
  lcd.createChar(2, level2);
  lcd.createChar(3, level3);
  lcd.createChar(4, level4);
  lcd.createChar(5, level5);
  lcd.createChar(6, loading);

  // Display loading screen and boot amp
  loadingScreen(2200);
  digitalWrite(ampPowerPin, HIGH);
  delay(100);
  ampReadPower = digitalRead(ampReadPin);
  if (ampReadPower == LOW) setStandby(LOW);
  ampReadPower_old = ampReadPower;

  // First display showing
  displayFreq();
  displayStereo();
  displaySignal();
}

void loop() {
  // Read rotary encoder changes and update frequency
  uint8_t x = R.read();
  if (x) 
  {
    x == DIR_CW ? freq+=0.1 : freq-=0.1;
    if (freq < 87.5) freq = 87.5;
    if (freq > 108.0) freq = 108.0;
    Serial.println(freq);
  }

  // Slow down screen updates to about once every second
  // This is needed for the Rotary encoder to work
  if ((slowDown += 1) > 30000) {

    // Soft poweroff by reading amp power status
    ampReadPower = digitalRead(ampReadPin);
    if (ampReadPower != ampReadPower_old) {
      ampReadPower_old = ampReadPower;
      setStandby(ampReadPower);
    }
    
    // Get Radio status
    Radio.read_status(buf);

    // Fill radio info
    stereo = Radio.stereo(buf);
    signal_level = Radio.signal_level(buf);
  
    // Only change display if 'stereo' changes
    if (stereo != stereo_old) {
      displayStereo();
      stereo_old = stereo;
    }
  
    // Only change display if 'signal' changes
    if (signal_level != signal_level_old) {
      displaySignal();
      signal_level_old = signal_level;
    }

    // Only change display and frequency if 'freq' changes
    if (freq != old_freq) {
      displayFreq();
  
      // Set timer for next block
      if (rotPot) {
        ms = millis();
        rotPot = false;
      }
  
      // Only change frequency if rotary encoder hasn't been changed in 500ms
      if (ms + 500 < millis() and temp_freq == freq) {
        Radio.set_frequency(freq);
        old_freq = freq;
        rotPot = true;
      }
      
      temp_freq = freq;

      // Write frequency to EEPROM
      EEPROM.put(0, freq);
    }
    
    slowDown = 0;
  }
}

/////////////////////////
//      FUNCTIONS      //
/////////////////////////

// Set standby state
void setStandby(int state) {
  if (state == HIGH) {
    // Disable amp so we don't get noise
    digitalWrite(ampPowerPin, LOW);
    // Enable display
    lcd.display();
    lcd.backlight();
    // enable radio
    digitalWrite(radioPin, state);
    Radio.set_frequency(freq);
    // give radio time to load
    loadingScreen(1400);
    displayFreq();
    // enable amp
    digitalWrite(ampPowerPin, HIGH);
  } else {
    // disable display
    lcd.clear();
    lcd.setCursor(0,0);
    lcd.print("Volume off...");
    delay(1000);
    lcd.noDisplay();
    lcd.noBacklight();
    // Disable radio
    digitalWrite(radioPin, state);
  }
  

}

// Display the wanted frequency
void displayFreq() {
  lcd.setCursor(0, 0);
  lcd.print("   ");
  if (freq < 100) {
    lcd.print(" ");
  }
  lcd.print(freq);
  lcd.print(" Mhz ");
}

// Display wether sound is in Stereo or Mono
void displayStereo() {
  lcd.setCursor(0, 1);
  if (stereo) lcd.print("Stereo");
  else lcd.print("Mono  ");
}

// Display the signal strength
void displaySignal() {
  lcd.setCursor(11, 1);
  signal_level >= 2 ? lcd.write((byte) 1) : lcd.print(" ");
  signal_level >= 4 ? lcd.write((byte) 2) : lcd.print(" ");
  signal_level >= 6 ? lcd.write((byte) 3) : lcd.print(" ");
  signal_level >= 8 ? lcd.write((byte) 4) : lcd.print(" ");
  signal_level >= 10 ? lcd.write((byte) 5) : lcd.print(" ");
}

// Clear 'old' LCD values to force an update
void clearLCDValues() {
  double old_freq;
  int stereo_old;
  int signal_level_old;  
}

void loadingScreen(int loadDelay) {
  // Wait for sound till radio module inits completely + show loading
  lcd.clear();
  lcd.setCursor(0,0);
  lcd.print("   Loading...   ");
  lcd.setCursor(0,1);
  for(int x=0 ; x<16 ; x++) {
    //lcd.print("-");
    lcd.write((byte) 6);
    delay((double) loadDelay/16);
  }
  lcd.clear();
}

 

Thank you very much for your time!

 

Best regards,

Thomas

 

Message was edited by: Thomas Hofkens changed up the scheme and code to reflect changes as proposed by others

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 8 years ago +2
    Hi Thomas, The SDA and SCL lines specifically either need a resistor (try about 4.7k) to +5v, or they should be omitted if the Arduino already has them integrated. There should be no resistors to 0V, which…
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to hofa +2
    Ok. The module already has the required resistors. They are R2 and R3 on your drawing. I had a more stable encoder when adding a few capacitors. It takes care that the operation isn't jumpy and nervous…
  • hofa
    hofa over 8 years ago in reply to shabaz +2
    Thanks all! As I said: first time for everything I'm putting on here... I understand that I shouldn't change the original post but I certainly didn't expect this much reaction so my apologies for that…
Parents
  • beacon_dave
    beacon_dave over 8 years ago

    Hi Thomas - perhaps you may want to take a look at this tutorial on pull-down / pull-up resistors

    http://www.electronics-tutorials.ws/logic/pull-up-resistor.html

    as it goes into a bit more detail than the TBHS BB8 with LED art.

     

    Thomas Hofkens wrote:

     

    Hi everyone,

     

    ...

    Also, I don't understand the concept around pull-down and pull-up resistors. I watched the latest TBHS (BB8 with LED art) and he speaks about it but it's all a bit too fast for me. I really do want to understand it.

     

    ...

    Thank you very much for your time!

     

    Best regards,

    Thomas

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • beacon_dave
    beacon_dave over 8 years ago

    Hi Thomas - perhaps you may want to take a look at this tutorial on pull-down / pull-up resistors

    http://www.electronics-tutorials.ws/logic/pull-up-resistor.html

    as it goes into a bit more detail than the TBHS BB8 with LED art.

     

    Thomas Hofkens wrote:

     

    Hi everyone,

     

    ...

    Also, I don't understand the concept around pull-down and pull-up resistors. I watched the latest TBHS (BB8 with LED art) and he speaks about it but it's all a bit too fast for me. I really do want to understand it.

     

    ...

    Thank you very much for your time!

     

    Best regards,

    Thomas

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • hofa
    hofa over 8 years ago in reply to beacon_dave

    I will read through it. It is hard though to read through these english articles because in dutch we have other words for all components (resistor <> weerstand, capacitor <> condensator, ...). Not that I don't understand it but it takes a lot of concentration when reading. Now 00:30 in Belgium and I told my wife I'd be crawling in to bed with her about 90 minutes ago... Maybe not the best time for learning