Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Sauna Heater Control. Help Needed.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 24 replies
  • Subscribers 417 subscribers
  • Views 5101 views
  • Users 0 members are here
Related

Sauna Heater Control. Help Needed.

studioab
studioab over 8 years ago

I've finished my first IoT project based on Arduino Yun. It's a remote control for my sauna. Everything is working as expected in test mode (relay is not connected to contactor so there is no real load), I was able to test this system for hours without any problems.

 

When I hook up contactor to relay, it turns the heater on and off, and everything seems to be working, but after a while (absolutely random, it could be an hour or a few minutes) LCD screen freezes, or sometimes, starts flashing random symbols, server is not responding to commands, rotary encoder isn't working and it seems Arduino freezes. The only workaround is to turn off the power and reset the system. After it restarts, everything is back to normal.

 

I came across this post 16*2 LCD getting weird characters symptoms are the same, I think high AC load is causing EMF impulse that is crashing Arduino. Power Module, Relay board, LCD, and Arduino board are really close to each other and inside the box.

 

I'm not sure if it violates the rules, but I would like to mention these people from the other post @WarrenW @Robert Peter Oakes @Gough Lui @neilk @D_Hersey

 

I think here are my options. What would you recommend to do?

 

- replace relays with solid state relay

- shield AC wires

- remove power module from the box

- don't use the same power module for relays

- ???

Attachments:
image
image
image
image
image
  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 8 years ago in reply to studioab +4
    I would like to say huge thank you to all people that contributed to this thread. I was able to eliminate all the issues causing arduino to crash Glad we could help. Do you guys think this project should…
  • jw0752
    jw0752 over 8 years ago +3
    Hi Eugene, The answer might be as simple as adding more decoupling capacitance with low ESR to the power feed to the Arduino. This can be done by putting a 100 nF capacitor and a 100 uF cap in parallel…
  • ralphjy
    ralphjy over 8 years ago +3
    Hi Eugene, Nice looking project. I would suspect your problem is that the 240V input glitches when your load switches and that causes the 5V to glitch. If you had a scope you could monitor the 5V supply…
Parents
  • mcb1
    mcb1 over 8 years ago

    studioab

    It looks like a nice project, and the pysical isolation to users is a great safety point.

    Your pictures show a number of 5v relays, and I'm presumming the contacts on these is switching the 240v mains power to the contactor.

     

    relay is not connected to contactor so there is no real load

    Does this mean you tested it with the 5v relays in place.?

     

    When I hook up contactor to relay

    Does this line mean the 240v connected to the relay contactor to power the contactor.

     

    Do you have any details of the 5v supply that you are using.?

    My suspicion is that when the heater is switched, the load from the 5v relays combined with the drop in mains voltage is causing the 5v supply line to fall enough to cause issues.

    There are several ways to overcome this, but the answers to the above will help decide which solution is more suitable.

     

     

    The proximity is not the issue here.

    Cheers

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • mcb1
    mcb1 over 8 years ago

    studioab

    It looks like a nice project, and the pysical isolation to users is a great safety point.

    Your pictures show a number of 5v relays, and I'm presumming the contacts on these is switching the 240v mains power to the contactor.

     

    relay is not connected to contactor so there is no real load

    Does this mean you tested it with the 5v relays in place.?

     

    When I hook up contactor to relay

    Does this line mean the 240v connected to the relay contactor to power the contactor.

     

    Do you have any details of the 5v supply that you are using.?

    My suspicion is that when the heater is switched, the load from the 5v relays combined with the drop in mains voltage is causing the 5v supply line to fall enough to cause issues.

    There are several ways to overcome this, but the answers to the above will help decide which solution is more suitable.

     

     

    The proximity is not the issue here.

    Cheers

    Mark