Arduino Forum i m having difficulty in this project somebody will help me....only pro programmers can do it
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
  • Replies 8 replies
  • Subscribers 392 subscribers
  • Views 1043 views
  • Users 0 members are here
Related

i m having difficulty in this project somebody will help me....only pro programmers can do it

Former Member
Former Member over 9 years ago

PROJECT

When your system is in the idle mode, RGB module’s color in your system stays in Red. This

represents the default state of your system.

As the next step, use the key board array (4 x 4 pushbuttons) in the kit to get the one of

your group member’s e-id. The e-id and student name must be displayed on the LCD panel.

If it is the right e-id, your system is enabled, otherwise there is no way you can enable the

system. Here, your system should sound differently depending on the e-id, for example, if

correct, sounds something good, if not, sound something weird.

 Once you have the system enabled correctly, change the color of RGB module into Green.

 Your system also has a push button to start a stepper (or a servo) motor. It is your choice

whether you want to use stepper or servo motor.

 When you keep the button pressed, the motor keeps rotating. (Note that 5 turns may

simulate a complete part machining cycle)

 When the motor rotates 5 full turns, turn your RGB module into Blue. After 5 seconds,

change the color of your RGB into Green.

 Each time your motor makes 5 full turns, you need to count up the number of machined

parts by “1” and display total number of machined parts on a “4 digital tube” included in the

kit.

 There is another push button with which you can finish the whole process and get out of

the process. If you push this button, you cannot continue. The only way you start over is to

input the right e-id number of your own group again. In other words, this button makes the

state of your system back to idle.

 

I have done till here so far

#include <LiquidCrystal.h>

#include <Wire.h>

#include <Keypad.h>

 

const byte rows = 4;

const byte cols = 4;

char* ourCode = "1234";

int currentPosition = 0;

 

 

char keys[rows][cols] = {

{'1','2','3','A'},

{'4','5','6','B'},

{'7','8','9','C'},

  {'*','0','#','D'}

};

byte rowPins[ROWS] = {A3, A2, A1, A0};

byte colPins[COLS] = {10, 9, 8, 7};

 

Keypad keypad = Keypad(makeKeymap(keys), rowPins, colPins, rows, cols);

 

// initialize the library with the numbers of the interface pins

LiquidCrystal lcd(12, 11, 5, 4, 3, 2);

int greenLED = 6;

int redLED = 13;

int blueLED = 1;

void setup() {

  // set up the LCD's number of columns and rows:

  lcd.begin(16,2);

   pinMode(redLED, OUTPUT);

  pinMode(greenLED, OUTPUT);

pinMode(blueLED, OUTPUT);

digitalWrite(redLED, LOW);

digitalWrite(greenLED, LOW);

digitalWrite(blueLED, LOW);

 

}

 

void loop() {

 

 

    char key = keypad.getKey();

 

  if (key == ‘0’|| key!='ourCode') {

lcd.setCursor(0,0);

 

  1. lcd.print("Invalid input");

  // Print a message to the LCD.

digitalWrite(redLED, HIGH);

  if (key==’ourCode’) {

digitalWrite(greenLED, High);

digitalWrite(redLED,LOW);

  lcd.setCursor(2, 0);

lcd.print("Name:james!");

  // print the number of seconds since reset:

    lcd.setCursor(2, 1);

lcd.print("YOUR ID:1234");

  

 

}

}

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 9 years ago in reply to gadget.iom +6
    'Coz no one would take this on except for money MK
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to Former Member +3
    Hello, first of all, it seems that you mention a series of components but the correspondence with the design is just partial. Then I see three Arduino board with the different connections while it seems…
  • gadget.iom
    gadget.iom over 9 years ago +2
    Why can only "pro programmers" do it?
Parents
  • gadget.iom
    gadget.iom over 9 years ago

    Why can only "pro programmers" do it?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • gadget.iom
    gadget.iom over 9 years ago

    Why can only "pro programmers" do it?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • michaelkellett
    michaelkellett over 9 years ago in reply to gadget.iom

    'Coz no one would take this on except for money image

     

    MK

    • Cancel
    • Vote Up +6 Vote Down