Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Noobie with newb questions for simple project
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 415 subscribers
  • Views 1399 views
  • Users 0 members are here
Related

Noobie with newb questions for simple project

masterbri
masterbri over 8 years ago

Hiw are y’all doin!! So, I’ve been playing around with an arduino project for quite a while now and finally got it to work after a year of tinkering. I was working on what seemed like a fairly straight forward led matrix thing using glediator and an Arduino UNO.

 

My current project that I’ve been looking into seems a little more complex to me in that I want to actually have different systems communicating with each other. I’m sure this is kinda child’s play to yall out there that are more familiar with this stuff so please bear with me as I still consider myself quite illiterate in this field!

 

heres my situation: I have two separate objects, one is essentially a transporter and the other would be package. The transporters job is to lift the package and move it to another location. I plan to have an Arduino UNO with an rfid sheild mounted in the transporter and an rfid tag mounted on the package. The first goal is to have the transporter read that the package is near and activate a switch that drops the lifting mech.

The transporter is also outfitted with a photo sensor that triggers an audible alarm letting me know when the package is centered on the lifting mech. The second goal is the have the arduino recognize that the sensor has been triggered, say for 3 seconds, and then activate he other switch which would raise the lifting mech.

 

To me it it seems like two gairly straightforward operations. my biggest obstacle is figuring out how to write a code to handle these two distinct operations within the ide, from scratch

 

i sure appreciate any help y’all could provide!!

thanks, Brian

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 8 years ago +4
    Hi Brian, I'm not sure it is as straightforward as you suggest : ( The devil is in the detail. At a high level, the pseudocode is simple: while(1) { result=readTag(); if(result) { lifting_mechanism…
  • beacon_dave
    beacon_dave over 8 years ago +3
    Perhaps take a look at this RFID tutorial: Tutorial 12 for Arduino: RFID Card Reading It's for a door lock however it covers a lot of the elements your project requires, namely the reading of a RFID tag…
  • fmilburn
    fmilburn over 8 years ago in reply to masterbri +2
    Updated suggestion for mains relay in USA: https://www.adafruit.com/product/2935
Parents
  • masterbri
    masterbri over 8 years ago

    Thank you guys!! I will look into all of the info that you guys provided so far.

    I think I have actually gotten away from the rfid portion in my project as there would be too many limiting factors: mainly my transporter and package are huge metal structures image which will throw the reliability of rfid too out of whack I think. Also, I found a novel way to lower my transporter using a sensor instead.

     

    The only task I need to figure out now is how to have my arduino activate a relay for a certain amount of time when another sensor is activated for a certain amount of time. Kind like: if this for x seconds, then this for y seconds...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fmilburn
    fmilburn over 8 years ago in reply to masterbri

    Hi Brian,

    It is not clear to me whether your issue is firmware or hardware

    The only task I need to figure out now is how to have my arduino activate a relay for a certain amount of time when another sensor is activated for a certain amount of time. Kind like: if this for x seconds, then this for y seconds...

    However, here are some thoughts:

    • If it is determining how to get an x value for a given y value then you can use least squares regression or set up a table and interpolate.  An internet search will turn up hits for both.  Do a search for "delay without blocking" to understand the proper way to implement a time delay.
    • If it is hardware and using a relay then do a search for "Arduino relay" and you will get numerous hits.  The quality of them can be quite bad and even dangerous is you are controlling mains.  I cannot recommend one without knowledge of what you are doing and what relay you will use.  Presuming it is low voltage though you can use an Arduino shield or to build your own - look for a tutorial that includes a transistor to control the relay and a flyback diode to protect the transistor - SparkFun has one I think.  If it is mains then I would stick with something like a PowerSwitch Tail if you are in the USA.  I am sure there are equivalents in Europe and other parts of the world.

    Frank

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • fmilburn
    fmilburn over 8 years ago in reply to masterbri

    Hi Brian,

    It is not clear to me whether your issue is firmware or hardware

    The only task I need to figure out now is how to have my arduino activate a relay for a certain amount of time when another sensor is activated for a certain amount of time. Kind like: if this for x seconds, then this for y seconds...

    However, here are some thoughts:

    • If it is determining how to get an x value for a given y value then you can use least squares regression or set up a table and interpolate.  An internet search will turn up hits for both.  Do a search for "delay without blocking" to understand the proper way to implement a time delay.
    • If it is hardware and using a relay then do a search for "Arduino relay" and you will get numerous hits.  The quality of them can be quite bad and even dangerous is you are controlling mains.  I cannot recommend one without knowledge of what you are doing and what relay you will use.  Presuming it is low voltage though you can use an Arduino shield or to build your own - look for a tutorial that includes a transistor to control the relay and a flyback diode to protect the transistor - SparkFun has one I think.  If it is mains then I would stick with something like a PowerSwitch Tail if you are in the USA.  I am sure there are equivalents in Europe and other parts of the world.

    Frank