Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Coding trouble
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 416 subscribers
  • Views 2555 views
  • Users 0 members are here
Related

Coding trouble

tech_nut81
tech_nut81 over 8 years ago

Hi all. I was wondering if anyone more experienced than myself would be willing to take a look at this code and help me understand what's going wrong. I keep getting this error message, "error: unterminated argument list invoking macro "F".

 

I'll fill ya in on what I'm trying to do. I want to control the water level in a tank using a float switch, solenoid valve and the arduino. I was using just the float switch and solenoid valve connected through a relay, but whenever the water level would start dropping due to water usage, the solenoid would cycle on and off very quickly while keeping the water level up. What I want to do is have the arduino put in a 2 minute delay when the switch is activated so that the tank fills up smoothly.

 

Comments, suggestions and ideas are all appreciated.

 

DJ

Attachments:
Solenoid control.zip
  • Sign in to reply
  • Cancel

Top Replies

  • tech_nut81
    tech_nut81 over 8 years ago in reply to andywest +4
    You're right andywest , it was the double quote. I went back in a put all the F macros back in and only removed the double quotes. Compiling completed successfully after that. Thank you so much for taking…
  • andywest
    andywest over 8 years ago +3
    The F() macro is defined in WString.h , which is part of the core Arduino package. If I understand correctly, it stores a string constant in flash rather than RAM. Very useful in situations where RAM is…
  • tech_nut81
    tech_nut81 over 8 years ago in reply to shabaz +3
    Awesome! I removed all instances of 'F( and the subsequent extra ')' . After that there were a few more errors regarding extra quotation marks. Once I removed all of those compiling was successful. The…
Parents
  • andywest
    andywest over 8 years ago

    The F() macro is defined in WString.h, which is part of the core Arduino package. If I understand correctly, it stores a string constant in flash rather than RAM. Very useful in situations where RAM is limited.

     

    I believe your problem is in Firmware.ino on line 75:

     

    Serial.println(F("(2) 12V Solenoid Valve - 3/4""));

     

    You have mismatched double quotes here. The first double quote after 3/4 terminates the string. The compiler then expects to see either more arguments or a closing parenthesis, but it encounters another double quote instead. That's what "unterminated argument list" means.

     

    To resolve this, try escaping the first double quote:

     

    Serial.println(F("(2) 12V Solenoid Valve - 3/4\""));

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 8 years ago in reply to andywest

    Thanks Andy!

     

    I see, that makes sense. It's vaguely coming back to me. (I don't use Arduino enough..).

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • andywest
    andywest over 8 years ago in reply to shabaz

    No problem. I mainly knew about F() because I've been programming the Arduboy recently. I agree that it's a poorly named macro.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • andywest
    andywest over 8 years ago in reply to shabaz

    No problem. I mainly knew about F() because I've been programming the Arduboy recently. I agree that it's a poorly named macro.

    • Cancel
    • Vote Up +3 Vote Down