Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Need some help with arduino counter project.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 416 subscribers
  • Views 737 views
  • Users 0 members are here
Related

Need some help with arduino counter project.

mustanov
mustanov over 8 years ago

Hello Guys!

I am very new to this community and I will appreciate every help that I can get.
I want to make a little project that will help me a lot in my work. I will try to explain the system that I need as much as possible.

The main task is that I have 5 sensors installed successively , that will count every object that passes in front of them and at the end I can monitor/read the quantities that are passed in front of every sensor and also calculate the difference between exact quantities
I want to monitor the differences like below:

S1-S2 %
S2-S3 %

S4-S3 %
S5-S4 %

I didn't decide how to read the values - from connection to PC or from some Display. I'm opened for suggestions.


I'm currently looking for similar projects so I can start from somewhere. I will be very grateful for hardware and coding support and suggestions from you.

Best Regards!

  • Sign in to reply
  • Cancel

Top Replies

  • luislabmo
    luislabmo over 8 years ago +3
    Hello mustanov I work on common platforms (Arduino, Teensy, Raspberry Pi), with the information given I can give you few simple ideas around those platforms, but is always good to provide more details…
  • luislabmo
    luislabmo over 8 years ago in reply to mustanov +1
    Hello mustanov , My best suggestion for you is to head to a Pololu QTR reflectance sensor (resouces section) , and check how to use their Arduino library . Basically they use two nice ways of using a IR…
Parents
  • mustanov
    mustanov over 8 years ago

    Hello Luis,

    Thank you for your guidance! I have Arduino Uno and I think for my task I will try to use IR Sensors. The object that I need to count are glasses, I will look for some coding now and will appreciate if you have some suggestions for it.

    Thanks in advance!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • luislabmo
    luislabmo over 8 years ago in reply to mustanov

    Hello mustanov,

     

    My best suggestion for you is to head to a Pololu QTR reflectance sensor (resouces section), and check how to use their Arduino library. Basically they use two nice ways of using a IR sensor (and the circuits are a bit different):

    • Analog: the reflectance measurement is output as an analog voltage.
    • Digital: the reflectance measurement is output as a digital voltage (for this one you basically use an arduino pin as an output to charge a capacitor, then use the same pin as input to measure how long does it take to discharge).

     

    I usually pick Analog, is just simpler to code IMO; I just define an Analog threshold to get rid of false alarms.

     

    Or you can just google IR sensor Arduino and take it from there.

     

    Luis

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • luislabmo
    luislabmo over 8 years ago in reply to mustanov

    Hello mustanov,

     

    My best suggestion for you is to head to a Pololu QTR reflectance sensor (resouces section), and check how to use their Arduino library. Basically they use two nice ways of using a IR sensor (and the circuits are a bit different):

    • Analog: the reflectance measurement is output as an analog voltage.
    • Digital: the reflectance measurement is output as a digital voltage (for this one you basically use an arduino pin as an output to charge a capacitor, then use the same pin as input to measure how long does it take to discharge).

     

    I usually pick Analog, is just simpler to code IMO; I just define an Analog threshold to get rid of false alarms.

     

    Or you can just google IR sensor Arduino and take it from there.

     

    Luis