Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum New Arduino Boards Look Interesting
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 416 subscribers
  • Views 894 views
  • Users 0 members are here
  • mkr
  • mkr vidor 4000
  • arduino_uno_wifi
Related

New Arduino Boards Look Interesting

14rhb
14rhb over 8 years ago

Looks like Arduino have brought out two new boards, the Uno WiFi Rev2 and the MKR Vidor 4000 (an FPGA/SAM D21 microcontroller).

Both look really interesting.

 

Time to do some more reading.....and more importantly find where I can get hold of one.

 

https://blog.arduino.cc/2018/05/17/say-hello-to-the-next-generation-of-arduino-boards/

 

Rod

  • Sign in to reply
  • Cancel

Top Replies

  • 14rhb
    14rhb over 8 years ago in reply to shabaz +2
    Yes, the FPGA is also my preferred 'first buy' out of these two. Regarding the SAMD21 the Microchip spec states that this as: "A low-power, high-performance Microchip's ARM Cortex -M0+ based flash microcontroller…
  • jomoenginer
    jomoenginer over 8 years ago in reply to shabaz +2
    I believe the intent was to keep the UNO as an ATmega 8-bit based board since they have the Zero with the SAMD21 chip; given they intend to keep the Zero in production. The ATmega4809 in the new UNO does…
  • shabaz
    shabaz over 8 years ago +1
    Interesting : ) Especially that smaller board. The larger one, I wish they'd gone for a Cortex-M though : ) Still, looks useful.
Parents
  • shabaz
    shabaz over 8 years ago

    Interesting : ) Especially that smaller board.

    The larger one, I wish they'd gone for a Cortex-M though : ) Still, looks useful.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 8 years ago

    Interesting : ) Especially that smaller board.

    The larger one, I wish they'd gone for a Cortex-M though : ) Still, looks useful.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • 14rhb
    14rhb over 8 years ago in reply to shabaz

    Yes, the FPGA is also my preferred 'first buy' out of these two. Regarding the SAMD21 the Microchip spec states that this as:

    "A low-power, high-performance Microchip's ARMRegistered CortexRegistered-M0+ based flash microcontroller, the ATSAMD21G18 is ideal for a wide range of home automation, consumer, metering, and industrial applications."

    So maybe your wish has partly come true? image but I'm guessing you were hoping for a newer/better core.

     

    I'm looking forward to seeing a whole new range of ideas being realised from these and hopefully both are as easy to use as the previous Arduino range.

     

    Rod

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • jomoenginer
    jomoenginer over 8 years ago in reply to shabaz

    I believe the intent was to keep the UNO as an ATmega 8-bit based board since they have the Zero with the SAMD21 chip; given they intend to keep the Zero in production.

    The  ATmega4809 in the new UNO does have  Configurable Custom Logic (CCL) which makes a bit more customizable:

    https://hackaday.com/tag/atmega4809/

     

    There is a Yun 2 that is listed as Coming Soon as well with a EAD of April 23rd. 2019 perhaps?.

    https://store.arduino.cc/usa/arduino-yun-rev-2

     

    Adafruit has the Metro M4 Express that is the same footprint as the UNO but with a SAMD21 which looks interesting.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • 14rhb
    14rhb over 8 years ago in reply to jomoenginer

    Hi Jon,

     

    Those CCL (same as Configurable Logic Cell on the Microchip range) are really useful for doing a small amount of fast logic rather than having the MCU tied up or having to employ another IC. There is a good Microchip application note for using the logic to drive WS2812/Neopixel chains.

     

    Rod