Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum HELP :'(
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 23 replies
  • Subscribers 418 subscribers
  • Views 3166 views
  • Users 0 members are here
  • python
  • help
  • blink led
  • arduinos
  • arduino coding
  • need help coding
Related

HELP :'(

the_future
the_future over 8 years ago

Coding Arduino in Python but got an error and have no idea why please help me

 

My Code:

 

 

import serial                                 # add Serial library for Serial communication

 

 

Arduino_Serial = serial.Serial('com4',9600)  #Create Serial port object called arduinoSerialData

print Arduino_Serial.readline()               #read the serial data and print it as line

print ("Enter 1 to ON LED and 0 to OFF LED")

 

 

while 1:                                      #infinite loop

    input_data = raw_input()                  #waits until user enters data

    print "you entered", input_data           #prints the data for confirmation

  

    if (input_data == '1'):                   #if the entered data is 1

        Arduino_Serial.write('1')             #send 1 to arduino

        print ("LED ON")

     

  

    if (input_data == '0'):                   #if the entered data is 0

        Arduino_Serial.write('0')             #send 0 to arduino

        print ("LED OFF")

 

image

  • Sign in to reply
  • Cancel

Top Replies

  • Dudley
    Dudley over 8 years ago in reply to shabaz +5
    I still call () brackets. I call {} braces and [] square brackets. Parentheses to me is related to sentence structure. Something added as an afterthought in an existing sentence - something you didn't…
  • jomoenginer
    jomoenginer over 8 years ago in reply to Dudley +5
    Some refer to '{}" as curly brackets, so I suppose '()' could be something like happy-sad face brackets. I still refer to '#' as the pound symbol due to my Unix background; '#!' = Pound Bang To each is…
  • gecoz
    gecoz over 8 years ago in reply to the_future +4
    Since the "python setup.py install" seems to be working, probably your Python 2.7 environment is correctly set up. On the other hand, the error you get using the "python3 ..." command is a strong indicator…
Parents
  • the_future
    the_future over 8 years ago

    Hi everyone long story short it now works image thanks everyone for the comments I actually just uninstalled the 3.x version and installed the 2.7 version and tried it again thanks everyone!!!!!!!!!

     

    look out for my next post it is about combining AI and arduino 

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • jomoenginer
    jomoenginer over 8 years ago in reply to the_future

    Nice.  Sometimes it's easier to just change the PATH and/or PYTHONPATH to only have the version of Python you would like to use, but it's good to see you resolved the issue.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • the_future
    the_future over 8 years ago in reply to jomoenginer

    very true I wont lie i shied away from that idea because i got confused and didn't understand what and how to do that 100%

    but I am very grateful!!!!

     

    I am trying to build my own project (BELOW) but just breaking it down and testing simple version of what I am trying to create over

    the summer to improve my skills

     

    image

     

    so please if anyone has any suggestions or improvements I am very open to learning

     

    also what libraries do you think i would need in python, I think i would need:

     

    *pyserial

    *pybrain

    ......and others like speech recognition and something or audio or speech to text conversion

    and more maybe ????

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • the_future
    the_future over 8 years ago in reply to jomoenginer

    very true I wont lie i shied away from that idea because i got confused and didn't understand what and how to do that 100%

    but I am very grateful!!!!

     

    I am trying to build my own project (BELOW) but just breaking it down and testing simple version of what I am trying to create over

    the summer to improve my skills

     

    image

     

    so please if anyone has any suggestions or improvements I am very open to learning

     

    also what libraries do you think i would need in python, I think i would need:

     

    *pyserial

    *pybrain

    ......and others like speech recognition and something or audio or speech to text conversion

    and more maybe ????

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Children
  • gecoz
    gecoz over 8 years ago in reply to the_future

    Hi,

     

    It sounds interesting.

     

    I suggest you post your request for suggestions/help either as a new discussion thread or, better still, as a blog post. Using a single discussion thread for more than one topic can create confusion, and you might end up missing out on valuable comments because people overlooked the thread.

     

    Fabio