Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Circuit Review
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 42 replies
  • Subscribers 416 subscribers
  • Views 5292 views
  • Users 0 members are here
Related

Circuit Review

s1buell
s1buell over 8 years ago

  I`m currently making some proto circuits and I would love some feed back/Ideas etc.

 

All these circuits will connect to Arduino or Arduino compatible devices.

 

Anyone have time to help out with some reviews?

 

First circuit is a 4-20ma board

  • Sign in to reply
  • Cancel

Top Replies

  • genebren
    genebren over 8 years ago in reply to s1buell +4
    You might need to modify your 4-20ma loop front end somewhat. First, the circuit as shown does not have a return path for the current loops. Also, the current loop may not necessarily be directly referenced…
  • genebren
    genebren over 8 years ago in reply to s1buell +4
    Tom, Again, I am not sure that you can count on the second leg of the 4-20ma loop to be at ground potential. You might end up shorting out a driver or introducing ground noise into the circuit. Here is…
  • genebren
    genebren over 8 years ago in reply to s1buell +4
    Tom, Here is an even better link. This shows how to differential sense the loop current. https://www.sensorsmag.com/components/implementing-a-4-ma-to-20-ma-sensor-interface Good luck! Gene
Parents
  • s1buell
    s1buell over 8 years ago

    Wow missed that one. Completing the loop would be nice.... image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • s1buell
    s1buell over 8 years ago

    Wow missed that one. Completing the loop would be nice.... image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • genebren
    genebren over 8 years ago in reply to s1buell

    Tom,

     

    Again, I am not sure that you can count on the second leg of the 4-20ma loop to be at ground potential.  You might end up shorting out a driver or introducing ground noise into the circuit.

     

    Here is a link to some information on the risks of assuming a ground potential on the low side of the loop.

    https://www.dataq.com/blog/data-acquisition/4-20-ma-current-loop-measurements/

     

    Also, not all 4-20ma loop devices are actually supplying current.  There are passive devices that act as a variable resister, and the measuring circuit actually supplies the drive.

     

    On the outside simple.  But potentially quite complex.  If you know the devices that you will be receiving from, then you can make some simplifications to the measuring circuit.

     

    Gene

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • genebren
    genebren over 8 years ago in reply to s1buell

    Tom,

     

    Here is an even better link.  This shows how to differential sense the loop current.

     

    https://www.sensorsmag.com/components/implementing-a-4-ma-to-20-ma-sensor-interface

     

    Good luck!

    Gene

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • abrain
    abrain over 8 years ago in reply to genebren

    Another useful source I found was instrumentation amplifier data sheets - the AMP04 from Analog Devices has a suggested 4-20mA receiver circuit that also shows some TVS protection diodes being used to protect the inputs, which could be useful in an industrial application?

     

    A

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • s1buell
    s1buell over 8 years ago in reply to genebren

    Great info but I have a problem with the shunt resistors. My goal is to create something general to be used with most 4-20ma sensors.

    Is this possible?

     

    I checked out the AMP04 like the circuit but the -15 +15VDC supply becomes an issue.

     

    I also found the RCV402 but there are expensive (old chip too). Anyone know of something newer and similar?

     

    I though making a general 4-20 industrial loop would be easy…… well. Simple concept….. so many options….. lol

     

     

    We sometimes use the Libelium 4-20ma device to connect to theses Siemens sensors. For sure the libelium board is not the complex.

    https://www.google.com/search?q=libelium+4-20&client=firefox-b-ab&source=lnms&tbm=isch&sa=X&ved=0ahUKEwigmbOI2sHbAhVDlJAKHRdBCLQQ_AUICigB&biw=1093&bih=482#imgrc=cbzOIBxvMb2TTM:

     

    Sensor:

    https://w3.siemens.com/mcms/sensor-systems/en/process-instrumentation/level-measurement-with-level-measuring-instruments/continuous/ultrasonic/transducers/pages/echomax-xps.aspx

     

    Control unit

      https://w3.siemens.com/mcms/sensor-systems/en/process-instrumentation/level-measurement-with-level-measuring-instruments/continuous/ultrasonic/controllers/Pages/MultiRanger-100-200.aspx

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • genebren
    genebren over 8 years ago in reply to s1buell

    Tom,

     

    In the article https://www.element14.com/community/external-link.jspa?url=https%3A%2F%2Fwww.sensorsmag.com%2Fcomponents%2Fimplementing-… , the circuit only uses a general purpose op-amp to perform the differential reading and the single ended power rail should work nicely with Arduino.  The shunt resistors are not that bad, it is just a matter of choosing as low a value as possible to get the voltage range you would like.  Going too high on the shunt resistor runs a risk of existing the drive or compliance voltage on the xmitter side (10K @ 20ma = 200V, which is most likely greater that the drive voltage, 5-28V).

     

    Looking at the Libelium devices, they are using jumpers on the receiver to manage the possibility that the xmitter is un-powered, so you could likely do the same.  I have used any thing from 100Ω to 200Ω (2 to 4V max across the resistor).

     

    Any generalize design will have a lot of variables when you are working with such an open protocol as 4-20mA loops.

    Good luck!

    Gene