Arduino Forum Tips on what sensor to use to measure lux levels?
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
  • Replies 4 replies
  • Subscribers 400 subscribers
  • Views 1479 views
  • Users 0 members are here
Related

Tips on what sensor to use to measure lux levels?

johnlarry
johnlarry over 6 years ago

Hello-

I have beginner level knowledge when it comes to Arduino, but I'm looking for a basic sensor that is able to measure lux levels when placed out in the sun. Eventually that data will be used to rotate a servo motor x amount of degrees based on variable lighting conditions.

Based on the small amount of research I've done so far, I've come across Sarkari Result Pnr Status

  • BH1750 Showbox
  • TSL2561

and I'm curious if anyone has experience with these sensors or is willing to add any recommendations.

Thanks in advance!

  • Sign in to reply
  • Cancel

Top Replies

  • fmilburn
    fmilburn over 6 years ago +5
    Hello John, I have used the TSL2561 and the Rohm RPR-0521RS with Arduino / Energia. I have not used the BH1750. My RoadTest of the RPR-0521 is here: Rohm Sensorshield Roadtest and I used the Rohm library…
  • Gough Lui
    Gough Lui over 6 years ago +5
    Be aware that some attenuation may be necessary. In my experience, some of the lux sensors are designed for integration into areas like smartphone mobile displays for auto-brightness feedback and will…
  • beacon_dave
    beacon_dave over 6 years ago +4
    There is a small Arduino based photometer project documented in this book: https://www.elektor.com/arduino-uno-45-projects-for-beginners-and-experts which may be of interest. It's just using an LDR and…
Parents
  • Gough Lui
    Gough Lui over 6 years ago

    Be aware that some attenuation may be necessary. In my experience, some of the lux sensors are designed for integration into areas like smartphone mobile displays for auto-brightness feedback and will not be able to handle full direct sun without saturating readings. A neutral density glass filter may be placed over the top of the sensor to extend its range.

     

    - Gough

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Gough Lui
    Gough Lui over 6 years ago

    Be aware that some attenuation may be necessary. In my experience, some of the lux sensors are designed for integration into areas like smartphone mobile displays for auto-brightness feedback and will not be able to handle full direct sun without saturating readings. A neutral density glass filter may be placed over the top of the sensor to extend its range.

     

    - Gough

    • Cancel
    • Vote Up +5 Vote Down