Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Arduno Code to C/C++ for LED Cube
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 415 subscribers
  • Views 1467 views
  • Users 0 members are here
  • led_cube
  • programming in c
  • led cube
  • c++ coding
  • 4x4_led_cube
Related

Arduno Code to C/C++ for LED Cube

dzuz
dzuz over 7 years ago

Does anyone know how to convert arduino code to c/c++?

 

I have made a 4x4x4 LED cube, but I need to have the code in c/c++, not just arduino code.

 

If anyone knows of a converter or can link a site to easily learn c/c++ on an arduino, that would be greatly appreciated. Thanks!

 

-Dan

  • Sign in to reply
  • Cancel

Top Replies

  • fmilburn
    fmilburn over 7 years ago +3
    Hi Daniel, Arduino code is C++ in an IDE with pin mapping and standard access to timers and other hardware features regardless of the microcontroller. There are also numerous libraries providing access…
Parents
  • fmilburn
    fmilburn over 7 years ago

    Hi Daniel,

     

    Arduino code is C++ in an IDE with pin mapping and standard access to timers and other hardware features regardless of the microcontroller.  There are also numerous libraries providing access to sensors, LEDs, motors and such. 

     

    So there is no conversion to C++ since it is already C++.  But it will be necessary to do all of the underlying register setting and library writing that an Arduino already provides.  In other words you will need to learn to implement basic C++ on a microcontroller - without this you will be lost.  It would be difficult to comment further without knowing the microcontroller you are using but my recommendation is to select one with good tutorials for getting started. You will need to learn how to use timers and set and change a gpio pin as a start. 

     

    Frank

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • fmilburn
    fmilburn over 7 years ago

    Hi Daniel,

     

    Arduino code is C++ in an IDE with pin mapping and standard access to timers and other hardware features regardless of the microcontroller.  There are also numerous libraries providing access to sensors, LEDs, motors and such. 

     

    So there is no conversion to C++ since it is already C++.  But it will be necessary to do all of the underlying register setting and library writing that an Arduino already provides.  In other words you will need to learn to implement basic C++ on a microcontroller - without this you will be lost.  It would be difficult to comment further without knowing the microcontroller you are using but my recommendation is to select one with good tutorials for getting started. You will need to learn how to use timers and set and change a gpio pin as a start. 

     

    Frank

    • Cancel
    • Vote Up +3 Vote Down