Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum USB to RS232
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 25 replies
  • Subscribers 417 subscribers
  • Views 4408 views
  • Users 0 members are here
Related

USB to RS232

s1buell
s1buell over 7 years ago

Does anyone here have any experience with this topic?

 

I`m going from a TUSB2077APTRTUSB2077APTR controller to two FT232RL-REELFT232RL-REEL IC`s just to test this prototype idea.

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 7 years ago in reply to s1buell +7
    Hello Tom, I quite like FPGAs - but then that's what I do quite a bit. If this is a commercial project I could help you with FPGA design for money ! If not, then I'll be able to help a bit on E14 with…
  • michaelkellett
    michaelkellett over 7 years ago +6
    It looks as if you want an Arduino with 8 RS232 ports. The neatest way to do this is to use an FPGA - something fairly small will do. You can connect the FPGA to the Arduino via UART or SPI at logic level…
  • beacon_dave
    beacon_dave over 7 years ago in reply to s1buell +5
    "The idea is to connect 7 RS232 connections. Then access them via Arduino (or similar type proto board) in the end." Perhaps take a look at the ATxmega A1U or A3U family of AVR 8-bit microcontroller which…
Parents
  • s1buell
    s1buell over 7 years ago
    • I wanted to start off with some simplicity and then evolve into a full industrial board.
    • I used the ATSAMD21G18 this processor is great (in my view) for IIOT applications
    • I love the sercom`s and the two internal DAC`s
    • I also made it Circuit Python capable (I think)

    The other idea I have is to componentize the architecture making easy to change processors or sensor communications  etc. That is why you see the power supplies very separate from the CPU

     

    After proving the concept, I will make it much more appealing to the eye. I like space and lots of test points when proving concepts 

     

     

    image

    image

    I did evolve it into a concept board already.... To much Coffee! (not produced). Need to prove the basics first.

    image

     

    That get your interest?

     

    Anyone work with this CPU before? I`m having a *** of a time with the boot loader and firmware?

     

    T

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to s1buell

    Hi Tom,

     

    Is it for production, or for others to self-assemble? The QFN package may be hard for others.

    It definitely needs some isolation, which could be done using (say) opto-isolators or relays. The board I'm working on is constrained in size, so it's only got two inputs and two outputs (using opto and relays in this case), but it's got an option to attach another board. It's described here at high-level, but full details and BoM will be published at some stage. It uses a Pi i.e. Cortex-A, and has the advantages and disadvantages of that, there's a market for Cortex-M controllers as you've noticed too.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 7 years ago in reply to s1buell

    Hi Tom,

     

    Is it for production, or for others to self-assemble? The QFN package may be hard for others.

    It definitely needs some isolation, which could be done using (say) opto-isolators or relays. The board I'm working on is constrained in size, so it's only got two inputs and two outputs (using opto and relays in this case), but it's got an option to attach another board. It's described here at high-level, but full details and BoM will be published at some stage. It uses a Pi i.e. Cortex-A, and has the advantages and disadvantages of that, there's a market for Cortex-M controllers as you've noticed too.