Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum USB to RS232
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 25 replies
  • Subscribers 417 subscribers
  • Views 4401 views
  • Users 0 members are here
Related

USB to RS232

s1buell
s1buell over 7 years ago

Does anyone here have any experience with this topic?

 

I`m going from a TUSB2077APTRTUSB2077APTR controller to two FT232RL-REELFT232RL-REEL IC`s just to test this prototype idea.

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 7 years ago in reply to s1buell +7
    Hello Tom, I quite like FPGAs - but then that's what I do quite a bit. If this is a commercial project I could help you with FPGA design for money ! If not, then I'll be able to help a bit on E14 with…
  • michaelkellett
    michaelkellett over 7 years ago +6
    It looks as if you want an Arduino with 8 RS232 ports. The neatest way to do this is to use an FPGA - something fairly small will do. You can connect the FPGA to the Arduino via UART or SPI at logic level…
  • beacon_dave
    beacon_dave over 7 years ago in reply to s1buell +5
    "The idea is to connect 7 RS232 connections. Then access them via Arduino (or similar type proto board) in the end." Perhaps take a look at the ATxmega A1U or A3U family of AVR 8-bit microcontroller which…
Parents
  • s1buell
    s1buell over 7 years ago

    You guys (anyone) interested in building an industrial CPU? I already have the proto board produced but I still have lots to do and extra eyes are always welcome.

     

    I would love some more experience on this one. 

     

    I really need someone to make me some firmware…. Lol

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • s1buell
    s1buell over 7 years ago

    You guys (anyone) interested in building an industrial CPU? I already have the proto board produced but I still have lots to do and extra eyes are always welcome.

     

    I would love some more experience on this one. 

     

    I really need someone to make me some firmware…. Lol

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • michaelkellett
    michaelkellett over 7 years ago in reply to s1buell

    Tell us a bit more - what processor, how many and what kind of IO.

     

    Shabaz is involved in similar project but I think he has already decided on RPI as thebrain.

     

    MK