Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum USB to RS232
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 25 replies
  • Subscribers 417 subscribers
  • Views 4411 views
  • Users 0 members are here
Related

USB to RS232

s1buell
s1buell over 7 years ago

Does anyone here have any experience with this topic?

 

I`m going from a TUSB2077APTRTUSB2077APTR controller to two FT232RL-REELFT232RL-REEL IC`s just to test this prototype idea.

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 7 years ago in reply to s1buell +7
    Hello Tom, I quite like FPGAs - but then that's what I do quite a bit. If this is a commercial project I could help you with FPGA design for money ! If not, then I'll be able to help a bit on E14 with…
  • michaelkellett
    michaelkellett over 7 years ago +6
    It looks as if you want an Arduino with 8 RS232 ports. The neatest way to do this is to use an FPGA - something fairly small will do. You can connect the FPGA to the Arduino via UART or SPI at logic level…
  • beacon_dave
    beacon_dave over 7 years ago in reply to s1buell +5
    "The idea is to connect 7 RS232 connections. Then access them via Arduino (or similar type proto board) in the end." Perhaps take a look at the ATxmega A1U or A3U family of AVR 8-bit microcontroller which…
Parents
  • s1buell
    s1buell over 7 years ago

    michaelkellett

     

    The first CPU project is just a project to test the CPU, create firmware etc. Its my first go at a cpu so I started with the basics (Just to play)

    The mian issue we are having now is the firmware. I`ve ordered a Atmel-ICE to start this part.

     

    I actually picked this processor mainly to work with circiut python and onboard memory storage. No more compiling. But the target was to make the CPU easy to program and for operations people to have access to the last code used (hence circuit python)

    https://en.wikipedia.org/wiki/CircuitPython

    https://github.com/adafruit/circuitpython

     

    image

     

    And the application of this unit will be more for IIOT sensor reading with long range data transmission.

    The STM32F407/417 looks is really nice! The price is also good $11.06000 Digikey. I will put this on my radar.

    • I have a ton of questions but need to do some reading on the cpu first.

     

    shabaz

    In the end it will be for production (If no one cancels the project.....again lol)

     

    Size is important but not a constraint for us (smaller the better). Im going to use 20pin connectors to allow for any type of expantion board to be added

     

    Here a picture of the concept:

    These have a two channel DAC to allow for 4-20ma boards to be added (concept picture only). Well its an actual PCB but untested.

     

    image

     

    Shabaz

     

    BTW love the project!!!!!   (https://www.element14.com/community/external-link.jspa?url=https%3A%2F%2Fmedium.com%2F%40shabaz_yousaf%2Fviki-an-open-so… )

     

    I would be interested in producing and playing with this project....

     

    We use a PI addon boad to connect to the PI`s only for reading sensors and a little control if needed (basic stuff)

     

    T

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • s1buell
    s1buell over 7 years ago

    michaelkellett

     

    The first CPU project is just a project to test the CPU, create firmware etc. Its my first go at a cpu so I started with the basics (Just to play)

    The mian issue we are having now is the firmware. I`ve ordered a Atmel-ICE to start this part.

     

    I actually picked this processor mainly to work with circiut python and onboard memory storage. No more compiling. But the target was to make the CPU easy to program and for operations people to have access to the last code used (hence circuit python)

    https://en.wikipedia.org/wiki/CircuitPython

    https://github.com/adafruit/circuitpython

     

    image

     

    And the application of this unit will be more for IIOT sensor reading with long range data transmission.

    The STM32F407/417 looks is really nice! The price is also good $11.06000 Digikey. I will put this on my radar.

    • I have a ton of questions but need to do some reading on the cpu first.

     

    shabaz

    In the end it will be for production (If no one cancels the project.....again lol)

     

    Size is important but not a constraint for us (smaller the better). Im going to use 20pin connectors to allow for any type of expantion board to be added

     

    Here a picture of the concept:

    These have a two channel DAC to allow for 4-20ma boards to be added (concept picture only). Well its an actual PCB but untested.

     

    image

     

    Shabaz

     

    BTW love the project!!!!!   (https://www.element14.com/community/external-link.jspa?url=https%3A%2F%2Fmedium.com%2F%40shabaz_yousaf%2Fviki-an-open-so… )

     

    I would be interested in producing and playing with this project....

     

    We use a PI addon boad to connect to the PI`s only for reading sensors and a little control if needed (basic stuff)

     

    T

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • shabaz
    shabaz over 7 years ago in reply to s1buell

    Hi Tom,

     

    That makes sense, the dual-module approach looks neat.

    Also, it's great to hear you find the VIKI project interesting. it should just be a matter of weeks and then we'll hopefully have the documentation, BoM, etc published.