Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum USB to RS232
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 25 replies
  • Subscribers 417 subscribers
  • Views 4411 views
  • Users 0 members are here
Related

USB to RS232

s1buell
s1buell over 7 years ago

Does anyone here have any experience with this topic?

 

I`m going from a TUSB2077APTRTUSB2077APTR controller to two FT232RL-REELFT232RL-REEL IC`s just to test this prototype idea.

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 7 years ago in reply to s1buell +7
    Hello Tom, I quite like FPGAs - but then that's what I do quite a bit. If this is a commercial project I could help you with FPGA design for money ! If not, then I'll be able to help a bit on E14 with…
  • michaelkellett
    michaelkellett over 7 years ago +6
    It looks as if you want an Arduino with 8 RS232 ports. The neatest way to do this is to use an FPGA - something fairly small will do. You can connect the FPGA to the Arduino via UART or SPI at logic level…
  • beacon_dave
    beacon_dave over 7 years ago in reply to s1buell +5
    "The idea is to connect 7 RS232 connections. Then access them via Arduino (or similar type proto board) in the end." Perhaps take a look at the ATxmega A1U or A3U family of AVR 8-bit microcontroller which…
Parents
  • phoenixcomm
    phoenixcomm over 7 years ago

    s1buell Tom, cool problem. Because everybody has thrown there 2 cents in I will toss mine into the ring. First I don't think that your Arduino could ever handle 8 UARTs full speed. I don't think that USB will work (again speed issues),

    first, remember that a URART is an 8-bit device with two registers, and the IO side of the gear you will need TTL to RS232 chip like a MAX back to the computer side of the world. all of the data lines are run in parallel between the USARTs and your CPU now. then you take the 8 interrupt lines and put them through an 8 to BCD encoder. As well as OR tieing them together to your interrupt pin.  the software looks at the interrupt pin, when it comes in it reads the URART address and gate the data on to the data bus and then read it. Here is a neet TI dual UART TL16C2752. Its package is a RHB 32 or QVFN 5mm x 5mm.

    Good Luck

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • phoenixcomm
    phoenixcomm over 7 years ago

    s1buell Tom, cool problem. Because everybody has thrown there 2 cents in I will toss mine into the ring. First I don't think that your Arduino could ever handle 8 UARTs full speed. I don't think that USB will work (again speed issues),

    first, remember that a URART is an 8-bit device with two registers, and the IO side of the gear you will need TTL to RS232 chip like a MAX back to the computer side of the world. all of the data lines are run in parallel between the USARTs and your CPU now. then you take the 8 interrupt lines and put them through an 8 to BCD encoder. As well as OR tieing them together to your interrupt pin.  the software looks at the interrupt pin, when it comes in it reads the URART address and gate the data on to the data bus and then read it. Here is a neet TI dual UART TL16C2752. Its package is a RHB 32 or QVFN 5mm x 5mm.

    Good Luck