Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum USB to RS232
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 25 replies
  • Subscribers 417 subscribers
  • Views 4387 views
  • Users 0 members are here
Related

USB to RS232

s1buell
s1buell over 7 years ago

Does anyone here have any experience with this topic?

 

I`m going from a TUSB2077APTRTUSB2077APTR controller to two FT232RL-REELFT232RL-REEL IC`s just to test this prototype idea.

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 7 years ago in reply to s1buell +7
    Hello Tom, I quite like FPGAs - but then that's what I do quite a bit. If this is a commercial project I could help you with FPGA design for money ! If not, then I'll be able to help a bit on E14 with…
  • michaelkellett
    michaelkellett over 7 years ago +6
    It looks as if you want an Arduino with 8 RS232 ports. The neatest way to do this is to use an FPGA - something fairly small will do. You can connect the FPGA to the Arduino via UART or SPI at logic level…
  • beacon_dave
    beacon_dave over 7 years ago in reply to s1buell +5
    "The idea is to connect 7 RS232 connections. Then access them via Arduino (or similar type proto board) in the end." Perhaps take a look at the ATxmega A1U or A3U family of AVR 8-bit microcontroller which…
Parents
  • shabaz
    shabaz over 7 years ago

    Hi,

     

    I'm not sure those two together will meet your requirement.

    You've posted in the Arduino space, are you looking to attach the Arduino serial pins to a PC via USB?

    If so, then the functionality you need is just a USB-to-UART chip.

     

    If you're looking to attach the Arduino serial pins to a RS232 device, then USB is not required, just a 'RS232 transceiver' chip.

     

    If it is completely unrelated to Arduino and you're looking to create some adapter to connect a PC to a RS232 device then the functionality you need is a USB to UART chip, and a RS232 transceiver chip.

    If you want two RS232 interfaces, a dual UART USB chip can be used (no need for a USB hub chip). and the RS232 transceiver chip(s).

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • s1buell
    s1buell over 7 years ago in reply to shabaz

    Ok....

     

     

     

    The idea is to connect 7 RS232 connections. Then access them via Arduino (or similar type proto board) in the end.

     

    I`m just starting with two channels for  testing. USB ---> TUSB2077APTRTUSB2077APTR-> FT232RL-REELFT232RL-REEL ---> ADM213EARUZADM213EARUZ 

     

    In the end I would like to have Arduino --> TUSB2077APTRTUSB2077APTR->  FT232RL-REELFT232RL-REEL ---> ADM213EARUZADM213EARUZ

     

    Now one thing to keep in mind each channel requires a separate ground so I will only have one channel per set ( FT232RL-REELFT232RL-REEL and ADM213EARUZADM213EARUZ)

     

    Does this help?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to s1buell

    Hi Tom,

     

    If it's possible to sketch what you wish to do (and specify the end equipment and purpose too) it will make it easier to follow, rather than specifying parts, because then I need to go looking at what each part does.

    The Arduino isn't a USB host, so it cannot attach to a hub to connect out to USB devices.  The Arduino plays a USB device role, not a host role (and technically not even that - the embedded programmer/debugger on the Arduino is the thing that is playing the USB device role).

    Unless you're using some unusual Arduino that I'm not aware of (I'm assuming Arduino Uno, but there are hundreds of Arduino variants/copies out there, so I'm not sure).

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • s1buell
    s1buell over 7 years ago in reply to s1buell

    Guy`s let me get back to you on this.

     

     

    The first test we did was Arduino to USB proto board then into a 8 channel RS232 hub and everything worked great. We could read all the RS232 data from all channels.

     

    Now for me the request is to make a shield to connect direct to the Arduino proto board. Let me check.

     

    Thanks for the responces

     

    T

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • s1buell
    s1buell over 7 years ago in reply to s1buell

    Guy`s let me get back to you on this.

     

     

    The first test we did was Arduino to USB proto board then into a 8 channel RS232 hub and everything worked great. We could read all the RS232 data from all channels.

     

    Now for me the request is to make a shield to connect direct to the Arduino proto board. Let me check.

     

    Thanks for the responces

     

    T

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • mp2100
    mp2100 over 7 years ago in reply to s1buell

    If I understand, you've used a hub something like this (easysync) device, except you want 8 ports ?  I've use this previously, with good results.

    image

    It's been a while since I opened this up, I can look into my parts bin and tell you what chip is inside that does the 'magic' converting 1 USB into multiple RS232.  I think it was an FTDI chip, which is  common.  https://www.ftdichip.com/

    • Cancel
    • Vote Up +3 Vote Down