Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Digital volume control
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 415 subscribers
  • Views 3513 views
  • Users 0 members are here
  • audio
  • app
  • arduino
  • Speakers
Related

Digital volume control

ctucht16
ctucht16 over 7 years ago

Hello every one I have a project I would like to try at work. We have an old radio at one bench and speakers running to every other bench. The volume is a pain to change. I thought what if I built an app that every one can change the volume individualy on our own workstations. I tried doing some reading on digital pots but I'm still lost in the sauce and am in serrious need of help.

 

So I need something to controll the speakers and design the app to controll the speakers from multiple computers on a network.

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 7 years ago +2
    Wow, I'm not sure I could work with a speaker nearby that I couldn't easily turn down/switch off at times. If you're just interested in productivity and want to have a quick solution, consider something…
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to Jan Cumps +1
    One of the possibilities is digital programmable logarithmic potentiometers, e.g.: https://www.analog.com/media/en/news-marketing-collateral/product-selection-guide/Choosing_the_Correct_Digipot.pdf If…
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to shabaz +1
    shabaz wrote: .... but I don't know what power level the amp operates at, ‘.. 30 Watt per channel. It’s a serious kit.
Parents
  • shabaz
    shabaz over 7 years ago

    Wow, I'm not sure I could work with a speaker nearby that I couldn't easily turn down/switch off at times.

    If you're just interested in productivity and want to have a quick solution, consider something like this 12-way rotary switch12-way rotary switch

    and lots of 10 ohm resistors (probably 1/2W ones should be fine, but I don't know what power level the amp operates at, so you may wish to go for (say) 1W resistors for some of them).

    Not the same as a remote-controlled app, but maybe quicker to assemble, connected directly to the speaker connections on your desk.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • ctucht16
    ctucht16 over 7 years ago in reply to shabaz

    Thank you but its not a fix I need quick its more of a project I want to try.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • billpenner
    billpenner over 7 years ago in reply to ctucht16

    Question. Do you want the volume controls at the amplifier or at each speaker.

    If at each speaker, google "speaker volume controls" there many to choose from.

    Impedance matching is probably necessary unless you are using low wattage speakers

    in which case, a simple low wattage wire wound potentiometer might work.

    These methods would require the Max volume to be set at the amplifier with the individual controls set at 0 Ohms

    each station could then reduce the volume as needed. the value of pots would need to be selected so as to allow desired volume reduction.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • billpenner
    billpenner over 7 years ago in reply to ctucht16

    Question. Do you want the volume controls at the amplifier or at each speaker.

    If at each speaker, google "speaker volume controls" there many to choose from.

    Impedance matching is probably necessary unless you are using low wattage speakers

    in which case, a simple low wattage wire wound potentiometer might work.

    These methods would require the Max volume to be set at the amplifier with the individual controls set at 0 Ohms

    each station could then reduce the volume as needed. the value of pots would need to be selected so as to allow desired volume reduction.