Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum I can't sample analog input signal to ardiuno uno for higher frequency . I am unable to read analog input signal with delay less than 4 milliseconds.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 414 subscribers
  • Views 727 views
  • Users 0 members are here
  • delay_timer
  • ac voltage sampling
  • ardiuno
Related

I can't sample analog input signal to ardiuno uno for higher frequency . I am unable to read analog input signal with delay less than 4 milliseconds.

rajivkr
rajivkr over 7 years ago

I am working on a project to read the analog signal from the input port of Arduino and print it to serial monitor i am unable to read the input signal with delay less than 4 ms, it works with delay higher than 4 ms .

  • Sign in to reply
  • Cancel

Top Replies

  • aspork42
    aspork42 over 7 years ago +2
    Another thought - You could run some tests - create a sample sketch to JUST read the ADC say, 10,000 times and see how long it takes to execute. Don't print anything to the serial port during that time…
  • dougw
    dougw over 7 years ago +1
    The UNO can sample the ADC at over 9,000 Hz, so the problem is not the A/D converter. The serial port may have a baud rate that is too slow to send data this quickly. At 9,600 baud the serial port sends…
  • dougw
    dougw over 7 years ago

    The UNO can sample the ADC at over 9,000 Hz, so the problem is not the A/D converter.

    The serial port may have a baud rate that is too slow to send data this quickly.

    At 9,600 baud the serial port sends about 1 byte per millisecond.

    At 115,200 baud it can send about 12 bytes per millisecond.

    If you need to go faster, you could try SPI.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • aspork42
    aspork42 over 7 years ago

    Another thought - You could run some tests - create a sample sketch to JUST read the ADC say, 10,000 times and see how long it takes to execute. Don't print anything to the serial port during that time. That could tell you if the serial port is slowing you down.

     

    You could then also set up your code to only print periodically to the serial port - say only when the value changes by a certain amount; and also every 1-200 ms.

     

    I also found this article that may have some stuff that helps you: https://forum.arduino.cc/index.php?topic=6549.0