Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum I can't sample analog input signal to ardiuno uno for higher frequency . I am unable to read analog input signal with delay less than 4 milliseconds.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 414 subscribers
  • Views 727 views
  • Users 0 members are here
  • delay_timer
  • ac voltage sampling
  • ardiuno
Related

I can't sample analog input signal to ardiuno uno for higher frequency . I am unable to read analog input signal with delay less than 4 milliseconds.

rajivkr
rajivkr over 7 years ago

I am working on a project to read the analog signal from the input port of Arduino and print it to serial monitor i am unable to read the input signal with delay less than 4 ms, it works with delay higher than 4 ms .

  • Sign in to reply
  • Cancel

Top Replies

  • aspork42
    aspork42 over 7 years ago +2
    Another thought - You could run some tests - create a sample sketch to JUST read the ADC say, 10,000 times and see how long it takes to execute. Don't print anything to the serial port during that time…
  • dougw
    dougw over 7 years ago +1
    The UNO can sample the ADC at over 9,000 Hz, so the problem is not the A/D converter. The serial port may have a baud rate that is too slow to send data this quickly. At 9,600 baud the serial port sends…
Parents
  • dougw
    dougw over 7 years ago

    The UNO can sample the ADC at over 9,000 Hz, so the problem is not the A/D converter.

    The serial port may have a baud rate that is too slow to send data this quickly.

    At 9,600 baud the serial port sends about 1 byte per millisecond.

    At 115,200 baud it can send about 12 bytes per millisecond.

    If you need to go faster, you could try SPI.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dougw
    dougw over 7 years ago

    The UNO can sample the ADC at over 9,000 Hz, so the problem is not the A/D converter.

    The serial port may have a baud rate that is too slow to send data this quickly.

    At 9,600 baud the serial port sends about 1 byte per millisecond.

    At 115,200 baud it can send about 12 bytes per millisecond.

    If you need to go faster, you could try SPI.