Arduino Forum MQTT client program not showing any results with Arduino
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
  • Replies 49 replies
  • Subscribers 405 subscribers
  • Views 4558 views
  • Users 0 members are here
Related

MQTT client program not showing any results with Arduino

Former Member
Former Member over 10 years ago

I modified the MQTT example present under MQTT library pubsubclient for Arduino.

My MQTT server address is 192.168.1.6 with port 8081.

To this MQTT server,another MQTT client in my mobile is able to connect.

But this is not working with Arduino.There is no error shown during compilation or during uploading.

Infact,I am not able to see the connection result messages such as "Connected" or "Not connected" which i given in Serial.println() in setup function.

I am resetting Arduino before uploading the program.Please let me know why this is not showing any output....

 

#include <SPI.h>

#include <Ethernet.h>

#include <PubSubClient.h>

// Update these with values suitable for your network.

byte mac[]    = {  0xDE, 0xED, 0xBA, 0xFE, 0xFE, 0xED };

byte server[] = {192, 168, 1, 6 };

//byte ip[]     = { 172, 16, 0, 100 };

 

 

void callback(char* topic, byte* payload, unsigned int length) {

  // handle message arrived

}

EthernetClient ethClient;

PubSubClient client(server, 8081, callback, ethClient);

void setup()

{

  Ethernet.begin(mac);

  if (client.connect("*")) {

     Serial.begin(9600);

    Serial.println("Connected to MQTT Server");

    client.publish("outTopic","hello world");

   // client.subscribe("inTopic");

  }

  else

  {

   Serial.println("Could not connect to MQTT Server");

  }

}

void loop()

{

  //client.loop();

 

}

  • Sign in to reply
  • Cancel

Top Replies

  • neilk
    neilk over 10 years ago in reply to Former Member +3
    generk4 and organtin Hi Radhamani and Giovanni - I had 30 minutes to spare so I copied the program from comment 19 and posted it into the Arduino IDE (I am using 1.6.1), compiled and uploaded it to a genuine…
  • Former Member
    Former Member over 10 years ago +3
    Hi Bob, Neil and Clem, I tried LM35 Temperature sensor with MQTT Arduino sketch and it works fine for me I am sooo happy Thanks once again for your wonderful support and help
  • Former Member
    Former Member over 10 years ago in reply to bobcroft +2
    Hi bob,Neil,Clem and many others who have helped and guided me in this issue, I have successfully completed MQTT program and Arduino is successfully publishing and subscribing messages Next step,I am going…
Parents
  • bobcroft
    bobcroft over 10 years ago

    Radhamani,

                             you do not appear to have set an IP address for your Ethernet shield and you do not appear to be using DHCP to get an IP address.  So you are not sending anything to the MQTT server.  You can prove whether or not your   Ethernet card / shield is working once you have an IP address by either 'pinging' from a Windows 'cmd' line.  Type cmd in the Windows search box, this will bring up cmd.exe, click on that to bring up the command window and in the window type "ping 192.168.1.xx" Do not type the ""  and enter your own IP address at xx.

     

    Hope that helps

     

    Bob

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 10 years ago in reply to bobcroft

    bobcroft is right. Look at Ethernet.begin(mac); and change appropriately. Further along, your callback does not handle any messages! This looks like skeleton code at best.


    Cheers,

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 10 years ago in reply to clem57

    Hi Clem,I am just doing basic setup of Ethernet configuration in this sketch.Hence,I hope callback is not required at this stage..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 10 years ago in reply to clem57

    Hi Clem,I am just doing basic setup of Ethernet configuration in this sketch.Hence,I hope callback is not required at this stage..