Arduino Forum Arduino timer issues
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
  • State Verified Answer
  • Replies 7 replies
  • Answers 1 answer
  • Subscribers 403 subscribers
  • Views 624 views
  • Users 0 members are here
Related

Arduino timer issues

Former Member
Former Member over 12 years ago

Hi Gurus

 

I am a first time Arduino user and  have had no experience with code writing at all and have decided to start learning, so this is my first sketch. I want to turn on an LED with the push of a button then delay the LED turning off, I have it functioning but the off delay period is not the same with each release of the button. Due to my lack of knowledge on writing code I need a little help with solving the problem which is driving me mad

 

I Have attached a copy of my code for you experts to look at (don't laugh)

 

Any help / guidance would be greatly appreciated

 

Thanks again

Lincoln

  • Sign in to reply
  • Cancel

Top Replies

  • billabott
    billabott over 12 years ago in reply to Former Member +1
    No Problem. The circuit diagram calls for using a pull down resistor. On rare occassions, it is possible run into a resistor that has an internal intermittant open. Otherwise, I don't know without seeing…
  • kjhart0133
    kjhart0133 over 12 years ago +1 verified
    Lincoln, I sent you a private message with some info. Let me know if you have any trouble reading it. Kevin H.
Parents
  • kjhart0133
    0 kjhart0133 over 12 years ago

    Lincoln ,

     

    Welcome to the world of Arduino. 

     

    To address your question: first, do you want to start timing the LED turnoff time from the moment you initially depress the switch, or from the moment you release the switch?  Second, in either case you will have to debounce the switch in order to get a consistent delay time.  Go to http://playground.arduino.cc//Code/Bounce for an excellent library that handles switch debounce.  Look at the example code at the end of the page and study the various "methods."  Soon you'll figure out how it works.

     

    Lastly, are you using the delay() function to time when to turn off the LED?  This is probably the simplest way to do it.  Just remember, though, delay() doesn't play well with one or more of the explicitly programmable timers or with interrupts.  Look at the Blink program for how to turn on and off an LED with a delay.

     

    Kevin H.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • kjhart0133
    0 kjhart0133 over 12 years ago

    Lincoln ,

     

    Welcome to the world of Arduino. 

     

    To address your question: first, do you want to start timing the LED turnoff time from the moment you initially depress the switch, or from the moment you release the switch?  Second, in either case you will have to debounce the switch in order to get a consistent delay time.  Go to http://playground.arduino.cc//Code/Bounce for an excellent library that handles switch debounce.  Look at the example code at the end of the page and study the various "methods."  Soon you'll figure out how it works.

     

    Lastly, are you using the delay() function to time when to turn off the LED?  This is probably the simplest way to do it.  Just remember, though, delay() doesn't play well with one or more of the explicitly programmable timers or with interrupts.  Look at the Blink program for how to turn on and off an LED with a delay.

     

    Kevin H.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer