Arduino Forum Reading analog values Arduino
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
  • State Verified Answer
  • Replies 11 replies
  • Answers 2 answers
  • Subscribers 402 subscribers
  • Views 1970 views
  • Users 0 members are here
  • arduino
  • analog
  • sensor
Related

Reading analog values Arduino

Former Member
Former Member over 12 years ago

Hello everyone,

 

Currently I am working a project..I have 8x8  piezoresistive sensor matrix (i simply used 2 muxs) and I have only 1 analog output that gives me 64 different voltage values (changes depending on the pressure,and its between 2.5 V -5V) for each scan..so what i want to do is,to scan the matrix 10 times and get the averaged values of each cell of the matrix called smoothing..I do know how to do it for single readings but as i mentioned above I get 64 values..so somehow for each loop i have to store 64 values each time and smooth the data..Here what I have wrote..

 


const int numReadings = 64;           // Number of readings for each scan
const int numLoop=10;                   //Number of loops for each scan
float readings[numReadings];         // the readings from the analog input after each scan
float totReadings[numLoop];         //total readings from the analog input  scan
int   index_readings = 0;              // the index of the current reading
int   index_loop=0;                      // the index of the current loop

float average[numReadings];       //Averaged value

int   total[numReadings][numLoop];

 

int inputPin = A0;                     //Determine the pin

void setup()
{
   Serial.begin(9600);                  
  // initialize all the readings
  for (int i = 0; i < numReadings; i++)
  readings[i] = 0; 
  // initialize all the loops
  for(int j=0; j<numLoop;j++)
  totReadings[j]=0;
}
void loop() {
 
  // read from the sensor: 


  totReadings[numLoop]=totReadings[numLoop]+readings[index_readings];

 

  readings[index_readings] = analogRead(inputPin);  //Read the data from sensor (64 values)
 
  // advance to the next position in the array: 
  index_readings = index_readings + 1;

 

  index_loop = index_loop + 1;   
 
  // if we're at the end of the array...
  if (index_readings >= numReadings)             
    // ...wrap around to the beginning:
    index_readings = 0;  
   
  if (index_loop >= numLoop)             
    // ...wrap around to the beginning:
  index_loop = 0;
 
  //Take the average value
  average[numReadings]=totReadings[numLoop]/numLoop;  //Averaged value divided by 10(number of loops)

  Serial.println(average[numReadings]);                              //Print the averaged value 64x1
  delay(100);

 

}
  }
    }

 

image

I havent tested it yet but I do not feel satisfied though..I would be grateful to you if you can give me some ideas for improvement..Thanks a lot in advance..

  • Sign in to reply
  • Cancel

Top Replies

  • billabott
    billabott over 12 years ago +1
    The ADC is 10 bits of resolution. 2^10=1024. You have thrown away half of your range: 0 to 2.5 volts. Consider doing something to correct that. At some point you will divide by 10 > 8 =2^3. So, the lower…
Parents
  • Former Member
    0 Former Member over 12 years ago

    Hello everyone again;)

     

    So any other recommendation or ideas?

     

    Thanks..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • billabott
    0 billabott over 12 years ago in reply to Former Member

    Are you wanting to do the computed average for samples sets 1..10 and then a separate computed average for sample sets 11..20, etc?    Or are looking to have a sliding window on the data input stream so you can compute the average for arbitrary sample sets x..x+9?   

     

    Can you add more comments to you code?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 12 years ago in reply to billabott

    actually not..let me make it clearer.--my sensor output gives 64 different voltage values for each loop. [its a sensor matrix 8*8 , 8 rows and 8 columns..i used 2 counter with different speed so that i can scan the whole matrix--after 1 scan i will get 64 different values 64x1] ..I want to make 10 loops[ 10 scans] and show the averaged value at the end..I have put the image in the previous answer..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 12 years ago in reply to billabott

    actually not..let me make it clearer.--my sensor output gives 64 different voltage values for each loop. [its a sensor matrix 8*8 , 8 rows and 8 columns..i used 2 counter with different speed so that i can scan the whole matrix--after 1 scan i will get 64 different values 64x1] ..I want to make 10 loops[ 10 scans] and show the averaged value at the end..I have put the image in the previous answer..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer