Arduino Forum Reading analog values Arduino
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
  • State Verified Answer
  • Replies 11 replies
  • Answers 2 answers
  • Subscribers 402 subscribers
  • Views 1985 views
  • Users 0 members are here
  • arduino
  • analog
  • sensor
Related

Reading analog values Arduino

Former Member
Former Member over 12 years ago

Hello everyone,

 

Currently I am working a project..I have 8x8  piezoresistive sensor matrix (i simply used 2 muxs) and I have only 1 analog output that gives me 64 different voltage values (changes depending on the pressure,and its between 2.5 V -5V) for each scan..so what i want to do is,to scan the matrix 10 times and get the averaged values of each cell of the matrix called smoothing..I do know how to do it for single readings but as i mentioned above I get 64 values..so somehow for each loop i have to store 64 values each time and smooth the data..Here what I have wrote..

 


const int numReadings = 64;           // Number of readings for each scan
const int numLoop=10;                   //Number of loops for each scan
float readings[numReadings];         // the readings from the analog input after each scan
float totReadings[numLoop];         //total readings from the analog input  scan
int   index_readings = 0;              // the index of the current reading
int   index_loop=0;                      // the index of the current loop

float average[numReadings];       //Averaged value

int   total[numReadings][numLoop];

 

int inputPin = A0;                     //Determine the pin

void setup()
{
   Serial.begin(9600);                  
  // initialize all the readings
  for (int i = 0; i < numReadings; i++)
  readings[i] = 0; 
  // initialize all the loops
  for(int j=0; j<numLoop;j++)
  totReadings[j]=0;
}
void loop() {
 
  // read from the sensor: 


  totReadings[numLoop]=totReadings[numLoop]+readings[index_readings];

 

  readings[index_readings] = analogRead(inputPin);  //Read the data from sensor (64 values)
 
  // advance to the next position in the array: 
  index_readings = index_readings + 1;

 

  index_loop = index_loop + 1;   
 
  // if we're at the end of the array...
  if (index_readings >= numReadings)             
    // ...wrap around to the beginning:
    index_readings = 0;  
   
  if (index_loop >= numLoop)             
    // ...wrap around to the beginning:
  index_loop = 0;
 
  //Take the average value
  average[numReadings]=totReadings[numLoop]/numLoop;  //Averaged value divided by 10(number of loops)

  Serial.println(average[numReadings]);                              //Print the averaged value 64x1
  delay(100);

 

}
  }
    }

 

image

I havent tested it yet but I do not feel satisfied though..I would be grateful to you if you can give me some ideas for improvement..Thanks a lot in advance..

  • Sign in to reply
  • Cancel

Top Replies

  • billabott
    billabott over 12 years ago +1
    The ADC is 10 bits of resolution. 2^10=1024. You have thrown away half of your range: 0 to 2.5 volts. Consider doing something to correct that. At some point you will divide by 10 > 8 =2^3. So, the lower…
Parents
  • billabott
    0 billabott over 12 years ago

    readings[index_readings] = analogRead(inputPin); //Read the data from sensor (64 values)

     

    // advance to the next position in the array:
    index_readings = index_readings + 1;

     

    The above is not how arduino code works.

    Using a nested loop structure is required.

     

    for (i =0; i < numLoop; i++;)

    {

         for (j=0; j < numReadings; j++)

         {

              readings[i,j] = analogRead(inputPin);     // opt to >>3  which is /8 if going that way

              // possible other i/o or calc here

         }

    }

        

        

     

     

    http://arduino.cc/en/Reference/For

     

    for (initialization; condition; increment) {

     

    //statement(s);

     

    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 12 years ago in reply to billabott

    Hello Billabott;

     

    Thank for your reply.. I modified the codes a bit..

     


    float readings[64];                    // the readings from the analog input after each scan
    float totReadings[10];               //total readings from the analog input  scan
    int i = 0;                                // the index of the current reading
    int j=0;                                   // the index of the current loop
    float average[64];                     //Averaged value
    int inputPin = A0;                     //Determine the pin

    void setup()
    {
    Serial.begin(9600);                  
    }
    void loop() {
       // initialize all the readings
      for (int i = 0; i < 64; i++)
      // initialize all the loops
      for(int j=0; j<10;j++)
      // read from the sensor: 
     
      totReadings[i,j]=totReadings[i,j]+ readings[i];
      readings[i] = analogRead(inputPin);  //Read the data from sensor (64 values)
      
      //Take the average value
      average[64]=totReadings[i,j]/j;                        //Averaged value divided by 10(number of loops)

      Serial.println(average[64]);                              //Print the averaged value 64x1

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • billabott
    0 billabott over 12 years ago in reply to Former Member

    Great!   But you need for use the curly braces open and close, { } ,to control the range of the for statements.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • billabott
    0 billabott over 12 years ago in reply to Former Member

    Great!   But you need for use the curly braces open and close, { } ,to control the range of the for statements.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 12 years ago in reply to billabott

    Hello again,

     

    I have noticed some mistakes..and marked them using arrow..

     

     

    float readings[64];                 // the readings from the analog input after each scan

    float totReadings[10];           //total readings from the analog input scan                                 -->>>one dimension array but below i used it as 2-dim array??

    int i = 0;                            // the index of the current reading

    int j=0;                            // the index of the current loop

    float average[64];            //Averaged value                                                                           -->>here must be 63..becoz i have 64 values..0...63 ??

    int inputPin = A0;          //Determine the pin

    void setup()
    {
    Serial.begin(9600);
    }
    void loop() {
    // initialize all the readings
    for (int i = 0; i < 64; i++)

    {

    for(int j=0; j<10;j++)

    {
    // read from the sensor:

     

    totReadings[i,j]=totReadings[i,j]+ readings[i];               //               --->>>>> here i have used totReadings as two-dimensional array ??
    readings[i] = analogRead(inputPin); //Read the data from sensor (64 values)

     

    //Take the average value
    average[64]=totReadings[i,j]/j;                                    //Averaged value divided by 10(number of loops)   

    Serial.println(average[64]);                                         //Print the averaged value 64x1

     

    }

    }

    }