Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino | The MKR Contest Series: Show Us How You Would Use the Arduino MKR Line!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 402 subscribers
  • Views 2344 views
  • Users 0 members are here
Related

Arduino | The MKR Contest Series: Show Us How You Would Use the Arduino MKR Line!

tariq.ahmad
tariq.ahmad over 7 years ago
image

Arduino Home

An Open-Source platform to create digital devices and interactive objects that sense and control physical devices.

Arduino Tutorials
Arduino Projects

 

MKR Giveways and Upcoming Livestream Series on MKR with Massimo Banzi Cofounder of Arduino!

 

Over the next 3 months we're going to be running a series of mini contests to encourage community members to repurpose their existing Arduino projects using the new MKR line.  Or to do new projects that demonstrates how an engineer would use the new MKR Line in their projects.

 

Current Contests:

 

Auto Hacks and Beyond with the MKR WiFi 1010 Board and CAN Shield
Winners Announcement: Auto Hacks and Beyond: Show Us How You Would Use the Arduino MKR WiFi 1010 Board and CAN Shield!

Arduino MKR WiFi 1010 Board

Arduino MKR CAN Shield

imageimage
Buy NowBuy NowBuy NowBuy Now

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

The MKR WIFI 1010 is equipped with an ESP32 module from U-BLOX. It speeds up and simplifies prototyping of WiFi based IoT  It aims to speed up and simplify the prototyping of WiFi based IoT applications using the ESP32 module and low power consumption. The board is composed of three main blocks:

  • SAMD21 Cortex-M0+ 32bit Low Power ARM MCU;
  • U-BLOX NINA-W10 Series Low Power 2.4GHz IEEERegistered 802.11 b/g/n Wi-Fi
  • ECC508 Crypto Authentication

The MKR WIFI 1010 includes 32-bit computational power, a rich set of I/O interfaces, and low power Wi-Fi with a Cryptochip for secure communication using SHA-256 encryption.

 

The Arduino Software (IDE) simplifies code development and programming. Ideal for IoT battery-powered projects in a compact form.

 

Its USB port can be used to supply power (5V) to the board. It has a Li-Po charging circuit that allows the Arduino MKR WIFI 1010 to run on battery power or an external 5 volt source, charging the Li-Po battery while running on external power. Switching from one source to the other is done automatically.

With this shield you can easily connect to a CAN (Controller Area Network) Bus. Discover new possibilities of interaction between your Arduino MKR Board and the CAN ecosystem.

 

The MKR CAN shield can simplify the connection of the MKR boards with industrial systems and especially with automotive applications.

 

This shield opens a new set of possible applications like smart vehicles, autonomous cars and drones. A CAN connection also provides the possibility to connect a MKR board directly with several types of industrial grade sensors, motors and displays.

 

The MKR CAN shield allows a MKR board to connect to the CAN bus using the MCP2515 SPI to CAN chip.

 

The Arduino MKR CAN Shield uses the MCP2515 chip by Microchip. This chip is an industry standard.

 

The switch close to the CAN bus connector allows to enable or disable the termination resistor.

 

Arduino MKR WiFi 1010 Pinout, SAMD21 Pin Mapping, Tech Specs, EAGLE Files, Github, Schematics, Reference Links, FAQ, and More!

 

Submission Deadline:

 

Submit Ideas until October 8th. 

 

On October 15th we'll have a Winners Announcement and send out the board and shield to repurpose an existing project or do a new project! 

 

 

 

Project14:  Clustered MCUs
Project14 | Clustered MCUs:  Anything Goes with Two or More MCUs!Clustered MCUs
imageimage
Buy NowBuy NowBuy NowBuy Now

The kit is based around the MKR1000—a powerful board that combines the functionality of the Zero and the Wi-Fi Shield—and enables Makers to add connectivity to their designs with minimal prior networking experience.

 

Each bundle includes: 1 Arduino MKR1000 board, with header soldered. 1 micro USB cable, 1 400-point breadboard, 70 solid-core jumper wires, 1 9V battery snap, 1 stranded jumper wire, 6 phototransistors, 3 potentiometers (10 kilohm),10 pushbuttons,1 temperature sensor (TMP36),1 tilt sensor, 1 alphanumeric LCD (16 x 2 characters), 1 bright white, 34 LEDs (1 bright white, 1 RGB, 8 red, 8 green, 8 yellow, 3 blue), 1 small DC motor (6/9V), 1 small servo motor, 1 piezo capsule (PKM17EPP-4001-B0), 1 H-bridge motor driver (L293D), 1 octocouplers (4NE5), 2 MOSFET transistors (IRF520), 5 capacitors (100uF), 5 diodes (1N4007), 3 transparent gels (R,G,B) 1 male pin strip (40 x 1), 20 resistors (220 ohm), 5 resistors (560 ohm), 5 resistors (1 kilohm), 5 resistors (4.7 kilohm), 20 resistors (10 kilohm), 5 resistors (1 megohm), 5 resistors (10 megohm)

 

Included Projects: I Love You Pillow, Puzzle Box, Pavlov's Cat, The Nerd, and Plant Communicator,

  • Allows you to turn your Arduino form factor based project into a MKR based one
  • Integrated LiPo battery charger
  • Operating Voltage 3.3V / DC
  • Current 700 mA
  • Input Voltage (recommended): 7-12V
  • Features 14 Digital I/O Pins, 6 Analog Input Pins and 1 Analog Output Pin Compatible with Arduino Uno

 

Example Projects: Clustered MCUs
Arduino Powered MSE-6 (Mouse Droid) - Droid in ActionFingerprint Skeleton Key - RFID Module
You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image
You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image
Clustered MCUs Vote or Submit Your Ideas!

Here's to the crazy ones: the theme this month is Clustered MCUs and it comes from 14rhb.  You can do any project that involves two or more MCUs. To make things interesting we are offering a Grand Prize Package of an Arduino MKR IoT Bundle(includes the MKR1000 Dev Board), an MKR1000 & Uno Shield Interface Adapter Board, an Arduino Uno, and some swag for the craziest project that uses two or more microcontrollers!

 

You can use any two microcontrollers or combinations of microcontrollers from any manufacturer.  It doesn't matter what board its on.  Arduino  is a popular choice for many of you on the community and it would be great to see some more Arduino Projects .  The MKR1000 kit and MKR1000 & Shield Interface were originally ordered in advance of the Open Arduino competition.  This was held to celebrate the birthday of Project14 by celebrating the birthday of Arduino .  They were also included in the kit used for the Design for a Cause - Design Challenge .

 

When we had the Project14 | The Birthday Special: Open Arduino: The Winners Announcement! , the grand prize was still waiting on the MKR1000 Kit and shield interface.  jomoenginer was the grand prize for his Imperial Mouse Droid project.  It used both an Arduino Uno and an Arduino Yun. Luckily,  Arduino who was sponsoring the Design for a Cause - Design Challenge stepped up to send over an MKR1000 Kit and MKR1000 & Shield interface and get it included with the rest of the Grand Prize winnings!

 

 

Submission Deadline: Submit any project that combines two or more microcontrollers from now until October 15th!

 

Upcoming Contests:

 

Arduino MKR WAN 1300 (LoRa Connectivity)Arduino MKR Vidor 4000 (on board FPGA)
imageimage
Buy NowBuy NowBuy NowBuy Now
You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image
You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Arduino MKR WAN 1300 allows you to add Lo-Ra connectivity to your projects with minimum previous experience in networking. It is based on the Atmel SAMD21 and a Murata  CMWX1ZZABZ Lo-Ra module.

 

Its design allows you to power the board using two 1.5V AA or AAA batteries or external 5V.  Switching from one source to the other is done automatically. A good 32 bit computational power similar to the MKR ZERO board, the usual rich set of I/O interfaces, low power Lo-Ra communication and the ease of use of the Arduino Software (IDE) for code development and programming.

 

All these features make this board the preferred choice for the emerging IoT battery-powered projects in a compact form factor. The USB port can be used to supply power (5V) to the board. The Arduino MKR WAN 1300 is able to run with or without the batteries connected and has limited power consumption.

With the MKR VIDOR 4000 you can configure it the way you want; you can essentially create your own controller board. It comes loaded with hardware and potential: an 8 MB SRAM; a 2 MB QSPI Flash chip — 1 MB allocated for user applications; a Micro HDMI connector; an MIPI camera connector; and Wifi & BLE powered by U-BLOX NINA W10 Series.

 

It also includes the classic MKR interface on which all pins are driven both by SAMD21 and FPGA. Plus, it has a Mini PCI Express connector with up to 25 user programmable pins. The FPGA contains 16K Logic Elements, 504 KB of embedded RAM, and 56 18x18 bit HW multipliers for high-speed DSP.

 

Each pin can toggle at over 150 MHz and can be configured for functions such as UARTs, (Q)SPI, high resolution/high frequency PWM, quadrature encoder, I2C, I2S, Sigma Delta DAC, etc. The on-board FPGA can be also used for high-speed DSP operations for audio and video processing. This board also features a Microchip SAMD21. Communication between FPGA and the SAMD21 is seamless.

In the comments below help come up with themes to do around the following MKR Add ons:

 

 

Arduino MKR ETH ShieldArduino MKR Connector Carrier
imageimage
Buy NowBuy NowBuy NowBuy Now

Are you developing a project for an environment where wireless connections are unavailable or would be inefficient? The MKR ETH shield allows to have a wired Ethernet connection between your MKR board and your network or the Internet. This is particularly useful for devices located where either electromagnetic noise is a problem or there are special safety requirements.

Do you have several components to connect to your project and would rather use connectors instead of soldering? The Arduino MKR CONNECTOR CARRIER provides Seeed Studio's Grove connectors to your MKR board. The MKR CONNECTOR CARRIER shield is an essential tool for rapidly prototyping activity. It allows you to connect easily and quickly sensors with Grove connectors. This shield can allow you to build applications with different IoT connectivities by simply changing the MKR board and with almost no changes to the code.

In the comments below help come up with themes to do around the following MKR Add ons:

 

 

Arduino MKR MEM ShieldArduino MKR Relay Shield
imageimage
Buy NowBuy NowBuy NowBuy Now

The Arduino MKR MEM shield will allow you to add more flash memory and storage. It provides 2-megabytes of flash memory. It also includes a slot for adding a microSD card to store several gigabytes of storage. This can allow you to store data for later analysis.

In the comments below help come up with themes to do around the following MKR Add ons:

 

 

 

You Can Help Decide the Next Two Themes in the Comments Below!

 

The Next Contest Will Begin on September 17th and have winners selected on October 15th!

 

It will be Followed By another Contest that will Begin on October 1st and winners selected after November 1st 

 

 

In the comments below help come up with themes to do around Arduino MKR LoRa and Arduino MKR Vidor!

 

The Grand Prize:

 

An Arduino Engineering Kit will be sent to the member whose project demonstrates the best use of the new MKR board for engineering.  You don't need to win any of these boards to qualify for the grand prize.  Simply have your MKR project up by December 3rd and we'll pick a winner on December 10th.  Be sure to tag it with mkr_projects or post it in Arduino Projects !

 

 

Arduino Engineering Kit - MATLAB/SIMULINK
imageimage
Buy NowBuy Now

Each Arduino Engineering Kit includes:

 

BOARDS
  • 1 Arduino MKR1000 Board
  • 1 Arduino MKR Motor Shield
  • 1 Arduino MKR IMU Shield

 

 

ELECTRICAL COMPONENTS

  • 1 DC Motor
  • 2 Geared DC Motors with Encoder
  • 1 Standard Micro Servo (180 degrees)
  • 1 Hall Sensor Module
  • 1 Ultrasonic Sensor Module
  • 1 Webcam
  • 1 LiPo Battery
  • 1 LiPo Battery Charger
  • 1 Micro USB Cable
  • 1 3-pin to 4-pin Tinkerkit Module Cable
  • 1 3-pin Tinkerkit Module Cable MECHANICAL

COMPONENTS

  • 3 Sets of Assembly Pieces
  • 2 Wheels
  • 1 Caster Wheel
  • 1 Timing Belt
  • 2 Timing Pulley
  • 2 DC Motor Mounting Brackets
  • 1 Metal Shaft (90mm)
  • 2 Metal D Shafts (50mm)
  • 2 Sets of Distance Spacers (6mm, 17mm)
  • 2 Sets of M2 Bolts (10mm, 25mm)
  • 3 Sets of M3 Bolts (10mm, 15mm, 25mm)
  • 1 Set of M2 Nuts
  • 1 Set of M3 Nuts
  • 1 Set of M3 Lock Nuts with Nylon Insert
  • 3 Shaft Collars
  • 1 Propeller Adapter Screw
  • 2 Magnets Ø8 mm
  • 1 Thread 5m
  • 2 Whiteboard Pens
  • 1 Sticker for Vision Recognition

The Arduino Engineering Kit is the ideal solution for university students, providing a state-of-the-art, hands-on incorporation of Arduino technology in an educational setting.

 

The kit is primarily for three types of users:

  • Students learning about engineering at a university or at a vocational school (e.g., Introductory Engineering, Controls, Mechatronics courses);
  • Professors teaching engineering who also want practical resources to demonstrate engineering concepts;
  • Makers with an interest or background in engineering, either professionally or as a hobby.

The Arduino Engineering Kit covers fundamental engineering concepts, key aspects of mechatronics, and MATLAB and Simulink programming.Included projects challenges students intellectually and helps develop physical engineering skills — and they’re just fun to do.

  • Self-Balancing Motorcycle This motorcycle will maneuver on its own on various terrains and remain upright using a flywheel for balance. It’s very exciting to build and to see in action.
  • Mobile Rover This vehicle can navigate between given reference points, move objects with a forklift and much more. It’s very fun to make and use.
  • Whiteboard Drawing Robot This amazing robot can take a drawing it’s given and duplicate it on a whiteboard. It’s most impressive.

 

The kit is sold in a hard plastic, stackable tool box for storage and years of reuse. Inside the box is an easy-to-use Arduino MKR1000 board, several customized parts, and a complete set of electrical and mechanical components needed to assemble all three projects

  • Sign in to reply
  • Cancel

Top Replies

  • 14rhb
    14rhb over 7 years ago +6
    When I look at the Arduino Vidor 4000, with its FPGA capability and SAMD21, I can't get away from thinking it would make a really great, reconfigurable and portable analysis tool. Perhaps a tool that could…
  • 14rhb
    14rhb over 7 years ago in reply to 14rhb +6
    After saying that I became really intrigued with what the Vidor 4000 can offer....and you know how one thing often leads to another. The postman has just called Rod
  • 14rhb
    14rhb over 7 years ago +5
    If anyone is a bit confused whether these products are standalone controller boards or shields then this diagram from the Arduino site should help: Source [ https://www.arduino.cc/en/Main/Products ] R…
  • 14rhb
    14rhb over 7 years ago

    When I look at the Arduino Vidor 4000, with its FPGA capability and SAMD21, I can't get away from thinking it would make a really great, reconfigurable and portable analysis tool. Perhaps a tool that could capture and display or create and replay SPI/I2C/UART data to investigate if a project is working.

     

    Once a basic setup is created and the amount of resource is better understood there might be enough to add additional functionality. It has an DAC so could also be used to create some basic waveforms (aka function generator) and some user defined patterns. Also being reconfigurable would allow the user to download additional functionality to replace existing ones should the device resources be insufficient for multiple setups (e.g. they may wish to create DMX512 signals for lighting control tests).

     

    Arduino Gets into FPGAs with MKR Vidor 4000

     

    Rod

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to 14rhb

    Hi Rod,

     

    It's a really great idea. Small portable tools are underrated but times have changed and lightweight hardware like this is powerful.

    Plus if it is (hopefully) easy-to-obtain and operate hardware like these Arduino boards, more people will use it to learn and troubleshoot what circuits are doing, which can only be a good thing.

    There are too many 1khz oscilloscopes based on the very resource constrained Uno, which goes to show nevertheless that people are motivated to use Arduino hardware for small tools.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • fmilburn
    fmilburn over 7 years ago

    I had a look at the datasheet for the engineering kit and it looks quite impresiive.  Several fun projects well beyond the usual stuff and educational documentation included.  Very nice...

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • 14rhb
    14rhb over 7 years ago

    If anyone is a bit confused whether these products are standalone controller boards or shields then this diagram from the Arduino site should help:

    image

    Source [https://www.arduino.cc/en/Main/Products ]

     

    Rod

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • 14rhb
    14rhb over 7 years ago in reply to 14rhb

    After saying that I became really intrigued with what the Vidor 4000 can offer....and you know how one thing often leads to another. The postman has just called image

    image

    Rod

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
  • tariq.ahmad
    tariq.ahmad over 7 years ago

    Hey 14rhb ,

     

    We'll be setting up a contest that focuses on the MKR Vidor 4000 and would love to hear what you have planned for your board!

     

    Are there any shields from here:

     

    Arduino | Upcoming MKR Livestreams, MKR Giveaways, and Arduino Engineering Kit Grand Prizes!

     

    These giveaways will be running throughout Massimo's 5 part series on the commercial uses of Arduino.

     

    Thinking of perhaps pulling together a poll with the ideas we receive to further explore what uses the community members have for the new MKR line....

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • 14rhb
    14rhb over 7 years ago in reply to tariq.ahmad

    tariq.ahmad

     

    Hi Tariq,

     

    I must admit I hadn't really looked at this new MKR range until your set of articles appeared. I then read a bit and got 'pulled in' - as well as the Vidor4000 I have a MKR WIFI 1010 on order. My excuse is that we're heading towards winter in the Northern Hemisphere so it is time to stock up on the fun stuffimage

     

    I'd like to use the Vidor4000 to make a device that helps me analyse bus signals and protocols - grabbing the bit stream and decoding it to bytes. At the same time being able to output a known pattern of bytes to aid testing of devices. That data can then be transferred to a host PC in slow-time for displaying. I'd look at SPI and I2C first, then UART/COM port.

     

    In my opinion, shields that look useful in supporting your great series include:

    (1) the MKR RS485 Shield: this would allow interfacing to the DMX512 standard. This could then be used to make a portable DMX512 lighting tester

    (2) the MKR MEM Shield: extending the amount of data that could be captured from the SPI/I2C capture

    (3) the MKR CAN Shield: the most obvious application use being a car fault code reader but there are many other safety critical applications it could be purposed to including robotics.

    (4) lastly the MKR Connector Carrier: this would make an ideal companion for the CAN shield application, allowing addition of servos etc as they could couple in some via the Grove connectors on this board Grove Inventor Kit + BBC micro:bit

     

    I found a video my Massimo Banzi detailing the Vidor4000 and that Arduino plan to produce some form of easy-to-use visual IDE. I'm looking forward to that as I'm hoping to use my Vidor4000 board when I want a quick solution rather than spending hours/days programming something like the Digilent Arty S7.

     

    Hope that helps,

     

    Rod

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • fmilburn
    fmilburn over 7 years ago

    I am interested in LoRa.  The project I have in mind would require one MKR WAN 1300 transmitting environmental data from a buoy or RC type controlled boat and a second MKR WAN 1300 base unit to receive.

    image

    LoRa is ideal for the application I have in mind since it is low power and being over water there is line of sight for the relatively long distances I would investigate.  LoRa would be used to communicate both data from the field unit and commands from the base unit.  The data being recorded might include temperature of water and air, water turbidity, location, etc.  At some point a small boat could be made autonomous similar to drones that have GPS with set waypoints and the ability to return to base.  Collected water samples could be taken at waypoints.

     

    Three are other shields that might prove useful - e.g. the relay shield.  I would have to think some more about that.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • 14rhb
    14rhb over 7 years ago in reply to fmilburn

    Hi Frank,

     

    Sounds like a useful idea. You could use the GPS to Dynamically Position (DP) your boat by means of some thrusters until the required time has elapsed....that would be cool, especially where tides and currents would normally take if 'off station'.

     

    Rod

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • fmilburn
    fmilburn over 7 years ago in reply to 14rhb

    This may be my next longer term project image   Remote sensing at sea is becoming an active area for amateur science.