Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Where is TCL file for microzed ZYNQ-7010?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 373 subscribers
  • Views 697 views
  • Users 0 members are here
  • avnet_zed
Related

Where is TCL file for microzed ZYNQ-7010?

dexterous.me82
dexterous.me82 over 6 years ago

I am trying to use xilinix JTAG to load uboot.elf on to the RAM.

However, I need the tcl file to preset the processor settings.

 

source "tcl file" so that it can load my uboot.elf.

 

 

  • Sign in to reply
  • Cancel
  • drozwood90
    drozwood90 over 6 years ago

    All build artifacts would be present under the project build folder on your hard drive.

     

    --Dan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • narrucmot
    narrucmot over 6 years ago

    What you need is the Zynq First Stage Boot Loader (FSBL) elf file.  This, along with the u-boot elf file and PL bitstream (if you have one), can be used to boot via JTAG or can be packaged into a boot.bin file for booting via SD card, etc.  A good place to start with learning the flow of booting u-boot and Linux is one of Avnet's posted PetaLinux BSPs for the MicroZed SOMs.  Xilinx User Guide 1144 is an excellent resource developing with PetaLinux.

     

    --Tom

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dexterous.me82
    dexterous.me82 over 6 years ago in reply to narrucmot

    I did that but I can't see anything on the console.

     

    Serial console is blank when I write fsbl.elf to RAM using JTAG?

     

    I have generated fsbl.elf using Symbols - FSBL_DEBUG_INFO.

    I do see that if I create a boot gen image using this FSBL.elf and place in SD card.

    And then if I change the jumper to SD card mode, I see FSBL prints on the console.

    However, I don't see prints coming on to the serial port if I do load the

    fsbl.elf using JTAG and JTAG mode.

     

     

    xsct% targets 2

    xsct% source ps7_init.tcl

    Info: ARM Cortex-A9 MPCore #0 (target 2) Stopped at 0xffffff28 (Suspended)

    Info: ARM Cortex-A9 MPCore #1 (target 3) Stopped at 0xffffff34 (Suspended)

    Downloading Program -- C:/Users/abc/Downloads/JTAG_microzed_zynq7010/fsbl.elf

            section, .text: 0x00000000 - 0x0000fedb

            section, .handoff: 0x0000fedc - 0x0000ff27

            section, .init: 0x0000ff28 - 0x0000ff3f

            section, .fini: 0x0000ff40 - 0x0000ff57

            section, .rodata: 0x0000ff58 - 0x000112d3

            section, .data: 0x000112d8 - 0x00014047

            section, .eh_frame: 0x00014048 - 0x0001404b

            section, .mmu_tbl: 0x00018000 - 0x0001bfff

            section, .init_array: 0x0001c000 - 0x0001c003

            section, .fini_array: 0x0001c004 - 0x0001c007

            section, .rsa_ac: 0x0001c008 - 0x0001d03f

            section, .bss: 0x0001d040 - 0x0001ee71

            section, .heap: 0x0001ee72 - 0x00020e7f

            section, .stack: 0xffff0000 - 0xffffd3ff

    100%    0MB   0.1MB/s  00:01

    Setting PC to Program Start Address 0x00000000

    Successfully downloaded C:/Users/abc/Downloads/JTAG_microzed_zynq7010/fsbl.elf

     

     

    Infact, I wrote a simple hello world program. However, this hello world isn't

    appearing on the console.