Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General LVDS Differential Clock to Single Ended
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 373 subscribers
  • Views 2623 views
  • Users 0 members are here
  • Zynq Mini-Module Plus (MMP) Hardware Design
  • zedboardcmty
Related

LVDS Differential Clock to Single Ended

cybero
cybero over 6 years ago

Hi, I'm using the Zynq Mini-Module Plus.

This board comes with a LVDS clock. Taking a look at the XDC provided by AVNET we can see:

 

## 200MHz System Clock

set_property LOC F14 [ get_ports CLK_N]

set_property IOSTANDARD LVDS [ get_ports CLK_N]

 

 

set_property LOC F15 [ get_ports CLK_P]

set_property IOSTANDARD LVDS [ get_ports CLK_P]

So, I wonder how can I convert this LVDS clock into a single ended clock because I've never seen this before. I've always worked with FPGA with single ended clocks so I'm a bit lost on this now.

 

Thanks in advance for the help.

  • Sign in to reply
  • Cancel

Top Replies

  • cybero
    cybero over 5 years ago +3
    Hi guys, Thanks for your replies. I would like to answer myself with the solution that I chose: to place an IBUFDS IBUFDS #( .CAPACITANCE("DONT_CARE"), .DIFF_TERM("FALSE"), .IBUF_DELAY_VALUE("0"), .IFD_DELAY_VALUE…
  • saadtiwana_int
    saadtiwana_int over 6 years ago +1
    Hi Salvador, Keep in mind that once any signal enters the FPGA, there is no more differential signals; everything is single ended. However, outside the FPGA (whether input or output) differential signals…
Parents
  • saadtiwana_int
    saadtiwana_int over 6 years ago

    Hi Salvador,

     

    Keep in mind that once any signal enters the FPGA, there is no more differential signals; everything is single ended. However, outside the FPGA (whether input or output) differential signals can be/are used whenever the signals are at higher frequncies for reasons like signal integrity, etc

     

    I haven't looked at the schematic of Zynq MMP, but from the XDC file, it looks like this is your system input clock. Since it is a differential clock, it is being given on a differential pin pair. However, inside the IO block in your FPGA where these are getting connected, these will be converted from differential to single ended clock, and most probably drive a clock region, and after that you don't need to worry about differential clocks...everything is single ended inside. Hope it helps you understand.

     

    Best Regards,
    Saad I. Tiwana

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • saadtiwana_int
    saadtiwana_int over 6 years ago

    Hi Salvador,

     

    Keep in mind that once any signal enters the FPGA, there is no more differential signals; everything is single ended. However, outside the FPGA (whether input or output) differential signals can be/are used whenever the signals are at higher frequncies for reasons like signal integrity, etc

     

    I haven't looked at the schematic of Zynq MMP, but from the XDC file, it looks like this is your system input clock. Since it is a differential clock, it is being given on a differential pin pair. However, inside the IO block in your FPGA where these are getting connected, these will be converted from differential to single ended clock, and most probably drive a clock region, and after that you don't need to worry about differential clocks...everything is single ended inside. Hope it helps you understand.

     

    Best Regards,
    Saad I. Tiwana

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • drozwood90
    drozwood90 over 6 years ago in reply to saadtiwana_int

    Hi there,

     

    Agreed.  You can just use "CLK_P" or "CLK_N" in your code (depending on which polarity you want).

     

    --Dan