Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Yocto BSP
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 13 replies
  • Subscribers 374 subscribers
  • Views 2031 views
  • Users 0 members are here
Related

Yocto BSP

e14 Contributor
e14 Contributor over 14 years ago

Is there any interest in a Yocto BSP for the zedboard? I can probably get a basic one together fairly easily, well if I can ever get a zedboard :)

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    I'm actually setting it up, so here's an overlay that adds support for Zedboard.

    https://github.com/milosoftware/meta-zynq

    Currently it builds u-boot and BOOT.bin (you'll need to have a FSBL binary to create BOOT.bin) and boots a rootfs from SD card.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    I'm actually setting it up, so here's an overlay that adds support for Zedboard.

    https://github.com/milosoftware/meta-zynq

    Currently it builds u-boot and BOOT.bin (you'll need to have a FSBL binary to create BOOT.bin) and boots a rootfs from SD card.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    I am working my way through it now.  Are there any zedboard specific instructions/settings?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Just ask if you have any questions...

    If you build "my-image" on the Zed, and (optionally) build the bitstream for the ADI framebuffer, you get a nice base image that fits in the internal flash.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    This evening I am getting git failures from Xilinx. Specifically U-Boot... Did something change.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    WARNING: Failed to fetch URL git://git.xilinx.com/u-boot-xarm.git;protocol=git, attempting MIRRORS if available
    ERROR: Fetcher failure: Fetch command failed with exit code 128, output:
    Cloning into bare repository '/home/cah/Backup/Code/zedboard/meta-zynq/oe-core/build/downloads/git2/git.xilinx.com.u-boot-xarm.git'...

    fatal: The remote end hung up unexpectedly

    ERROR: Function failed: Fetcher failure for URL: 'git://git.xilinx.com/u-boot-xarm.git;protocol=git'. Unable to fetch URL from any source.
    ERROR: Logfile of failure stored in: /home/cah/Backup/Code/zedboard/meta-zynq/oe-core/build/tmp-eglibc/work/zynq_zc702-oe-linux-gnueabi/u-boot-zynq/xilinx-zc702-r1/temp/log.do_fetch.14282
    ERROR: Task 67 (/home/cah/Backup/Code/zedboard/meta-zynq/oe-core/meta-zynq/recipes-bsp/u-boot/u-boot-zynq_git.bb, do_fetch) failed with exit code '1'

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    It is up and running again.. (for now)
    While I am here your how to has a couple of tweeks I would make

    metz-zynq -> meta-zynq
    MACHINE = "zynq-zc702 -> MACHINE ?= "zynq-zc702
    Now clone the meta-zynq layer in the oe-core directory ->
    Which oe-core directory?  You have them nested.  Can you make it more clear?

    I note your bug on BOOT.BIN and just use ISE.  Can you go through a short procedure of producing the BOOT.BIN?  If nothing else can you link to the Xilinx documentation that spells it out?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Can you give a bit more context, I don't understand any of your questions/suggestions.

    Contact me by e-mail if you like, because it's a pain to post anything on this board, I don't visit it often...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Any idea what could cause this?

    ERROR: Function failed: do_compile (see /home/cah/Backup/Code/zedboard/meta-zynq/oe-core/build/tmp-eglibc/work/zynq_zc702-oe-linux-gnueabi/u-boot/v2011.06+git13+b1af6f532e0d348b153d5c148369229d24af361a-r3/temp/log.do_compile.3932 for further information)
    ERROR: Logfile of failure stored in: /home/cah/Backup/Code/zedboard/meta-zynq/oe-core/build/tmp-eglibc/work/zynq_zc702-oe-linux-gnueabi/u-boot/v2011.06+git13+b1af6f532e0d348b153d5c148369229d24af361a-r3/temp/log.do_compile.3932
    Log data follows:
    | DEBUG: Executing shell function do_compile
    | NOTE: make -j 8 CROSS_COMPILE=arm-oe-linux-gnueabi- CC=arm-oe-linux-gnueabi-gcc  --sysroot=/home/cah/Backup/Code/zedboard/meta-zynq/oe-core/build/tmp-eglibc/sysroots/zynq-zc702 zynq_zc70x_config
    | awk '(NF && $1 !~ /^#/) { print $1 ": " $1 "_config; $(MAKE)" }' boards.cfg > .boards.depend
    | make: *** No rule to make target `zynq_zc70x_config'.  Stop.
    | make: *** [zynq_zc70x_config] Error 1
    | ERROR: oe_runmake failed
    | ERROR: Function failed: do_compile (see /home/cah/Backup/Code/zedboard/meta-zynq/oe-core/build/tmp-eglibc/work/zynq_zc702-oe-linux-gnueabi/u-boot/v2011.06+git13+b1af6f532e0d348b153d5c148369229d24af361a-r3/temp/log.do_compile.3932 for further information)
    ERROR: Task 6 (/home/cah/Backup/Code/zedboard/meta-zynq/oe-core/oe-core/meta/recipes-bsp/u-boot/u-boot_2011.06.bb, do_compile) failed with exit code '1'
    NOTE: Tasks Summary: Attempted 490 tasks of which 484 didn't need to be rerun and 1 failed.
    No currently running tasks (490 of 497)

    Summary: 1 task failed:
      /home/cah/Backup/Code/zedboard/meta-zynq/oe-core/oe-core/meta/recipes-bsp/u-boot/u-boot_2011.06.bb, do_compile
    Summary: There was 1 ERROR message shown, returning a non-zero exit code.