Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Segmentation fault
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 373 subscribers
  • Views 532 views
  • Users 0 members are here
Related

Segmentation fault

e14 Contributor
e14 Contributor over 13 years ago

Dear All,

I was trying to solder two wires to my board's power input. Then it turned out that the power fuse is dead after soldering! :-(

Now after that this issue has been fixed, when I transfer a compiled program into my zynq linux I either receive "Segmentation fault" or "Illegal instruction" error while I run my program. Although there is no problem with the built-in programs.

What might be the possible problem(s)?!

All the best,
Rzi

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    To add on to Kevin's response, I would suggest running your applications in the qemu emulator to ensure that it is not compiled incorrectly.  Directions on downloading the emulator here:

    http://wiki.xilinx.com/zynq-qemu

    Download, extract, and run the emulator.  There is an FTP server that is loaded up in the ram-disk image.  You can ftp into the qemu VM with this command:

    $ ftp 127.0.0.1 10021

    Let us know if the files are compiled correctly (run within the qemu VM) and if they are we can debug the hardware form there.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    To add on to Kevin's response, I would suggest running your applications in the qemu emulator to ensure that it is not compiled incorrectly.  Directions on downloading the emulator here:

    http://wiki.xilinx.com/zynq-qemu

    Download, extract, and run the emulator.  There is an FTP server that is loaded up in the ram-disk image.  You can ftp into the qemu VM with this command:

    $ ftp 127.0.0.1 10021

    Let us know if the files are compiled correctly (run within the qemu VM) and if they are we can debug the hardware form there.