Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General USB-to-UART Recognition Issue Windows 7
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 9 replies
  • Subscribers 374 subscribers
  • Views 969 views
  • Users 0 members are here
Related

USB-to-UART Recognition Issue Windows 7

e14 Contributor
e14 Contributor over 13 years ago

Recently I received my ZedBoard after a long decision process I went through for choosing a development board. My intentions are to use it mostly for hardware design and yes it has a interesting smell (reminds me of soy-sauce).
My problem occurs when using the usb-uart bridge to communicate via terminal program. I connected the micro usb cable from J14 to my computers usb port several times like in the GettingStartedGuide p.11/p.12 described, but the drivers are not automatically installed by win7. So I manually installed the drivers like in the cypress CY7C64225 usb-to-uart setup guide described (several times), but the device is not recognized. The only way the drivers are automatically  installed correctly on the win7 machine and a serial connection can be obtained through the terminal software, is when a powered monitor is connected to the vga connector.
Can anyone tell me what I am doing wrong here or do I allways have connected a monitor to the ZedBoard to communicate via the cypress device?

thanks and regards
pkarch3000

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    I'm having an issue with the USB to UART drivers from Cypress.  When I connect the USB cable to my Windows 7 machine, sometimes it detects a Diligent device and installs drivers for a USB serial converter.  However, no comm ports are available under the device manager.  I've downloaded the CyUSBSerial_v3 drivers from Cypress but when I try and update the driver through device manager, it says no suitable drivers were found in the directory containing the drivers.  I'm a little lost now.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    I'm having an issue with the USB to UART drivers from Cypress.  When I connect the USB cable to my Windows 7 machine, sometimes it detects a Diligent device and installs drivers for a USB serial converter.  However, no comm ports are available under the device manager.  I've downloaded the CyUSBSerial_v3 drivers from Cypress but when I try and update the driver through device manager, it says no suitable drivers were found in the directory containing the drivers.  I'm a little lost now.