Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General bitstream
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 367 subscribers
  • Views 1019 views
  • Users 0 members are here
Related

bitstream

Former Member
Former Member over 13 years ago

Hi, I have a problem in sending the bitstream to the ZedBoard

I'm using windows Vista 32 bit
I started with SW 14.1 and now Iu2019m in 14.2

1) I connected Teraterm through usb port J14, I booted from SD then I grounded JP9 and JP10, and I got the message:
Program FPGA failed
Reason:
FPGA configuration encountered errors.
2) I connected to J14, booted from SD, grounded JP9-JP10, then connected to J17 (USB-JTAG): got the FPGA error as above
3) I connected to J17, booted from SD, grounded JP9-JP10: got the FPGA error as above

Is there something else that I have to do?

If go to iMPACT and click on u201Cboundary scanu201D receive: u201Cright click to add device or initialize JTAG chainu201D
If I right click and then u201Cinitialize chainu201D I get the error message: u201CWARNING:iMPACT:923 u2013 Can no find cable, check cable setup!

If I right click and then u201Ccable setupu201D I get the error message: u201CERROR:iMPACT u2013 This function requires that a target is opened first.u201D

I wonder:
- is there any jumper configuration that I miss?
- And then what usb port do I have to use to send the bitstream, the J14 (USB-UART) or the J17 (USB-JTAG)?

Do I have a not working ZedBoard?

best regards,

Roberto

  • Sign in to reply
  • Cancel
Parents
  • bhfletcher
    0 bhfletcher over 13 years ago

    That's strange, as the Digilent drivers are supposed to get installed with the ISE 14.2, unless you uncheck the Cable Drivers option during your install.  In any case, I'm glad that you got this working.

     

    In the future, if you have problems with your Digilent JTAG, you can reinstall the Digilent JTAG directly from your Xilinx installation.  For example, on my Win7 64-bit machine, I can go to C:\Xilinx\14.2\ISE_DS\common\bin\nt64\digilent and find install_digilent.exe, which allows me to reinstall the Digilent JTAG without downloading from the Digilent site or reinstalling from the ISE installer.

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • bhfletcher
    0 bhfletcher over 13 years ago

    That's strange, as the Digilent drivers are supposed to get installed with the ISE 14.2, unless you uncheck the Cable Drivers option during your install.  In any case, I'm glad that you got this working.

     

    In the future, if you have problems with your Digilent JTAG, you can reinstall the Digilent JTAG directly from your Xilinx installation.  For example, on my Win7 64-bit machine, I can go to C:\Xilinx\14.2\ISE_DS\common\bin\nt64\digilent and find install_digilent.exe, which allows me to reinstall the Digilent JTAG without downloading from the Digilent site or reinstalling from the ISE installer.

     

    Bryan