Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General bitstream
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 367 subscribers
  • Views 1019 views
  • Users 0 members are here
Related

bitstream

Former Member
Former Member over 13 years ago

Hi, I have a problem in sending the bitstream to the ZedBoard

I'm using windows Vista 32 bit
I started with SW 14.1 and now Iu2019m in 14.2

1) I connected Teraterm through usb port J14, I booted from SD then I grounded JP9 and JP10, and I got the message:
Program FPGA failed
Reason:
FPGA configuration encountered errors.
2) I connected to J14, booted from SD, grounded JP9-JP10, then connected to J17 (USB-JTAG): got the FPGA error as above
3) I connected to J17, booted from SD, grounded JP9-JP10: got the FPGA error as above

Is there something else that I have to do?

If go to iMPACT and click on u201Cboundary scanu201D receive: u201Cright click to add device or initialize JTAG chainu201D
If I right click and then u201Cinitialize chainu201D I get the error message: u201CWARNING:iMPACT:923 u2013 Can no find cable, check cable setup!

If I right click and then u201Ccable setupu201D I get the error message: u201CERROR:iMPACT u2013 This function requires that a target is opened first.u201D

I wonder:
- is there any jumper configuration that I miss?
- And then what usb port do I have to use to send the bitstream, the J14 (USB-UART) or the J17 (USB-JTAG)?

Do I have a not working ZedBoard?

best regards,

Roberto

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 12 years ago

    Hey
    I generated the system.bit unfortunately when I want export hardware for sdk I can't chekck the box include bitstream I don't understand. I use the ise 14.4. Do you have ideas of the problem ?
    Cordially.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 12 years ago

    Hey
    I generated the system.bit unfortunately when I want export hardware for sdk I can't chekck the box include bitstream I don't understand. I use the ise 14.4. Do you have ideas of the problem ?
    Cordially.